<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Layerscape中的主题 Re: LS1046 I2C problem</title>
    <link>https://community.nxp.com/t5/Layerscape/LS1046-I2C-problem/m-p/810362#M3610</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;thank you for your quick answer.&lt;/P&gt;&lt;P&gt;The value of SCFG_RCWMUXCR0 was 00330000 and when I set it to 0 the IIC3 started to work.&lt;/P&gt;&lt;P&gt;Concerning with IIC4 I don't know since I couldn't try it so far but I thin so it will work.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But the IIC2....the RCW source is SDHC/MMC, the physical boot source is an eMMC chip that doesn't use the SDHC_CD_B, SDHC_WP&amp;nbsp;&lt;/P&gt;&lt;P&gt;so I thought they could be used for IIC2 and I set the IIC_EXT field in the RCW to use those signals as IIC SDA &amp;amp;&amp;amp; SCL.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank for your help&lt;/P&gt;&lt;P&gt;Gabor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 19 Dec 2018 09:07:23 GMT</pubDate>
    <dc:creator>gaborkocsis</dc:creator>
    <dc:date>2018-12-19T09:07:23Z</dc:date>
    <item>
      <title>LS1046 I2C problem</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1046-I2C-problem/m-p/810360#M3608</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Everybody,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We have made our own custom board based on a LS1046A. LS1046A has four I2C buses. The first works well, but the other three doesn't. In the RCW I've set the appropriate bits to their proper values (Bits 445-447, IIC_EXT field).&lt;/P&gt;&lt;P&gt;Despite of this the I2C2 / I2C3 / I2C4 doesn't work. In the U-BOOT I tried to scan the I2C buses. On the I2C1 the installed devices can be seen, but on the others they can't&amp;nbsp; be seen.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;On the I2C buses we have installed some temperature sensors, their addresses are setup correctly, there can't be address conflicts.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For example I tried the followings:&lt;/P&gt;&lt;P&gt;=&amp;gt; i2c dev 2&lt;BR /&gt;Setting bus to 2&lt;BR /&gt;=&amp;gt; i2c probe&lt;BR /&gt;Valid chip addresses:wait_for_sr_state: Arbitration lost sr=92 cr=0 state=2020&lt;BR /&gt;i2c_init_transfer: failed for chip 0x0 retry=0&lt;BR /&gt;wait_for_sr_state: Arbitration lost sr=92 cr=0 state=2020&lt;BR /&gt;i2c_init_transfer: failed for chip 0x0 retry=1&lt;BR /&gt;wait_for_sr_state: Arbitration lost sr=92 cr=0 state=2020&lt;BR /&gt;i2c_init_transfer: failed for chip 0x0 retry=2&lt;BR /&gt;i2c_init_transfer: give up i2c_regs=0x21a0000&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Where do I have to setup something?&lt;/P&gt;&lt;P&gt;(I've read the QorIQ-SDK-2.0-1703 but I couldn't find relevant info for this problem)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance,&lt;/P&gt;&lt;P&gt;Gabor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 Dec 2018 09:54:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1046-I2C-problem/m-p/810360#M3608</guid>
      <dc:creator>gaborkocsis</dc:creator>
      <dc:date>2018-12-18T09:54:05Z</dc:date>
    </item>
    <item>
      <title>Re: LS1046 I2C problem</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1046-I2C-problem/m-p/810361#M3609</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;1) Concerning IIC2&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Which RCW source is used?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The selection of the SD card for an RCW/PBI source makes the secondary function (SDHC IO's such as SDHC_CD_B, SDHC_WP) available on the I2C2 interface pins, and hence, the I2C2 interface is not available in this configuration.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Additional information can be provided in a Technical Case:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; open &lt;A href="https://community.nxp.com/www.nxp.com" target="test_blank"&gt;www.nxp.com&lt;/A&gt;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; Select "Support" -&amp;gt; "All Support Options"&lt;BR /&gt;&amp;nbsp;&amp;nbsp; Click "Go to Tickets" &lt;BR /&gt;&amp;nbsp;&amp;nbsp; Log in with your NXP login and password &lt;BR /&gt;&amp;nbsp;&amp;nbsp; On the "Group, Create and View your support cases" page press "+ Add a new case" to start the process.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2) Concerning IIC3 &amp;amp; 4&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What is the SCFG_RCWPMUXCR0 value?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 Dec 2018 02:23:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1046-I2C-problem/m-p/810361#M3609</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2018-12-19T02:23:05Z</dc:date>
    </item>
    <item>
      <title>Re: LS1046 I2C problem</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1046-I2C-problem/m-p/810362#M3610</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;thank you for your quick answer.&lt;/P&gt;&lt;P&gt;The value of SCFG_RCWMUXCR0 was 00330000 and when I set it to 0 the IIC3 started to work.&lt;/P&gt;&lt;P&gt;Concerning with IIC4 I don't know since I couldn't try it so far but I thin so it will work.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But the IIC2....the RCW source is SDHC/MMC, the physical boot source is an eMMC chip that doesn't use the SDHC_CD_B, SDHC_WP&amp;nbsp;&lt;/P&gt;&lt;P&gt;so I thought they could be used for IIC2 and I set the IIC_EXT field in the RCW to use those signals as IIC SDA &amp;amp;&amp;amp; SCL.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank for your help&lt;/P&gt;&lt;P&gt;Gabor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 Dec 2018 09:07:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1046-I2C-problem/m-p/810362#M3610</guid>
      <dc:creator>gaborkocsis</dc:creator>
      <dc:date>2018-12-19T09:07:23Z</dc:date>
    </item>
    <item>
      <title>Re: LS1046 I2C problem</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1046-I2C-problem/m-p/810363#M3611</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;1) The selection of the SD card for an RCW/PBI source makes the secondary function (SDHC IO's such as SDHC_CD_B, SDHC_WP) available on the I2C2 interface pins, and hence, the I2C2 interface is not available in this configuration.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Additional information can be provided in a Technical Case:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; open &lt;A href="https://community.nxp.com/www.nxp.com" target="test_blank"&gt;www.nxp.com&lt;/A&gt;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; Select "Support" -&amp;gt; "All Support Options"&lt;BR /&gt;&amp;nbsp;&amp;nbsp; Click "Go to Tickets" &lt;BR /&gt;&amp;nbsp;&amp;nbsp; Log in with your NXP login and password &lt;BR /&gt;&amp;nbsp;&amp;nbsp; On the "Group, Create and View your support cases" page press "+ Add a new case" to start the process.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 Dec 2018 09:45:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1046-I2C-problem/m-p/810363#M3611</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2018-12-19T09:45:17Z</dc:date>
    </item>
  </channel>
</rss>