<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LayerscapeのトピックRe: Porting from MPC8248 to LS1020A</title>
    <link>https://community.nxp.com/t5/Layerscape/Porting-from-MPC8248-to-LS1020A/m-p/431344#M360</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you Lunmin and Alexander,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We will try to following your recommendations&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Victor.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 28 Oct 2015 19:59:28 GMT</pubDate>
    <dc:creator>victormazin</dc:creator>
    <dc:date>2015-10-28T19:59:28Z</dc:date>
    <item>
      <title>Porting from MPC8248 to LS1020A</title>
      <link>https://community.nxp.com/t5/Layerscape/Porting-from-MPC8248-to-LS1020A/m-p/431341#M357</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Our task is to port the Linux operation system and set of servers and drivers (written in C language) from Freescale MPC8248 processor to Freescale LS1020A processor.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Which first steps could you recommend to us?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Victor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 26 Oct 2015 19:27:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Porting-from-MPC8248-to-LS1020A/m-p/431341#M357</guid>
      <dc:creator>victormazin</dc:creator>
      <dc:date>2015-10-26T19:27:19Z</dc:date>
    </item>
    <item>
      <title>Re: Porting from MPC8248 to LS1020A</title>
      <link>https://community.nxp.com/t5/Layerscape/Porting-from-MPC8248-to-LS1020A/m-p/431342#M358</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We do not offer porting guide for this case.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I recommend building a new Linux from our Linux SDK we offer for LS1020A processor, and than port your applications from MPC8248 to LS1020A using build tools supplied in our Linux SDK.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Alexander&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 28 Oct 2015 02:05:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Porting-from-MPC8248-to-LS1020A/m-p/431342#M358</guid>
      <dc:creator>alexander_yakov</dc:creator>
      <dc:date>2015-10-28T02:05:48Z</dc:date>
    </item>
    <item>
      <title>Re: Porting from MPC8248 to LS1020A</title>
      <link>https://community.nxp.com/t5/Layerscape/Porting-from-MPC8248-to-LS1020A/m-p/431343#M359</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Victor Mazin,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you are using new platform other than LS1021ATWR, as Alexander has suggested, you're recommend to porting from Freescale QorIQ SDK, since it has already included support for LS1021A.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Some steps of porting u-boot including creating configuration file based on ls1021atwr.h, ls1021atwr.c, ddr.c, ls1_rcw.cfg, ls1_pbi.cfg and rebuilding images, porting Linux including creating new file based on mach-ls1021a.c, ls1021a_defconfig, new device tree, and so on. There is application note of U-Boot and Linux porting on T4240 system, although it's not for LS1021A I think it may be also helpful.&lt;/P&gt;&lt;P&gt;&lt;A href="http://cache.freescale.com/files/32bit/doc/app_note/AN4814.pdf?fsrch=1&amp;amp;sr=1&amp;amp;pageNum=1" title="http://cache.freescale.com/files/32bit/doc/app_note/AN4814.pdf?fsrch=1&amp;amp;sr=1&amp;amp;pageNum=1"&gt;http://cache.freescale.com/files/32bit/doc/app_note/AN4814.pdf?fsrch=1&amp;amp;sr=1&amp;amp;pageNum=1&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Lunmin&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 28 Oct 2015 03:50:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Porting-from-MPC8248-to-LS1020A/m-p/431343#M359</guid>
      <dc:creator>lunminliang</dc:creator>
      <dc:date>2015-10-28T03:50:25Z</dc:date>
    </item>
    <item>
      <title>Re: Porting from MPC8248 to LS1020A</title>
      <link>https://community.nxp.com/t5/Layerscape/Porting-from-MPC8248-to-LS1020A/m-p/431344#M360</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you Lunmin and Alexander,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We will try to following your recommendations&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Victor.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 28 Oct 2015 19:59:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Porting-from-MPC8248-to-LS1020A/m-p/431344#M360</guid>
      <dc:creator>victormazin</dc:creator>
      <dc:date>2015-10-28T19:59:28Z</dc:date>
    </item>
  </channel>
</rss>