<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic dpaa2_net: dpni disable failed (-110) DPAA2, DPDK in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/dpaa2-net-dpni-disable-failed-110-DPAA2-DPDK/m-p/809156#M3598</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using DPDK on LS2088ardb board.&lt;/P&gt;&lt;P&gt;I have allocated 1 DPNI and connected it to 1 DPMAC.1 (SPF+).&lt;/P&gt;&lt;P&gt;When I start DPDK testpmd application it works and can be closed only if incomming trafic is ~100 pkt/s.&lt;/P&gt;&lt;P&gt;If I send packets on wirespeed from another PC testpmd application can not be closed (even after traffic generator is stopped)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is only one error:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Shutting down port 0...&lt;BR /&gt;Stopping ports...&lt;BR /&gt;dpaa2_net: dpni disable failed (-110)&lt;BR /&gt;dpaa2_net: Failure (ret -110) in disabling dpni 0 dev&lt;BR /&gt;Done&lt;BR /&gt;Closing ports...&lt;BR /&gt;dpaa2_net: Failure cleaning dpni device: err=-110&lt;BR /&gt;Done&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If I run testpmd application it can not receive any packets.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Output from /dev/fsl_mc_console&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;[E:36f3b2a5ec, ifp_mng_cmd_enqueue:1708, CTLU]&amp;nbsp; Busy: No available Management command descriptor&lt;BR /&gt;[E:36f43fbafc, ifp_mng_cmd_enqueue:1708, CTLU]&amp;nbsp; Busy: No available Management command descriptor&lt;BR /&gt;[E:36f4cccaf0, ifp_mng_cmd_enqueue:1708, CTLU]&amp;nbsp; Busy: No available Management command descriptor&lt;/P&gt;&lt;P&gt;....&lt;/P&gt;&lt;P&gt;[E:36f9c18a2e, qbman_rec_isr:354, QBMAN]&amp;nbsp; QBMAN recoverable event 0x20040000&lt;BR /&gt;[E:36fb871426, qbman_rec_isr:387, QBMAN]&amp;nbsp; [FQ#7]: 12036&lt;/P&gt;&lt;P&gt;...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What does error -110 means? Is there any document about&amp;nbsp; /dev/fsl_mc_console ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 01 Aug 2018 12:10:31 GMT</pubDate>
    <dc:creator>nic30</dc:creator>
    <dc:date>2018-08-01T12:10:31Z</dc:date>
    <item>
      <title>dpaa2_net: dpni disable failed (-110) DPAA2, DPDK</title>
      <link>https://community.nxp.com/t5/Layerscape/dpaa2-net-dpni-disable-failed-110-DPAA2-DPDK/m-p/809156#M3598</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using DPDK on LS2088ardb board.&lt;/P&gt;&lt;P&gt;I have allocated 1 DPNI and connected it to 1 DPMAC.1 (SPF+).&lt;/P&gt;&lt;P&gt;When I start DPDK testpmd application it works and can be closed only if incomming trafic is ~100 pkt/s.&lt;/P&gt;&lt;P&gt;If I send packets on wirespeed from another PC testpmd application can not be closed (even after traffic generator is stopped)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is only one error:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Shutting down port 0...&lt;BR /&gt;Stopping ports...&lt;BR /&gt;dpaa2_net: dpni disable failed (-110)&lt;BR /&gt;dpaa2_net: Failure (ret -110) in disabling dpni 0 dev&lt;BR /&gt;Done&lt;BR /&gt;Closing ports...&lt;BR /&gt;dpaa2_net: Failure cleaning dpni device: err=-110&lt;BR /&gt;Done&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If I run testpmd application it can not receive any packets.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Output from /dev/fsl_mc_console&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;[E:36f3b2a5ec, ifp_mng_cmd_enqueue:1708, CTLU]&amp;nbsp; Busy: No available Management command descriptor&lt;BR /&gt;[E:36f43fbafc, ifp_mng_cmd_enqueue:1708, CTLU]&amp;nbsp; Busy: No available Management command descriptor&lt;BR /&gt;[E:36f4cccaf0, ifp_mng_cmd_enqueue:1708, CTLU]&amp;nbsp; Busy: No available Management command descriptor&lt;/P&gt;&lt;P&gt;....&lt;/P&gt;&lt;P&gt;[E:36f9c18a2e, qbman_rec_isr:354, QBMAN]&amp;nbsp; QBMAN recoverable event 0x20040000&lt;BR /&gt;[E:36fb871426, qbman_rec_isr:387, QBMAN]&amp;nbsp; [FQ#7]: 12036&lt;/P&gt;&lt;P&gt;...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What does error -110 means? Is there any document about&amp;nbsp; /dev/fsl_mc_console ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 01 Aug 2018 12:10:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/dpaa2-net-dpni-disable-failed-110-DPAA2-DPDK/m-p/809156#M3598</guid>
      <dc:creator>nic30</dc:creator>
      <dc:date>2018-08-01T12:10:31Z</dc:date>
    </item>
    <item>
      <title>Re: dpaa2_net: dpni disable failed (-110) DPAA2, DPDK</title>
      <link>https://community.nxp.com/t5/Layerscape/dpaa2-net-dpni-disable-failed-110-DPAA2-DPDK/m-p/809157#M3599</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;A _jive_internal="true" data-content-finding="Community" data-userid="308315" data-username="nic30" href="https://community.nxp.com/people/nic30"&gt;nic nic&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is a known issue in our internal system, the development team is working on it now.&lt;/P&gt;&lt;P&gt;When killing the application while the traffic is running.&lt;/P&gt;&lt;P&gt;Application kill with print:&lt;/P&gt;&lt;P&gt;dpaa2_net: dpni disable failed (-110)&lt;BR /&gt; dpaa2_net: Failure (ret -110) in disabling dpni 2 dev&lt;BR /&gt; dpaa2_net: Failure cleaning dpni device: err=-110&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;After this - it is not possible to use the system for dpdk without re-starting the board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Will fix this issue in the coming release.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Aug 2018 08:33:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/dpaa2-net-dpni-disable-failed-110-DPAA2-DPDK/m-p/809157#M3599</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2018-08-15T08:33:49Z</dc:date>
    </item>
  </channel>
</rss>