<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Layerscape中的主题 LS1043ARDB-PD USB console can't work</title>
    <link>https://community.nxp.com/t5/Layerscape/LS1043ARDB-PD-USB-console-can-t-work/m-p/798002#M3532</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;i got LS1043ARDB-PD and start booting it. The USB console port can't work. it always keep in bootloader mode.&lt;/P&gt;&lt;P&gt;i download LS1043ARDB-PD design file and enter&amp;nbsp;k22fx512_ls1020a_if_mbed.bin to bootloader disk. it still keep in bootloader mode after update. could you please help to check thanks?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 06 Sep 2018 09:21:55 GMT</pubDate>
    <dc:creator>tedlin</dc:creator>
    <dc:date>2018-09-06T09:21:55Z</dc:date>
    <item>
      <title>LS1043ARDB-PD USB console can't work</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1043ARDB-PD-USB-console-can-t-work/m-p/798002#M3532</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;i got LS1043ARDB-PD and start booting it. The USB console port can't work. it always keep in bootloader mode.&lt;/P&gt;&lt;P&gt;i download LS1043ARDB-PD design file and enter&amp;nbsp;k22fx512_ls1020a_if_mbed.bin to bootloader disk. it still keep in bootloader mode after update. could you please help to check thanks?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Sep 2018 09:21:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1043ARDB-PD-USB-console-can-t-work/m-p/798002#M3532</guid>
      <dc:creator>tedlin</dc:creator>
      <dc:date>2018-09-06T09:21:55Z</dc:date>
    </item>
    <item>
      <title>Re: LS1043ARDB-PD USB console can't work</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1043ARDB-PD-USB-console-can-t-work/m-p/798003#M3533</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please confirm that the following steps were performed:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Plug in power to LS board. Hold down Reset button while plugging the PC USB cable into the CSAM USB connector on the board.&lt;BR /&gt;On Windows, the board will be mapped as a Mass Storage Device under a volume labelled 'BOOTLOADER'.&lt;BR /&gt;LED for MBED status will blink in green on the board to acknowledge it is in bootloader mode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. Copy the attached binary into the 'BOOTLOADER’&lt;BR /&gt;2. Wait the binary copy to finish; LED for MBED status will blink with higher rate on finish;&lt;BR /&gt;3. Unplug the USB cable from the board, then plug it back in to power cycle the module&lt;BR /&gt;4. The board should be ready to connect to CodeWarrior&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also, there is a known issue with MBED operation under Win10.&lt;/P&gt;&lt;P&gt;This is the work around we have confirmed to fix the mbed issue on Win10 PC's:&lt;BR /&gt;- Go to the "Start" option on the PC and type the command&amp;nbsp; "Services"&lt;BR /&gt;- Than you should see the following "Services" window open&lt;BR /&gt;- Select the "Storage Services" and on the left-hand side of the window click the "Stop the service"&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="Services-Win10.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/68520i5008CF4023C2B09A/image-size/large?v=v2&amp;amp;px=999" role="button" title="Services-Win10.jpg" alt="Services-Win10.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 07 Sep 2018 02:49:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1043ARDB-PD-USB-console-can-t-work/m-p/798003#M3533</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2018-09-07T02:49:00Z</dc:date>
    </item>
    <item>
      <title>Re: LS1043ARDB-PD USB console can't work</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1043ARDB-PD-USB-console-can-t-work/m-p/798004#M3534</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am seeing the same issue with a LS1043ADB .. It worked initially and I had USB console, but now all I ever see is the bootloader drive.&amp;nbsp; I tried using the attached files, but when I removed/replaced the USB I got the bootloader back.&amp;nbsp; This is there a newer version of the bootloader file?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 29 Sep 2019 18:06:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1043ARDB-PD-USB-console-can-t-work/m-p/798004#M3534</guid>
      <dc:creator>snoble</dc:creator>
      <dc:date>2019-09-29T18:06:24Z</dc:date>
    </item>
  </channel>
</rss>