<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Layerscape中的主题 Re: LS2085 IIC AND SDHC Interface.</title>
    <link>https://community.nxp.com/t5/Layerscape/LS2085-IIC-AND-SDHC-Interface/m-p/427093#M341</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN lang="EN-US" style="font-size: 10.0pt;"&gt;If a GPIO pin is used as &lt;/SPAN&gt;&lt;SPAN lang="EN-US" style="font-size: 10.0pt;"&gt;SDHC card detection signal, &lt;/SPAN&gt;&lt;SPAN lang="EN-US" style="font-size: 10.0pt;"&gt;Card insertion status enable (CINSEN) and Card removal status enable (CRMSEN) interrupts should be masked.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="EN-US" style="font-size: 10.0pt;"&gt;If the LS2085 is configured for booting from SDHC, the &lt;/SPAN&gt;&lt;SPAN lang="EN-US" style="font-size: 10.0pt;"&gt;SDHC_CD_B will be assigned to the SDHC not I2C controller.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="EN-US" style="font-size: 10.0pt;"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;/P&gt;&lt;P&gt;Pavel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 20 Oct 2015 09:34:33 GMT</pubDate>
    <dc:creator>Pavel</dc:creator>
    <dc:date>2015-10-20T09:34:33Z</dc:date>
    <item>
      <title>LS2085 IIC AND SDHC Interface.</title>
      <link>https://community.nxp.com/t5/Layerscape/LS2085-IIC-AND-SDHC-Interface/m-p/427092#M340</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I am using LS2085 processor in which IIC2_SCL and SDHC_CD_B pins are multiplexed together. I want to use both of these interfaces IIC and well as SDHC. &lt;/P&gt;&lt;P&gt;SDHC application is for booting purpose while IIC2 is used for&amp;nbsp; DDRs and retimers. My confusion is that will SDHC interface work without using SDHC_CD_B pin since &lt;/P&gt;&lt;P&gt;I am using it as IIC CLK line? I was also planning to use some GPIO to work as SDHC_CD pin, but I am not sure this will work because I am using SDHC for boot purpose&lt;/P&gt;&lt;P&gt;and GPIOs will not be detected before UBOOT.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 04 Sep 2015 13:03:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS2085-IIC-AND-SDHC-Interface/m-p/427092#M340</guid>
      <dc:creator>rahulsoni</dc:creator>
      <dc:date>2015-09-04T13:03:47Z</dc:date>
    </item>
    <item>
      <title>Re: LS2085 IIC AND SDHC Interface.</title>
      <link>https://community.nxp.com/t5/Layerscape/LS2085-IIC-AND-SDHC-Interface/m-p/427093#M341</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN lang="EN-US" style="font-size: 10.0pt;"&gt;If a GPIO pin is used as &lt;/SPAN&gt;&lt;SPAN lang="EN-US" style="font-size: 10.0pt;"&gt;SDHC card detection signal, &lt;/SPAN&gt;&lt;SPAN lang="EN-US" style="font-size: 10.0pt;"&gt;Card insertion status enable (CINSEN) and Card removal status enable (CRMSEN) interrupts should be masked.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="EN-US" style="font-size: 10.0pt;"&gt;If the LS2085 is configured for booting from SDHC, the &lt;/SPAN&gt;&lt;SPAN lang="EN-US" style="font-size: 10.0pt;"&gt;SDHC_CD_B will be assigned to the SDHC not I2C controller.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="EN-US" style="font-size: 10.0pt;"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;/P&gt;&lt;P&gt;Pavel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 20 Oct 2015 09:34:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS2085-IIC-AND-SDHC-Interface/m-p/427093#M341</guid>
      <dc:creator>Pavel</dc:creator>
      <dc:date>2015-10-20T09:34:33Z</dc:date>
    </item>
  </channel>
</rss>