<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Layerscape中的主题 Re: DP DDR memory on LS2088a</title>
    <link>https://community.nxp.com/t5/Layerscape/DP-DDR-memory-on-LS2088a/m-p/774759#M3403</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you do not need for the AIOP then the LS2084A is better. It is like the LS2088A without the AIOP and 32-bit DDR controller. Unfortunately there is not public document which describes how the LS2088A DPAA2 hardware utilizes that DDR memory. Please consider creating a Technical Case to obtain additional information – for the required steps see &lt;/P&gt;&lt;P&gt;&lt;A data-containerid="2009" data-containertype="14" data-content-finding="Community" data-objectid="381898" data-objecttype="1" href="https://community.freescale.com/thread/381898"&gt;How I could create a Service Request?&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 10 Apr 2018 13:18:50 GMT</pubDate>
    <dc:creator>r8070z</dc:creator>
    <dc:date>2018-04-10T13:18:50Z</dc:date>
    <item>
      <title>DP DDR memory on LS2088a</title>
      <link>https://community.nxp.com/t5/Layerscape/DP-DDR-memory-on-LS2088a/m-p/774758#M3402</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P style="margin: 0in 0in 0.0001pt; font-size: 12pt; color: #000000; text-indent: 0px;"&gt;&lt;SPAN style="font-size: 11pt;"&gt;We have an LS2088a based custom board. Do we need to populate the memory associated with 32-bit DDR4 controller (2) on LS2088a? This memory is referred to as DP DDR memory in the -boot code. Purpose of this memory is not entirely clear to me. Only reference I find is that this is intended to be used by the AIOP. Does this need to be populated even if we are not using AIOP interface?&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin: 0in 0in 0.0001pt; font-size: 12pt; color: #000000; text-indent: 0px;"&gt;&lt;/P&gt;&lt;P style="margin: 0in 0in 0.0001pt; font-size: 12pt; color: #000000; text-indent: 0px;"&gt;&lt;SPAN style="font-size: 11pt;"&gt;If there is a document that describes purpose and use of this DP DDR memory, can anyone please point me to it?&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin: 0in 0in 0.0001pt; font-size: 12pt; color: #000000; text-indent: 0px;"&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 06 Apr 2018 22:40:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/DP-DDR-memory-on-LS2088a/m-p/774758#M3402</guid>
      <dc:creator>sp_qoriq</dc:creator>
      <dc:date>2018-04-06T22:40:43Z</dc:date>
    </item>
    <item>
      <title>Re: DP DDR memory on LS2088a</title>
      <link>https://community.nxp.com/t5/Layerscape/DP-DDR-memory-on-LS2088a/m-p/774759#M3403</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you do not need for the AIOP then the LS2084A is better. It is like the LS2088A without the AIOP and 32-bit DDR controller. Unfortunately there is not public document which describes how the LS2088A DPAA2 hardware utilizes that DDR memory. Please consider creating a Technical Case to obtain additional information – for the required steps see &lt;/P&gt;&lt;P&gt;&lt;A data-containerid="2009" data-containertype="14" data-content-finding="Community" data-objectid="381898" data-objecttype="1" href="https://community.freescale.com/thread/381898"&gt;How I could create a Service Request?&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 10 Apr 2018 13:18:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/DP-DDR-memory-on-LS2088a/m-p/774759#M3403</guid>
      <dc:creator>r8070z</dc:creator>
      <dc:date>2018-04-10T13:18:50Z</dc:date>
    </item>
  </channel>
</rss>