<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic GPIO pins on LS1046ARDB in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/GPIO-pins-on-LS1046ARDB/m-p/760343#M3312</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Are there any GPIO pins available on the LS1046ARDB?&amp;nbsp;&lt;/P&gt;&lt;P&gt;I didn't find anything about it in the getting started guide or the reference manual.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I know, that the LS1046A comes with a GPIO module, but&amp;nbsp;there seems to be no pin available on the RDB connected to a GPIO port.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 24 Apr 2018 11:29:51 GMT</pubDate>
    <dc:creator>andreasr</dc:creator>
    <dc:date>2018-04-24T11:29:51Z</dc:date>
    <item>
      <title>GPIO pins on LS1046ARDB</title>
      <link>https://community.nxp.com/t5/Layerscape/GPIO-pins-on-LS1046ARDB/m-p/760343#M3312</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Are there any GPIO pins available on the LS1046ARDB?&amp;nbsp;&lt;/P&gt;&lt;P&gt;I didn't find anything about it in the getting started guide or the reference manual.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I know, that the LS1046A comes with a GPIO module, but&amp;nbsp;there seems to be no pin available on the RDB connected to a GPIO port.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 24 Apr 2018 11:29:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/GPIO-pins-on-LS1046ARDB/m-p/760343#M3312</guid>
      <dc:creator>andreasr</dc:creator>
      <dc:date>2018-04-24T11:29:51Z</dc:date>
    </item>
    <item>
      <title>Re: GPIO pins on LS1046ARDB</title>
      <link>https://community.nxp.com/t5/Layerscape/GPIO-pins-on-LS1046ARDB/m-p/760344#M3313</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12.0pt;"&gt;As I could see in the LS1046ARDB schematics there are not pins dedicated for GPIO. According to the LS1046A manual all pins used by the GPIO modules are shared with other peripheral controllers. The RDB uses most of those controllers. You may create technical case with request for the LS1046ARDB schematics and check if you can use some pins as GPIO for your case. Please see &lt;A _jive_internal="true" class="" data-containerid="2009" data-containertype="14" data-objectid="381898" data-objecttype="1" href="https://community.nxp.com/thread/381898"&gt;How I could create a Techical Case?&lt;/A&gt;&amp;nbsp;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Apr 2018 16:54:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/GPIO-pins-on-LS1046ARDB/m-p/760344#M3313</guid>
      <dc:creator>r8070z</dc:creator>
      <dc:date>2018-04-25T16:54:52Z</dc:date>
    </item>
  </channel>
</rss>