<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic FRDM-LS1012A USB3.0 Host in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/FRDM-LS1012A-USB3-0-Host/m-p/754849#M3278</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am testing USB 3.0 on a Freedom board and trying to get USB3.0 Super Speed to read a Flash Drive.&amp;nbsp; I've tried two different sticks and they both show up on the High Speed bus instead of the Super Speed bus.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1d6b:0003 (bus 2, device 1, speed 5000M)&lt;BR /&gt;0781:5581 (bus 1, device 3, speed 480M) path: 1 // FLASH DRIVE&lt;BR /&gt;1d6b:0002 (bus 1, device 1, speed 480M)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1d6b:0003 (bus 2, device 1, speed 5000M)&lt;BR /&gt;090c:1000 (bus 1, device 4, speed 480M) path: 1 // FLASH DRIVE&lt;BR /&gt;1d6b:0002 (bus 1, device 1, speed 480M)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The board is running the firmware the device shipped with.&amp;nbsp; Is there anything special that needs to be done to get USB 3.0 Super Speed working?&amp;nbsp; I would have expected the USB drive to show up on bus 2, perhaps this is an issue with OTG?&amp;nbsp; I read elsewhere that USB3.0 dosn't function if OTG is enabled but am not sure how to change that in the Linux.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 30 Dec 2017 07:52:24 GMT</pubDate>
    <dc:creator>michaelmarques</dc:creator>
    <dc:date>2017-12-30T07:52:24Z</dc:date>
    <item>
      <title>FRDM-LS1012A USB3.0 Host</title>
      <link>https://community.nxp.com/t5/Layerscape/FRDM-LS1012A-USB3-0-Host/m-p/754849#M3278</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am testing USB 3.0 on a Freedom board and trying to get USB3.0 Super Speed to read a Flash Drive.&amp;nbsp; I've tried two different sticks and they both show up on the High Speed bus instead of the Super Speed bus.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1d6b:0003 (bus 2, device 1, speed 5000M)&lt;BR /&gt;0781:5581 (bus 1, device 3, speed 480M) path: 1 // FLASH DRIVE&lt;BR /&gt;1d6b:0002 (bus 1, device 1, speed 480M)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1d6b:0003 (bus 2, device 1, speed 5000M)&lt;BR /&gt;090c:1000 (bus 1, device 4, speed 480M) path: 1 // FLASH DRIVE&lt;BR /&gt;1d6b:0002 (bus 1, device 1, speed 480M)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The board is running the firmware the device shipped with.&amp;nbsp; Is there anything special that needs to be done to get USB 3.0 Super Speed working?&amp;nbsp; I would have expected the USB drive to show up on bus 2, perhaps this is an issue with OTG?&amp;nbsp; I read elsewhere that USB3.0 dosn't function if OTG is enabled but am not sure how to change that in the Linux.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 30 Dec 2017 07:52:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/FRDM-LS1012A-USB3-0-Host/m-p/754849#M3278</guid>
      <dc:creator>michaelmarques</dc:creator>
      <dc:date>2017-12-30T07:52:24Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-LS1012A USB3.0 Host</title>
      <link>https://community.nxp.com/t5/Layerscape/FRDM-LS1012A-USB3-0-Host/m-p/1498292#M10964</link>
      <description>&lt;P&gt;Have you been able to solve this problem?&lt;/P&gt;</description>
      <pubDate>Sat, 30 Jul 2022 08:14:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/FRDM-LS1012A-USB3-0-Host/m-p/1498292#M10964</guid>
      <dc:creator>CedricBerger</dc:creator>
      <dc:date>2022-07-30T08:14:47Z</dc:date>
    </item>
  </channel>
</rss>