<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LayerscapeのトピックRe: LS1012 boot</title>
    <link>https://community.nxp.com/t5/Layerscape/LS1012-boot/m-p/749593#M3228</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Alexander,&lt;BR /&gt;sorry for the late reply, we managed to have three reworked board with new processors.&lt;BR /&gt;The cfg_eng_use and cfg_eng_use2 pins are tied to "11" with a pullup to select the external oscillator.&lt;BR /&gt;With these new processors we have a stable situation in wich pushing reset the board starts activity on SPI, but not at power on. Power supply sequences are from MC34VR5100A1EP, powered @ 3.7V.&lt;BR /&gt;Even maintainig pushed the reset button at power on and then releasing it the board doesn't boot, we need a full reset cycle to start activity on SPI.&lt;BR /&gt;Additionally, the time from the release of the reset to SPI activity is different from the one on the freedom board : on the freedom, when we release the reset button, activity starts within some 300 uSec., on our board there are more than 3 mSec. of delay.&lt;BR /&gt;Our suspect is we have a floating pin somewhere, but looking at the specs we can't find it, and everything is pulled up/down as per data sheet and application notes.&lt;BR /&gt;Do you know if someone have ever seen this behavior before?&lt;/P&gt;&lt;P&gt;Thank you and regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 22 Jun 2018 07:05:11 GMT</pubDate>
    <dc:creator>Filippo</dc:creator>
    <dc:date>2018-06-22T07:05:11Z</dc:date>
    <item>
      <title>LS1012 boot</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1012-boot/m-p/749589#M3224</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;BR /&gt;on a custom LS1012 board we are facing this issue : clocks and resets ( both the PORESET_B and TRST_B ) come from the same source and are fine, RCW source ( CLK_OUT ) is open / pulled up to 1.8V , QSPI_A_CS0 and QSPI_A_DATA1 are pulled down to 0 to select the external oscillator, but we can't see any activity on QSPI to load RCW.&lt;BR /&gt;Powers are within the ranges, JTAG is enabled with TCK pulled high with a 4.7k to 1.8V.&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;Anybody has hints about this?&lt;BR /&gt;We have not yet tried with JTAG, can this be of some help?&lt;BR /&gt;Thanks and regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Apr 2018 12:49:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1012-boot/m-p/749589#M3224</guid>
      <dc:creator>Filippo</dc:creator>
      <dc:date>2018-04-19T12:49:22Z</dc:date>
    </item>
    <item>
      <title>Re: LS1012 boot</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1012-boot/m-p/749590#M3225</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;It's difficult to say without seeing your schematics.&lt;/P&gt;&lt;P&gt;You could try to see in the oscilloscope the configuration signals (&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;QSPI_A_CS0&lt;SPAN&gt;&amp;nbsp;,&amp;nbsp;&lt;SPAN style="background-color: #ffffff;"&gt;QSPI_A_DATA1, CLK_OUT&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;) and EXTAL when PORESET_B goes up. Is the QSPI in reset in that moment? Has it clock?.&lt;/P&gt;&lt;P&gt;Maybe a fabrication problem: a signal not connected. You could test if you could see the protection diodes with a tester in configuration signals inputs and compare it with development board behaviour (the problem is that you also see the QSPI protection diodes in that signals).&lt;/P&gt;&lt;P&gt;Hope it helps.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Apr 2018 07:01:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1012-boot/m-p/749590#M3225</guid>
      <dc:creator>zmlopez</dc:creator>
      <dc:date>2018-04-20T07:01:05Z</dc:date>
    </item>
    <item>
      <title>Re: LS1012 boot</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1012-boot/m-p/749591#M3226</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Miguel,&lt;/P&gt;&lt;P&gt;sure, difficult...&lt;BR /&gt;Just to clarify : I have no QSPI connected, &lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;QSPI_A_CS0&lt;SPAN&gt; and &lt;SPAN style="background-color: #ffffff;"&gt;QSPI_A_DATA1 are pulled down with a 10K res, EXTAL is connected to a 1.8V clock source @ 25MHz and XTAL is connected to GND, but I can't see any clock to the QSPI nor chip select or other signals.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;&lt;SPAN style="background-color: #ffffff;"&gt;QSPI_A_DAT2 is pulled up with a 4.7K and&amp;nbsp;SDHC1_CD_B is pulled up with a 4.7K.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;We have the same behavior on 5 boards.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Apr 2018 07:25:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1012-boot/m-p/749591#M3226</guid>
      <dc:creator>Filippo</dc:creator>
      <dc:date>2018-04-20T07:25:43Z</dc:date>
    </item>
    <item>
      <title>Re: LS1012 boot</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1012-boot/m-p/749592#M3227</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;There is nothing mentioned about cfg_eng_use and cfg_eng_use2 pins. According to LS1012 Reference Manual, Section 4.4.4.2 "Transconductance selection control", these pins should be "11" for external oscillator. Note that internal weak pull-up may be not adequate, if there is any device connected to these pins.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Alexander&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 04 May 2018 14:09:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1012-boot/m-p/749592#M3227</guid>
      <dc:creator>alexander_yakov</dc:creator>
      <dc:date>2018-05-04T14:09:39Z</dc:date>
    </item>
    <item>
      <title>Re: LS1012 boot</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1012-boot/m-p/749593#M3228</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Alexander,&lt;BR /&gt;sorry for the late reply, we managed to have three reworked board with new processors.&lt;BR /&gt;The cfg_eng_use and cfg_eng_use2 pins are tied to "11" with a pullup to select the external oscillator.&lt;BR /&gt;With these new processors we have a stable situation in wich pushing reset the board starts activity on SPI, but not at power on. Power supply sequences are from MC34VR5100A1EP, powered @ 3.7V.&lt;BR /&gt;Even maintainig pushed the reset button at power on and then releasing it the board doesn't boot, we need a full reset cycle to start activity on SPI.&lt;BR /&gt;Additionally, the time from the release of the reset to SPI activity is different from the one on the freedom board : on the freedom, when we release the reset button, activity starts within some 300 uSec., on our board there are more than 3 mSec. of delay.&lt;BR /&gt;Our suspect is we have a floating pin somewhere, but looking at the specs we can't find it, and everything is pulled up/down as per data sheet and application notes.&lt;BR /&gt;Do you know if someone have ever seen this behavior before?&lt;/P&gt;&lt;P&gt;Thank you and regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 22 Jun 2018 07:05:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1012-boot/m-p/749593#M3228</guid>
      <dc:creator>Filippo</dc:creator>
      <dc:date>2018-06-22T07:05:11Z</dc:date>
    </item>
    <item>
      <title>Re: LS1012 boot</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1012-boot/m-p/749594#M3229</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Just a quick update : we worked to have exactly the same power scheme the freedom board has, so the MC34VR5100A1EP is powered from the same 3.3V that goes to the LS1012 EVDD pin ( 159 ). The difference we see is the freedom PMIC is a MC34VR5100A0EP but our is a MC34VR5100A1EP, indicating that sequences and voltages may be different ( maybe ? ). Reset in our board is some 600 mSec. ( specs says more than 300 mSec. ).&lt;BR /&gt;Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 22 Jun 2018 13:51:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1012-boot/m-p/749594#M3229</guid>
      <dc:creator>Filippo</dc:creator>
      <dc:date>2018-06-22T13:51:30Z</dc:date>
    </item>
  </channel>
</rss>