<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Question about boot error (&amp;quot;DIMM is not supported by this board&amp;quot;) of LS1046ARDB. in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/Question-about-boot-error-quot-DIMM-is-not-supported-by-this/m-p/738406#M3158</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV class=""&gt;&lt;P&gt;The described issue has to be thoroughly investigated and replicated on the LS1046ARDB locally.&lt;/P&gt;&lt;P&gt;To start the investigation it is required to collect additional information.&lt;/P&gt;&lt;P&gt;Most convenient way to perform aforesaid is by creating a Technical Case referring the following:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/381898"&gt;How I could create a Service Request?&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 13 Feb 2018 12:28:37 GMT</pubDate>
    <dc:creator>ufedor</dc:creator>
    <dc:date>2018-02-13T12:28:37Z</dc:date>
    <item>
      <title>Question about boot error ("DIMM is not supported by this board") of LS1046ARDB.</title>
      <link>https://community.nxp.com/t5/Layerscape/Question-about-boot-error-quot-DIMM-is-not-supported-by-this/m-p/738405#M3157</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;We used the following DDR 4 memory instead of DDR 4 memory (MTA18ASF1G72AZ-2G3B1ZG) on LS1046ARDB&lt;BR /&gt;&amp;nbsp; - CT4GDFS8213&lt;BR /&gt;&amp;nbsp; - TS512MLH64V1H&lt;/P&gt;&lt;P&gt;When using these DDR4 memories, we will see the "DIMM is not supported by this board" message.&lt;/P&gt;&lt;P&gt;====&amp;nbsp; LS1046ARM&amp;nbsp; ====&lt;BR /&gt;1.4.3 DDR memory controller&lt;BR /&gt;The chip offers one 32/64-bit DDR controller supporting ECC protected memories. The&lt;BR /&gt;32/64-bit DDR4 controller operates at up to 2.1 GT/s. Some key DDR controller features&lt;BR /&gt;are as follows:&lt;BR /&gt;=====================&lt;BR /&gt;If not satisfying the above, I guess that this error message will be output.&lt;BR /&gt;However, we think that these DDR4 memories satisfy this spec.&lt;/P&gt;&lt;P&gt;Could you advise us the cause of this error message?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Best Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 13 Feb 2018 11:23:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Question-about-boot-error-quot-DIMM-is-not-supported-by-this/m-p/738405#M3157</guid>
      <dc:creator>kazuyayamauchi</dc:creator>
      <dc:date>2018-02-13T11:23:16Z</dc:date>
    </item>
    <item>
      <title>Re: Question about boot error ("DIMM is not supported by this board") of LS1046ARDB.</title>
      <link>https://community.nxp.com/t5/Layerscape/Question-about-boot-error-quot-DIMM-is-not-supported-by-this/m-p/738406#M3158</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV class=""&gt;&lt;P&gt;The described issue has to be thoroughly investigated and replicated on the LS1046ARDB locally.&lt;/P&gt;&lt;P&gt;To start the investigation it is required to collect additional information.&lt;/P&gt;&lt;P&gt;Most convenient way to perform aforesaid is by creating a Technical Case referring the following:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/381898"&gt;How I could create a Service Request?&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 13 Feb 2018 12:28:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Question-about-boot-error-quot-DIMM-is-not-supported-by-this/m-p/738406#M3158</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2018-02-13T12:28:37Z</dc:date>
    </item>
  </channel>
</rss>