<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic LS1021 Suspend to ram under linux possible? in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/LS1021-Suspend-to-ram-under-linux-possible/m-p/422135#M313</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would like to know if it is possible to suspend to ram on the LS1021.&lt;/P&gt;&lt;P&gt;Also is frequency scaling possible?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Dennis&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 23 Jun 2015 05:55:47 GMT</pubDate>
    <dc:creator>dwokke</dc:creator>
    <dc:date>2015-06-23T05:55:47Z</dc:date>
    <item>
      <title>LS1021 Suspend to ram under linux possible?</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1021-Suspend-to-ram-under-linux-possible/m-p/422135#M313</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would like to know if it is possible to suspend to ram on the LS1021.&lt;/P&gt;&lt;P&gt;Also is frequency scaling possible?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Dennis&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 23 Jun 2015 05:55:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1021-Suspend-to-ram-under-linux-possible/m-p/422135#M313</guid>
      <dc:creator>dwokke</dc:creator>
      <dc:date>2015-06-23T05:55:47Z</dc:date>
    </item>
    <item>
      <title>Re: LS1021 Suspend to ram under linux possible?</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1021-Suspend-to-ram-under-linux-possible/m-p/422136#M314</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Dennis Wokke,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For your question about suspend to ram and frequency scaling on LS1021A, QorIQ-SDK-1.7 give below highlights in Section 1.3 What's new:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/57912i2CBBBF66DF33BECC/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;This pdf is available at:&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.freescale.com/files/soft_dev_tools/doc/support_info/QorIQ-SDK-1.7-IC-RevB.zip" title="http://www.freescale.com/files/soft_dev_tools/doc/support_info/QorIQ-SDK-1.7-IC-RevB.zip"&gt;http://www.freescale.com/files/soft_dev_tools/doc/support_info/QorIQ-SDK-1.7-IC-RevB.zip&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Lunmin&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 25 Jun 2015 09:27:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1021-Suspend-to-ram-under-linux-possible/m-p/422136#M314</guid>
      <dc:creator>lunminliang</dc:creator>
      <dc:date>2015-06-25T09:27:02Z</dc:date>
    </item>
    <item>
      <title>Re: LS1021 Suspend to ram under linux possible?</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1021-Suspend-to-ram-under-linux-possible/m-p/422137#M315</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Lunmin,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Maybe I should have been more clear on my objective.&lt;/P&gt;&lt;P&gt;I have the TWR-LS1021a board. In the documentation I have read that it will not do deep-sleep mode.&lt;/P&gt;&lt;P&gt;Also I read there was a silicon issue regarding power mangement, however I am unable to find the reference to this.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I want to use the LS1021a for un upcoming project, but can only use it if I am 100% certain I can get low power while the system is idle. It should go into deep sleep mode a lt of the time to preserve battery power. As I cannot test this on the TWR-LS1021a I'm at a loss.&lt;/P&gt;&lt;P&gt;Maybe you can give me some certainty about this.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I must say I had not seen the Rev B yet, and that looks promising.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Dennis&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 25 Jun 2015 13:19:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1021-Suspend-to-ram-under-linux-possible/m-p/422137#M315</guid>
      <dc:creator>dwokke</dc:creator>
      <dc:date>2015-06-25T13:19:39Z</dc:date>
    </item>
  </channel>
</rss>