<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Layerscape中的主题 PCIE Endpoint DMA to host</title>
    <link>https://community.nxp.com/t5/Layerscape/PCIE-Endpoint-DMA-to-host/m-p/722446#M3005</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are planning on using a LS1088A-based system as a PCIe endpoint to a desktop/server host.&amp;nbsp; Is there a DMA module in LS1088A that can be used for endpoint-initiated DMA data access through PCIe bus?&amp;nbsp; If possible it should also be capable of burst transfers.&amp;nbsp; I'm checking on qDMA but it seems it is more on networking purposes, while we will not be using it and will be heavily relying on PCIe for data transfers.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If not, what can we use instead that is from NXP?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 11 Apr 2018 09:15:53 GMT</pubDate>
    <dc:creator>aabitria</dc:creator>
    <dc:date>2018-04-11T09:15:53Z</dc:date>
    <item>
      <title>PCIE Endpoint DMA to host</title>
      <link>https://community.nxp.com/t5/Layerscape/PCIE-Endpoint-DMA-to-host/m-p/722446#M3005</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are planning on using a LS1088A-based system as a PCIe endpoint to a desktop/server host.&amp;nbsp; Is there a DMA module in LS1088A that can be used for endpoint-initiated DMA data access through PCIe bus?&amp;nbsp; If possible it should also be capable of burst transfers.&amp;nbsp; I'm checking on qDMA but it seems it is more on networking purposes, while we will not be using it and will be heavily relying on PCIe for data transfers.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If not, what can we use instead that is from NXP?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Apr 2018 09:15:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/PCIE-Endpoint-DMA-to-host/m-p/722446#M3005</guid>
      <dc:creator>aabitria</dc:creator>
      <dc:date>2018-04-11T09:15:53Z</dc:date>
    </item>
    <item>
      <title>Re: PCIE Endpoint DMA to host</title>
      <link>https://community.nxp.com/t5/Layerscape/PCIE-Endpoint-DMA-to-host/m-p/722447#M3006</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The qDMA is universal DMA engine of&amp;nbsp; LS1088A which can perform DMA transfers from memory to memory. So it can transfer data in-between local memory of a LS1088A based PCIe endpoint and a desktop/server host (PCIe Root Complex). Some LS1088A peripherals also have DMA to transfer data in-between peripheral and memory. May be it will be right for you if you need to transfer data from the LS1088A peripheral(s) to the host. Notice there are LS1043A and LS1046A devices in the QorIQ family which have eDMA with relatively simple program model.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Apr 2018 11:21:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/PCIE-Endpoint-DMA-to-host/m-p/722447#M3006</guid>
      <dc:creator>r8070z</dc:creator>
      <dc:date>2018-04-12T11:21:20Z</dc:date>
    </item>
    <item>
      <title>Re: PCIE Endpoint DMA to host</title>
      <link>https://community.nxp.com/t5/Layerscape/PCIE-Endpoint-DMA-to-host/m-p/722448#M3007</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for the reply.&amp;nbsp; Where can I find further info on LS1088A qDMA like its reference manual or how to utilize it (for baremetal purposes)?&amp;nbsp; I've looked for and checked for it in LS1088ARM, LS1088ASECRM, and DPAA2 (Data Path DMA?) User Manuals but those documents just mentioned qDMA in passing and and were not really helpful.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does LS1088A have a qDMA similar to that of LS1046A?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Apr 2018 12:21:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/PCIE-Endpoint-DMA-to-host/m-p/722448#M3007</guid>
      <dc:creator>aabitria</dc:creator>
      <dc:date>2018-04-12T12:21:29Z</dc:date>
    </item>
    <item>
      <title>Re: PCIE Endpoint DMA to host</title>
      <link>https://community.nxp.com/t5/Layerscape/PCIE-Endpoint-DMA-to-host/m-p/722449#M3008</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I saw LS1088A qDMA in document named “LS1088A Family DPAA2 Low-Level Hardware Reference Manual” which is in preliminary state. Due to that it is not public. As I can see there is a noticeable difference between LS1046A qDMA and LS1088A qDMA.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 13 Apr 2018 03:52:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/PCIE-Endpoint-DMA-to-host/m-p/722449#M3008</guid>
      <dc:creator>r8070z</dc:creator>
      <dc:date>2018-04-13T03:52:34Z</dc:date>
    </item>
    <item>
      <title>Re: PCIE Endpoint DMA to host</title>
      <link>https://community.nxp.com/t5/Layerscape/PCIE-Endpoint-DMA-to-host/m-p/722450#M3009</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I see.&amp;nbsp; I'd be interested to see that document if it details how to use the LS1088A qDMA in a generic way (independent of the networking function) as that of LS1046A.&amp;nbsp; Will that be released soon?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 13 Apr 2018 11:51:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/PCIE-Endpoint-DMA-to-host/m-p/722450#M3009</guid>
      <dc:creator>aabitria</dc:creator>
      <dc:date>2018-04-13T11:51:08Z</dc:date>
    </item>
  </channel>
</rss>