<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic QuadSPI_SR: BUSY bit stuck  in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/QuadSPI-SR-BUSY-bit-stuck/m-p/722176#M3004</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, i'm using a ls1046a with n25q128a nor flash.&lt;BR /&gt;U-Boot is able to erase, read and write small data but if I try it with more data, get timeout:&lt;BR /&gt;&amp;lt;p&amp;gt;&lt;BR /&gt;fsl_qspi_claim_bus: Timeout (reg=000000000155015c mask=00000007 wait_set=0)&lt;BR /&gt;ERROR : The controller is busy &lt;BR /&gt;SF: 639916 bytes @ 0x10000 Written: ERROR -110&lt;BR /&gt;&amp;lt;/p&amp;gt;&lt;/P&gt;&lt;P&gt;As you can see, I stuck in the function fsl_qspi_claim_bus. The register QuadSPI_SR has the value: 0x00380001&lt;BR /&gt;The busy bit is set and also the RXFULL bit is set. RXFULL bit description in in the datasheet:&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;SPAN&gt;RX Buffer Full. Asserted when the RX Buffer is full, i.e. that QSPI_RBSR[RDBFL] field is equal to 32.&lt;/SPAN&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;But in my case, the&amp;nbsp;QSPI_RBSR register is 0x00000000&lt;BR /&gt;Has any one an idea, what's going wrong?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 01 Mar 2018 11:37:45 GMT</pubDate>
    <dc:creator>volkerhaspel</dc:creator>
    <dc:date>2018-03-01T11:37:45Z</dc:date>
    <item>
      <title>QuadSPI_SR: BUSY bit stuck</title>
      <link>https://community.nxp.com/t5/Layerscape/QuadSPI-SR-BUSY-bit-stuck/m-p/722176#M3004</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, i'm using a ls1046a with n25q128a nor flash.&lt;BR /&gt;U-Boot is able to erase, read and write small data but if I try it with more data, get timeout:&lt;BR /&gt;&amp;lt;p&amp;gt;&lt;BR /&gt;fsl_qspi_claim_bus: Timeout (reg=000000000155015c mask=00000007 wait_set=0)&lt;BR /&gt;ERROR : The controller is busy &lt;BR /&gt;SF: 639916 bytes @ 0x10000 Written: ERROR -110&lt;BR /&gt;&amp;lt;/p&amp;gt;&lt;/P&gt;&lt;P&gt;As you can see, I stuck in the function fsl_qspi_claim_bus. The register QuadSPI_SR has the value: 0x00380001&lt;BR /&gt;The busy bit is set and also the RXFULL bit is set. RXFULL bit description in in the datasheet:&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;SPAN&gt;RX Buffer Full. Asserted when the RX Buffer is full, i.e. that QSPI_RBSR[RDBFL] field is equal to 32.&lt;/SPAN&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;But in my case, the&amp;nbsp;QSPI_RBSR register is 0x00000000&lt;BR /&gt;Has any one an idea, what's going wrong?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 01 Mar 2018 11:37:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/QuadSPI-SR-BUSY-bit-stuck/m-p/722176#M3004</guid>
      <dc:creator>volkerhaspel</dc:creator>
      <dc:date>2018-03-01T11:37:45Z</dc:date>
    </item>
  </channel>
</rss>