<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LayerscapeのトピックRe: Configuring OpenOCD to work with LS1043a-RDB</title>
    <link>https://community.nxp.com/t5/Layerscape/Configuring-OpenOCD-to-work-with-LS1043a-RDB/m-p/719241#M2973</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;A _jive_internal="true" data-content-finding="Community" data-userid="315628" data-username="forestgodfrey" href="https://community.nxp.com/people/forestgodfrey"&gt;Forest Godfrey&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We only provide CodeWarrior debugging solution for LS1043ARDB, which is also use gdb as the debugger.&lt;/P&gt;&lt;P&gt;You could refer to the document &lt;A href="https://community.nxp.com/docs/DOC-331981"&gt;Use CodeWarrior for ARMv8 to Debug U-boot and Linux Kernel and Bring up Bare Boards&lt;/A&gt; for how to debug Linux Kernel with CodeWarrior, you could install the evaluation version CodeWarrior and refer to configuration scripts provided in CodeWarrior.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 06 May 2018 10:39:40 GMT</pubDate>
    <dc:creator>yipingwang</dc:creator>
    <dc:date>2018-05-06T10:39:40Z</dc:date>
    <item>
      <title>Configuring OpenOCD to work with LS1043a-RDB</title>
      <link>https://community.nxp.com/t5/Layerscape/Configuring-OpenOCD-to-work-with-LS1043a-RDB/m-p/719240#M2972</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am attempting to use OpenOCD and gdb to debug the kernel on the LS1043a-RDB.&amp;nbsp; I've seen references to a version of it packaged with Eclipse that would do this, but I haven't been able to figure out how to download that.&amp;nbsp; Also, we don't use Eclipse in our environment so all I really need out of that are the various target and chip configuration scripts.&amp;nbsp; Has anyone gotten this working?&amp;nbsp; I build the master branch of OpenOCD with CMSIS-DAP support and it sees the LS1043 with two tap's (a Freescale tap and an ARM tap).&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 20 Mar 2018 18:27:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Configuring-OpenOCD-to-work-with-LS1043a-RDB/m-p/719240#M2972</guid>
      <dc:creator>forestgodfrey</dc:creator>
      <dc:date>2018-03-20T18:27:17Z</dc:date>
    </item>
    <item>
      <title>Re: Configuring OpenOCD to work with LS1043a-RDB</title>
      <link>https://community.nxp.com/t5/Layerscape/Configuring-OpenOCD-to-work-with-LS1043a-RDB/m-p/719241#M2973</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;A _jive_internal="true" data-content-finding="Community" data-userid="315628" data-username="forestgodfrey" href="https://community.nxp.com/people/forestgodfrey"&gt;Forest Godfrey&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We only provide CodeWarrior debugging solution for LS1043ARDB, which is also use gdb as the debugger.&lt;/P&gt;&lt;P&gt;You could refer to the document &lt;A href="https://community.nxp.com/docs/DOC-331981"&gt;Use CodeWarrior for ARMv8 to Debug U-boot and Linux Kernel and Bring up Bare Boards&lt;/A&gt; for how to debug Linux Kernel with CodeWarrior, you could install the evaluation version CodeWarrior and refer to configuration scripts provided in CodeWarrior.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 06 May 2018 10:39:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Configuring-OpenOCD-to-work-with-LS1043a-RDB/m-p/719241#M2973</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2018-05-06T10:39:40Z</dc:date>
    </item>
  </channel>
</rss>