<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Layerscape中的主题 Re: Programming U-Boot to SD card</title>
    <link>https://community.nxp.com/t5/Layerscape/Programming-U-Boot-to-SD-card/m-p/415036#M283</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Adrian,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for the help.&amp;nbsp; With those commands I am able to build u-boot with spl.&amp;nbsp; However, after writing the new binary image to the SD card, I am unable to see any console prompt from u-boot.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;These are the steps I have done so far:&lt;/P&gt;&lt;P&gt;Edit meta-fsl-arm/conf/machine/ls1021atwr.conf to use UBOOT_CONFIG ??= "sdcard"&lt;/P&gt;&lt;P&gt;$ cd build_ls1021atwr_release/&lt;/P&gt;&lt;P&gt;$ bitbake -c cleansstate u-boot&lt;/P&gt;&lt;P&gt;$ bitbake -c patch u-boot&lt;/P&gt;&lt;P&gt;$ bitbake -c compile -f u-boot&lt;/P&gt;&lt;P&gt;$ cd tmp/work/ls1021atwr-fsl-linux-gnueabi/u-boot-ls1/2014.07-r0/git/&lt;/P&gt;&lt;P&gt;$ sudo dd if=u-boot.bin of=/dev/sdN bs=512 seek=8 &amp;amp;&amp;amp; sync&lt;/P&gt;&lt;P&gt;$ umount /dev/sdN1&lt;/P&gt;&lt;P&gt;The DIP switch SW2 is set to 00101111 and SW3 is 01100001.&amp;nbsp; J19/J20 are both shorted to 2:3.&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Doing a hexdump of u-boot.bin shows the eSDHC preable word AA 55 AA 55 at address 0x1000 (LSA1021A Reference Manual rev E pgs 252 &amp;amp; 266).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;This discussion (&lt;/SPAN&gt;&lt;A class="jive-link-thread-small" data-containerid="2009" data-containertype="14" data-objectid="371771" data-objecttype="1" href="https://community.freescale.com/thread/371771"&gt;https://community.freescale.com/thread/371771&lt;/A&gt;&lt;SPAN&gt;) has attached a working u-boot_prebuilt.bin. After extracting and running through the same steps as above, I &lt;/SPAN&gt;&lt;STRONG&gt;was&lt;/STRONG&gt; able to get a u-boot prompt.&amp;nbsp; So that confirms that my switches are in the correct position and u-boot is getting written to the card.&amp;nbsp; I suspect that my u-boot.bin is still not being built correctly.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Are there any other steps required to make u-boot boot on SD?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Josh&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 29 Oct 2015 20:51:30 GMT</pubDate>
    <dc:creator>joshkurland</dc:creator>
    <dc:date>2015-10-29T20:51:30Z</dc:date>
    <item>
      <title>Programming U-Boot to SD card</title>
      <link>https://community.nxp.com/t5/Layerscape/Programming-U-Boot-to-SD-card/m-p/415025#M272</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We use QorIQ_SDK_LS1021A_0.4 SDK for LS1021A processor.&lt;/P&gt;&lt;P&gt;I would like to ask :&lt;/P&gt;&lt;P&gt;Where is the u-boot-with-spl-pbl.bin file mentioned in the Freescale Linux LS1021A SDK v0.4, Rev. A, Jul 2015 manual (page 73)&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Victor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 20 Oct 2015 21:13:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Programming-U-Boot-to-SD-card/m-p/415025#M272</guid>
      <dc:creator>victormazin</dc:creator>
      <dc:date>2015-10-20T21:13:55Z</dc:date>
    </item>
    <item>
      <title>Re: Programming U-Boot to SD card</title>
      <link>https://community.nxp.com/t5/Layerscape/Programming-U-Boot-to-SD-card/m-p/415026#M273</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Victor Mazin,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is a similar question on the target previously, please check if help:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/377390"&gt;how do i get u-boot-with-spl-pbl.bin?&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Lunmin&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Oct 2015 05:46:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Programming-U-Boot-to-SD-card/m-p/415026#M273</guid>
      <dc:creator>lunminliang</dc:creator>
      <dc:date>2015-10-21T05:46:23Z</dc:date>
    </item>
    <item>
      <title>Re: Programming U-Boot to SD card</title>
      <link>https://community.nxp.com/t5/Layerscape/Programming-U-Boot-to-SD-card/m-p/415027#M274</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif;"&gt;After U-Boot sdcard build complete, u-boot-with-spl-pbl.bin should be available in \Freescale-Linux-SDK-for-LS1021A-Rev2-v0.4-20150803-yocto\build_ls1021atwr_release\tmp\work\ls1021atwr-fsl-linux-gnueabi\u-boot-ls1\2014.07-r0\git\spl\&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif;"&gt;Adrian&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Oct 2015 05:47:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Programming-U-Boot-to-SD-card/m-p/415027#M274</guid>
      <dc:creator>addiyi</dc:creator>
      <dc:date>2015-10-21T05:47:00Z</dc:date>
    </item>
    <item>
      <title>Re: Programming U-Boot to SD card</title>
      <link>https://community.nxp.com/t5/Layerscape/Programming-U-Boot-to-SD-card/m-p/415028#M275</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HI Adrian,&lt;/P&gt;&lt;P&gt;Thank you for your answer.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I did not find the &lt;SPAN style="color: #51626f; font-family: Arial;"&gt;u-boot-with-spl-pbl.bin file because the &lt;/SPAN&gt;&lt;SPAN style="color: #51626f; font-family: Arial;"&gt;\Freescale-Linux-SDK-for-LS1021A-Rev2-v0.4-20150803-yocto\build_ls1021atwr_release\tmp\work\ls1021atwr-fsl-linux-gnueabi\u-boot-ls1\2014.07-r0\git folder does&amp;nbsp; not content the spl directory on my computer. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; font-family: Arial;"&gt;Could you give more explanation what "U-boot sdcard build" is?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Victor &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Oct 2015 13:38:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Programming-U-Boot-to-SD-card/m-p/415028#M275</guid>
      <dc:creator>victormazin</dc:creator>
      <dc:date>2015-10-21T13:38:00Z</dc:date>
    </item>
    <item>
      <title>Re: Programming U-Boot to SD card</title>
      <link>https://community.nxp.com/t5/Layerscape/Programming-U-Boot-to-SD-card/m-p/415029#M276</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Did you select sdcard for UBOOT_CONFIG in ls1021atwr.conf (\Freescale-Linux-SDK-for-LS1021A-Rev2-v0.4-20150803-yocto\meta-fsl-arm\conf\machine\)?&lt;/P&gt;&lt;P&gt;Using UBOOT_CONFIG ??= "sdcard", uboot will be build for sdcard and spl folder will be available in uboot folder.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Adrian&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Oct 2015 14:09:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Programming-U-Boot-to-SD-card/m-p/415029#M276</guid>
      <dc:creator>addiyi</dc:creator>
      <dc:date>2015-10-21T14:09:00Z</dc:date>
    </item>
    <item>
      <title>Re: Programming U-Boot to SD card</title>
      <link>https://community.nxp.com/t5/Layerscape/Programming-U-Boot-to-SD-card/m-p/415030#M277</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Lunmin,&lt;/P&gt;&lt;P&gt;Thank&amp;nbsp; you for your answer.&amp;nbsp; I followed your recommendation from the previous discussion:&lt;/P&gt;&lt;P&gt;1. Change the config in /meta-fsl-arm/conf/machine/ls1021atwr.conf&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; “ UBOOT_CONFIG ??= "sdcard"&lt;/P&gt;&lt;P&gt;2. $bitbake u-boot -c cleansstate&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; $bitbake u-boot&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However I did not received the expected file (u-boot-with-spl-pbl.bin). I received the files:&lt;/P&gt;&lt;P&gt;u-boot-spl&lt;/P&gt;&lt;P&gt;u-boot-spl.bin&lt;/P&gt;&lt;P&gt;u-boot-spl.pbl&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Which file from this list should I use to program my SD card?&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Victor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Oct 2015 15:00:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Programming-U-Boot-to-SD-card/m-p/415030#M277</guid>
      <dc:creator>victormazin</dc:creator>
      <dc:date>2015-10-21T15:00:25Z</dc:date>
    </item>
    <item>
      <title>Re: Programming U-Boot to SD card</title>
      <link>https://community.nxp.com/t5/Layerscape/Programming-U-Boot-to-SD-card/m-p/415031#M278</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, I changed the config file. After that I was able to find the SPL directory.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However I did not received the expected file (u-boot-with-spl-pbl.bin). I received the files:&lt;/P&gt;&lt;P&gt;u-boot-spl&lt;/P&gt;&lt;P&gt;u-boot-spl.bin&lt;/P&gt;&lt;P&gt;u-boot-spl.pbl&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Which file from this list should I use to program my SD card?&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Victor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Oct 2015 15:25:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Programming-U-Boot-to-SD-card/m-p/415031#M278</guid>
      <dc:creator>victormazin</dc:creator>
      <dc:date>2015-10-21T15:25:33Z</dc:date>
    </item>
    <item>
      <title>Re: Programming U-Boot to SD card</title>
      <link>https://community.nxp.com/t5/Layerscape/Programming-U-Boot-to-SD-card/m-p/415032#M279</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The binary for programming into sd card is u-boot.bin (\build_ls1021atwr_release\tmp\work\ls1021atwr-fsl-linux-gnueabi\u-boot-ls1\2014.07-r0\git\). you can open it in a hex editor and you will see that this binary contains rcw+pbi+uboot. Also, in this folder you can find the elf file, in case you need to debug u-boot.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In spl folder, you can find the spl elf file in case you need to debug u-boot secondary program loader. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Adrian&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 Oct 2015 06:31:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Programming-U-Boot-to-SD-card/m-p/415032#M279</guid>
      <dc:creator>addiyi</dc:creator>
      <dc:date>2015-10-22T06:31:44Z</dc:date>
    </item>
    <item>
      <title>Re: Programming U-Boot to SD card</title>
      <link>https://community.nxp.com/t5/Layerscape/Programming-U-Boot-to-SD-card/m-p/415033#M280</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you Adrian,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Victor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 Oct 2015 14:59:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Programming-U-Boot-to-SD-card/m-p/415033#M280</guid>
      <dc:creator>victormazin</dc:creator>
      <dc:date>2015-10-22T14:59:31Z</dc:date>
    </item>
    <item>
      <title>Re: Programming U-Boot to SD card</title>
      <link>https://community.nxp.com/t5/Layerscape/Programming-U-Boot-to-SD-card/m-p/415034#M281</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I am also having trouble getting &lt;SPAN style="color: #51626f; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif;"&gt;u-boot-with-spl-pbl.bin.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif;"&gt;I edited meta-fsl-arm/conf/machine/ls1021atwr.conf to use UBOOT_CONFIG ??= "sdcard".&amp;nbsp; I then ran bitbake u-boot -c cleansstate and bitbake u-boot with no errors.&amp;nbsp; However the folder tmp/work/ls1021atwr-fsl-linux-gnueabi/u-boot-ls1/2014.07-r0/git is still empty. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif;"&gt;Are there any other steps necessary to make &lt;SPAN style="color: #51626f; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif;"&gt;u-boot-with-spl-pbl.bin?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif;"&gt;Thank you,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif;"&gt;Josh&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 28 Oct 2015 14:57:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Programming-U-Boot-to-SD-card/m-p/415034#M281</guid>
      <dc:creator>joshkurland</dc:creator>
      <dc:date>2015-10-28T14:57:29Z</dc:date>
    </item>
    <item>
      <title>Re: Programming U-Boot to SD card</title>
      <link>https://community.nxp.com/t5/Layerscape/Programming-U-Boot-to-SD-card/m-p/415035#M282</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Josh,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Try the following steps:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;bitbake -c cleansstate u-boot&lt;/P&gt;&lt;P&gt;bitbake -c patch u-boot&lt;/P&gt;&lt;P&gt;bitbake -c compile -f u-boot&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Adrian&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Oct 2015 07:32:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Programming-U-Boot-to-SD-card/m-p/415035#M282</guid>
      <dc:creator>addiyi</dc:creator>
      <dc:date>2015-10-29T07:32:44Z</dc:date>
    </item>
    <item>
      <title>Re: Programming U-Boot to SD card</title>
      <link>https://community.nxp.com/t5/Layerscape/Programming-U-Boot-to-SD-card/m-p/415036#M283</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Adrian,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for the help.&amp;nbsp; With those commands I am able to build u-boot with spl.&amp;nbsp; However, after writing the new binary image to the SD card, I am unable to see any console prompt from u-boot.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;These are the steps I have done so far:&lt;/P&gt;&lt;P&gt;Edit meta-fsl-arm/conf/machine/ls1021atwr.conf to use UBOOT_CONFIG ??= "sdcard"&lt;/P&gt;&lt;P&gt;$ cd build_ls1021atwr_release/&lt;/P&gt;&lt;P&gt;$ bitbake -c cleansstate u-boot&lt;/P&gt;&lt;P&gt;$ bitbake -c patch u-boot&lt;/P&gt;&lt;P&gt;$ bitbake -c compile -f u-boot&lt;/P&gt;&lt;P&gt;$ cd tmp/work/ls1021atwr-fsl-linux-gnueabi/u-boot-ls1/2014.07-r0/git/&lt;/P&gt;&lt;P&gt;$ sudo dd if=u-boot.bin of=/dev/sdN bs=512 seek=8 &amp;amp;&amp;amp; sync&lt;/P&gt;&lt;P&gt;$ umount /dev/sdN1&lt;/P&gt;&lt;P&gt;The DIP switch SW2 is set to 00101111 and SW3 is 01100001.&amp;nbsp; J19/J20 are both shorted to 2:3.&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Doing a hexdump of u-boot.bin shows the eSDHC preable word AA 55 AA 55 at address 0x1000 (LSA1021A Reference Manual rev E pgs 252 &amp;amp; 266).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;This discussion (&lt;/SPAN&gt;&lt;A class="jive-link-thread-small" data-containerid="2009" data-containertype="14" data-objectid="371771" data-objecttype="1" href="https://community.freescale.com/thread/371771"&gt;https://community.freescale.com/thread/371771&lt;/A&gt;&lt;SPAN&gt;) has attached a working u-boot_prebuilt.bin. After extracting and running through the same steps as above, I &lt;/SPAN&gt;&lt;STRONG&gt;was&lt;/STRONG&gt; able to get a u-boot prompt.&amp;nbsp; So that confirms that my switches are in the correct position and u-boot is getting written to the card.&amp;nbsp; I suspect that my u-boot.bin is still not being built correctly.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Are there any other steps required to make u-boot boot on SD?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Josh&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Oct 2015 20:51:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Programming-U-Boot-to-SD-card/m-p/415036#M283</guid>
      <dc:creator>joshkurland</dc:creator>
      <dc:date>2015-10-29T20:51:30Z</dc:date>
    </item>
    <item>
      <title>Re: Programming U-Boot to SD card</title>
      <link>https://community.nxp.com/t5/Layerscape/Programming-U-Boot-to-SD-card/m-p/415037#M284</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Josh,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could you provide info about the SDK version you are using and CPU revision?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Adrian&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 30 Oct 2015 06:39:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Programming-U-Boot-to-SD-card/m-p/415037#M284</guid>
      <dc:creator>addiyi</dc:creator>
      <dc:date>2015-10-30T06:39:53Z</dc:date>
    </item>
    <item>
      <title>Re: Programming U-Boot to SD card</title>
      <link>https://community.nxp.com/t5/Layerscape/Programming-U-Boot-to-SD-card/m-p/415038#M285</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Adrian,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;From your suggestion, I re-downloaded the QorIQ SDK v1.8 SOURCE SDK from Freescale's website and rebuilt u-boot following the previous steps.&amp;nbsp; This time I had no problems.&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you very much for the help,&lt;/P&gt;&lt;P&gt;Josh&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 30 Oct 2015 16:04:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Programming-U-Boot-to-SD-card/m-p/415038#M285</guid>
      <dc:creator>joshkurland</dc:creator>
      <dc:date>2015-10-30T16:04:48Z</dc:date>
    </item>
  </channel>
</rss>