<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LayerscapeのトピックRe: DDR3L bit swapping with LS1012A processor within byte</title>
    <link>https://community.nxp.com/t5/Layerscape/DDR3L-bit-swapping-with-LS1012A-processor-within-byte/m-p/680901#M2628</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It is possible to swap bits within a byte lane.&lt;/P&gt;&lt;P&gt;Please refer to the AN3940, Table 1. DDR3 Designer Checklist, 45:&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/webapp/Download?colCode=AN3940&amp;amp;location=null&amp;amp;fsrch=1&amp;amp;sr=9&amp;amp;pageNum=2&amp;amp;Parent_nodeId=&amp;amp;Parent_pageType=" title="https://www.nxp.com/webapp/Download?colCode=AN3940&amp;amp;location=null&amp;amp;fsrch=1&amp;amp;sr=9&amp;amp;pageNum=2&amp;amp;Parent_nodeId=&amp;amp;Parent_pageType="&gt;https://www.nxp.com/webapp/Download?colCode=AN3940&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Note that the MMDC supports only x16 data bus width.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 24 Jul 2017 13:48:12 GMT</pubDate>
    <dc:creator>ufedor</dc:creator>
    <dc:date>2017-07-24T13:48:12Z</dc:date>
    <item>
      <title>DDR3L bit swapping with LS1012A processor within byte</title>
      <link>https://community.nxp.com/t5/Layerscape/DDR3L-bit-swapping-with-LS1012A-processor-within-byte/m-p/680900#M2627</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am designing custom board using &lt;STRONG&gt;LS1012A processor&lt;/STRONG&gt; and interface with two 1Gx8 DDR3L micron DDR3L chip. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;During layout, I am facing issue of &lt;STRONG&gt;routing of data lines&lt;/STRONG&gt; so that as per&lt;STRONG&gt; AN3940&lt;/STRONG&gt; (Hardware and Layout Design &lt;BR /&gt;Considerations for DDR3 SDRAM Memory Interfaces) &lt;STRONG&gt;I have swapped the datalines in D0 to D7 at first DDR3L end&lt;/STRONG&gt;.&lt;/P&gt;&lt;P&gt;Also, attached swapped connections of first DDR3L with Processor.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So, will it work for me? because I can't see any information or guide to change this bits from firmware configuration level and confusion on the connections.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Looking for your help.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 24 Jul 2017 10:48:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/DDR3L-bit-swapping-with-LS1012A-processor-within-byte/m-p/680900#M2627</guid>
      <dc:creator>nilavchoksi</dc:creator>
      <dc:date>2017-07-24T10:48:56Z</dc:date>
    </item>
    <item>
      <title>Re: DDR3L bit swapping with LS1012A processor within byte</title>
      <link>https://community.nxp.com/t5/Layerscape/DDR3L-bit-swapping-with-LS1012A-processor-within-byte/m-p/680901#M2628</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It is possible to swap bits within a byte lane.&lt;/P&gt;&lt;P&gt;Please refer to the AN3940, Table 1. DDR3 Designer Checklist, 45:&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/webapp/Download?colCode=AN3940&amp;amp;location=null&amp;amp;fsrch=1&amp;amp;sr=9&amp;amp;pageNum=2&amp;amp;Parent_nodeId=&amp;amp;Parent_pageType=" title="https://www.nxp.com/webapp/Download?colCode=AN3940&amp;amp;location=null&amp;amp;fsrch=1&amp;amp;sr=9&amp;amp;pageNum=2&amp;amp;Parent_nodeId=&amp;amp;Parent_pageType="&gt;https://www.nxp.com/webapp/Download?colCode=AN3940&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Note that the MMDC supports only x16 data bus width.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 24 Jul 2017 13:48:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/DDR3L-bit-swapping-with-LS1012A-processor-within-byte/m-p/680901#M2628</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2017-07-24T13:48:12Z</dc:date>
    </item>
  </channel>
</rss>