<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Layerscape中的主题 Re: LS1020A JTAG does not work</title>
    <link>https://community.nxp.com/t5/Layerscape/LS1020A-JTAG-does-not-work/m-p/676375#M2589</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I connected 32kHz RTC clock. Didn't help.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 08 Jun 2017 12:43:24 GMT</pubDate>
    <dc:creator>dainiuszilys</dc:creator>
    <dc:date>2017-06-08T12:43:24Z</dc:date>
    <item>
      <title>LS1020A JTAG does not work</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1020A-JTAG-does-not-work/m-p/676372#M2586</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm trying to run custom PCB with LS1020A. I use J-Link as JTAG adapter.&lt;/P&gt;&lt;P&gt;But the LS1020A does not respond properly. Here is a log of access:&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;Tue Jun 06, 2017 16:07:39: Could not measure total IR len. TDO is constant high. &lt;BR /&gt;Tue Jun 06, 2017 16:07:39: TotalIRLen = ?, IRPrint = 0x..FFFFFFFFFFFFF814C7B00009 &lt;BR /&gt;Tue Jun 06, 2017 16:07:39: Could not measure total IR len. TDO is constant high. &lt;BR /&gt;Tue Jun 06, 2017 16:07:39: TotalIRLen = ?, IRPrint = 0x..FFFFFFFFFFFFFE0C80000009 &lt;BR /&gt;Tue Jun 06, 2017 16:07:39: Could not measure total IR len. TDO is constant high. &lt;BR /&gt;Tue Jun 06, 2017 16:07:39: TotalIRLen = ?, IRPrint = 0x..000000000000000000000000 &lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;There are no any other devices in the JTAG chain. No visual noise on jtag lines, pulses are nice.&lt;/P&gt;&lt;P&gt;RCW is hard-coded. RESET_REQ_B is released (logic 1).&lt;/P&gt;&lt;P&gt;Tryed with uSD card RCW + software. Situation is the same - the response on TDO is almost random, software starts running (output on UART exists). So CPU is alive, but I can't access it via JTAG to debug.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Tryed various JTAG clocks - 32khz - 1MHz, - no influence.&lt;/P&gt;&lt;P&gt;Hardware connection seems to be fine: SCAN_MODE_B, TEST_SEL_B - pull-ups to 1.8V, TRST_B connected to PORESET_B. TCK has pull-up of 10k, as recommended. System clock is 100MHz.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Where could be a problem?&lt;/P&gt;&lt;P&gt;J-Link works on LS1021A Tower board, so adapter should be compatable with my PCB as well.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 06 Jun 2017 13:33:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1020A-JTAG-does-not-work/m-p/676372#M2586</guid>
      <dc:creator>dainiuszilys</dc:creator>
      <dc:date>2017-06-06T13:33:12Z</dc:date>
    </item>
    <item>
      <title>Re: LS1020A JTAG does not work</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1020A-JTAG-does-not-work/m-p/676373#M2587</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;LS1021A and LS1020A are based on the same silicon, so if your J-link works on LS1021A, than it should also work on LS1020A.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please perform the following:&lt;/P&gt;&lt;P&gt;1. Please verify all power supplies are stable at their desired values, and power supply noise is as expected.&lt;/P&gt;&lt;P&gt;2. Please check TRST state. If TRST is connected to PORESET, please make sure TRST is asserted at least once at power-on, and than released.&lt;/P&gt;&lt;P&gt;3. Please look JTAG pins by scope for extra noise caused by signal reflections on long traces.&lt;/P&gt;&lt;P&gt;4. Please compare scope screenshots of JTAG signals with similar screenshots from "good" board&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Alexander&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 07 Jun 2017 05:44:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1020A-JTAG-does-not-work/m-p/676373#M2587</guid>
      <dc:creator>alexander_yakov</dc:creator>
      <dc:date>2017-06-07T05:44:10Z</dc:date>
    </item>
    <item>
      <title>Re: LS1020A JTAG does not work</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1020A-JTAG-does-not-work/m-p/676374#M2588</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I made the comparison of JTAG signals. No answer so far. Wrong PCB returns random response, while the Tower board always returns the same response to the same request.&lt;/P&gt;&lt;P&gt;Here are diagrams of wrong response of LS1020A:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="wrong1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/19966i6BA58C7F4058FF2B/image-size/large?v=v2&amp;amp;px=999" role="button" title="wrong1.png" alt="wrong1.png" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="wrong2.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/20023iA29AEF547CEB069A/image-size/large?v=v2&amp;amp;px=999" role="button" title="wrong2.png" alt="wrong2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here is the response of Tower board, which is always the same, and understandable by JTAG adapter:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="good.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/20123i313F13F12E9D8625/image-size/large?v=v2&amp;amp;px=999" role="button" title="good.png" alt="good.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;TCK frequency in both cases is 1MHz.&lt;/P&gt;&lt;P&gt;TRST_B was reset just before capturing diagrams in all 3 cases.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So still no idea, what's wrong with the PCB...&lt;/P&gt;&lt;P&gt;Maybe a kind of security bits are on by default?&lt;/P&gt;&lt;P&gt;RTC has no 32kHz clock in my PCB. Maybe that's the reason?&lt;/P&gt;&lt;P&gt;Anything else can disable debug port?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 07 Jun 2017 09:07:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1020A-JTAG-does-not-work/m-p/676374#M2588</guid>
      <dc:creator>dainiuszilys</dc:creator>
      <dc:date>2017-06-07T09:07:11Z</dc:date>
    </item>
    <item>
      <title>Re: LS1020A JTAG does not work</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1020A-JTAG-does-not-work/m-p/676375#M2589</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I connected 32kHz RTC clock. Didn't help.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 08 Jun 2017 12:43:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1020A-JTAG-does-not-work/m-p/676375#M2589</guid>
      <dc:creator>dainiuszilys</dc:creator>
      <dc:date>2017-06-08T12:43:24Z</dc:date>
    </item>
  </channel>
</rss>