<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Twin die DDR3L interface with LS1012 in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/Twin-die-DDR3L-interface-with-LS1012/m-p/671631#M2515</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have question regarding DDR3L memory interface on LS1012 processor&lt;/P&gt;&lt;P&gt;I'm designing a custom board which will have DDR3L memory and density 2GByte as well two Die or two chipsets (1GByte).&lt;/P&gt;&lt;P&gt;I've explored datasheet of LS1012 and found only one CS, one CKE, and one ODT pins are available.&lt;/P&gt;&lt;P&gt;Please let me know how to interface 2GByte DDR3L memory with LS1012 and which signals are required to the configuration of two two chip or dual die.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;P&gt;Regars,&lt;/P&gt;&lt;P&gt;Alpesh&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 01 Jun 2017 09:47:46 GMT</pubDate>
    <dc:creator>alpeshmandani</dc:creator>
    <dc:date>2017-06-01T09:47:46Z</dc:date>
    <item>
      <title>Twin die DDR3L interface with LS1012</title>
      <link>https://community.nxp.com/t5/Layerscape/Twin-die-DDR3L-interface-with-LS1012/m-p/671631#M2515</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have question regarding DDR3L memory interface on LS1012 processor&lt;/P&gt;&lt;P&gt;I'm designing a custom board which will have DDR3L memory and density 2GByte as well two Die or two chipsets (1GByte).&lt;/P&gt;&lt;P&gt;I've explored datasheet of LS1012 and found only one CS, one CKE, and one ODT pins are available.&lt;/P&gt;&lt;P&gt;Please let me know how to interface 2GByte DDR3L memory with LS1012 and which signals are required to the configuration of two two chip or dual die.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;P&gt;Regars,&lt;/P&gt;&lt;P&gt;Alpesh&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 01 Jun 2017 09:47:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Twin-die-DDR3L-interface-with-LS1012/m-p/671631#M2515</guid>
      <dc:creator>alpeshmandani</dc:creator>
      <dc:date>2017-06-01T09:47:46Z</dc:date>
    </item>
    <item>
      <title>Re: Twin die DDR3L interface with LS1012</title>
      <link>https://community.nxp.com/t5/Layerscape/Twin-die-DDR3L-interface-with-LS1012/m-p/671632#M2516</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The only way to get 2GB of memory is to use two 8Gb x8 DDR3L devices to form 16-bit DDR bus. These can be for example MT41K1G8 devices from Micron. Both devices should be connected to the same address, command, clock&amp;nbsp; CS, MCKE and ODT signals. Data group signals should be connected individually to the devices in point-to-point way, one byte lane to one device, second byte lane to the other device.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Bulat&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 01 Jun 2017 11:38:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Twin-die-DDR3L-interface-with-LS1012/m-p/671632#M2516</guid>
      <dc:creator>Bulat</dc:creator>
      <dc:date>2017-06-01T11:38:29Z</dc:date>
    </item>
    <item>
      <title>Re: Twin die DDR3L interface with LS1012</title>
      <link>https://community.nxp.com/t5/Layerscape/Twin-die-DDR3L-interface-with-LS1012/m-p/671633#M2517</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Bulat,&lt;/P&gt;&lt;P&gt;Thanks for your providing answer.&lt;/P&gt;&lt;P&gt;I will design schematic as per above suggestion and send back to you for review.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Alpesh&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 01 Jun 2017 13:53:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Twin-die-DDR3L-interface-with-LS1012/m-p/671633#M2517</guid>
      <dc:creator>alpeshmandani</dc:creator>
      <dc:date>2017-06-01T13:53:48Z</dc:date>
    </item>
    <item>
      <title>Re: Twin die DDR3L interface with LS1012</title>
      <link>https://community.nxp.com/t5/Layerscape/Twin-die-DDR3L-interface-with-LS1012/m-p/671634#M2518</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Bulat,&lt;/P&gt;&lt;P&gt;&amp;nbsp;I am considering to connect two individual 8Gb/4Gb X 8 bit memory&amp;nbsp; from a 16bit bus width of the processor to expand up to 2Gbyte.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please let me know which Routing Topologies ( Fly- By Topology or T-Topology) are best for the DDR3L memory interface.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Alpesh Mandani&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 06 Jun 2017 04:59:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Twin-die-DDR3L-interface-with-LS1012/m-p/671634#M2518</guid>
      <dc:creator>alpeshmandani</dc:creator>
      <dc:date>2017-06-06T04:59:17Z</dc:date>
    </item>
  </channel>
</rss>