<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic DDR4-1600 errata clarification on LS1043 in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/DDR4-1600-errata-clarification-on-LS1043/m-p/669308#M2485</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The LS1043 A-007864 errata says "If a DRAM data bus width of 16 bits or less is used with DDR4 memories running at 1600 MT/s data rate, then tCCD_L is violated by the controller". Does this refer to the component data width or the full width of the controller? If the latter, does this mean that tCCD_L will be five cycles when the controller data width is 32 bits?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We have two 16-bit components combined to a 32-bit memory and we are experiencing memory corruption at 1600 MT/s. Things appear to work at 1333 MT/s.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 31 May 2017 08:55:32 GMT</pubDate>
    <dc:creator>perchrc</dc:creator>
    <dc:date>2017-05-31T08:55:32Z</dc:date>
    <item>
      <title>DDR4-1600 errata clarification on LS1043</title>
      <link>https://community.nxp.com/t5/Layerscape/DDR4-1600-errata-clarification-on-LS1043/m-p/669308#M2485</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The LS1043 A-007864 errata says "If a DRAM data bus width of 16 bits or less is used with DDR4 memories running at 1600 MT/s data rate, then tCCD_L is violated by the controller". Does this refer to the component data width or the full width of the controller? If the latter, does this mean that tCCD_L will be five cycles when the controller data width is 32 bits?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We have two 16-bit components combined to a 32-bit memory and we are experiencing memory corruption at 1600 MT/s. Things appear to work at 1333 MT/s.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 31 May 2017 08:55:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/DDR4-1600-errata-clarification-on-LS1043/m-p/669308#M2485</guid>
      <dc:creator>perchrc</dc:creator>
      <dc:date>2017-05-31T08:55:32Z</dc:date>
    </item>
    <item>
      <title>Re: DDR4-1600 errata clarification on LS1043</title>
      <link>https://community.nxp.com/t5/Layerscape/DDR4-1600-errata-clarification-on-LS1043/m-p/669309#M2486</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The errata refers to DDR bus width of the controller.&lt;/P&gt;&lt;P&gt;What kind of corruptions in your case? Did you check ERR_DETECT register after DDR initialization for errors?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Bulat&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 01 Jun 2017 10:51:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/DDR4-1600-errata-clarification-on-LS1043/m-p/669309#M2486</guid>
      <dc:creator>Bulat</dc:creator>
      <dc:date>2017-06-01T10:51:01Z</dc:date>
    </item>
  </channel>
</rss>