<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Layerscapeのトピック [LS1043ARDB] Cores boot at different exception levels</title>
    <link>https://community.nxp.com/t5/Layerscape/LS1043ARDB-Cores-boot-at-different-exception-levels/m-p/667167#M2463</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Iam having a problem with one of the LS1043ARDB board (Orange box), after U-boot loads my program, core0 is at exception level 2 (EL2), but the other cores boot at EL1 and get hang when trying to switch to EL2. I have another LS1043ARDB board (Gray box) and all the cores boot at EL2. the same uboot image is on both boards: "U-Boot 2016.012.0+ga9b437f (May 15 2016 - 11:01:10 +0800)", and both boards have the same dip switch settings. I have however noticed the below differences in the uboot boot log:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The orange box (not working):&lt;/P&gt;&lt;P&gt;CPLD:&amp;nbsp; V1.4&lt;/P&gt;&lt;P&gt;PPA Firmware: Version 0.1&lt;/P&gt;&lt;P&gt;EEPROM: NXID v1&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The gray box (working):&lt;/P&gt;&lt;P&gt;CPLD:&amp;nbsp; V1.5&lt;/P&gt;&lt;P&gt;PPA Firmware: Version 0.2&lt;/P&gt;&lt;P&gt;EEPROM: Invalid ID (0b 0c 03 04)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any idea why the orange box has the cores boot at different EL? Should&amp;nbsp; the color of the box mean something (like secure)?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 20 Jun 2017 14:44:11 GMT</pubDate>
    <dc:creator>zalbassam</dc:creator>
    <dc:date>2017-06-20T14:44:11Z</dc:date>
    <item>
      <title>[LS1043ARDB] Cores boot at different exception levels</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1043ARDB-Cores-boot-at-different-exception-levels/m-p/667167#M2463</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Iam having a problem with one of the LS1043ARDB board (Orange box), after U-boot loads my program, core0 is at exception level 2 (EL2), but the other cores boot at EL1 and get hang when trying to switch to EL2. I have another LS1043ARDB board (Gray box) and all the cores boot at EL2. the same uboot image is on both boards: "U-Boot 2016.012.0+ga9b437f (May 15 2016 - 11:01:10 +0800)", and both boards have the same dip switch settings. I have however noticed the below differences in the uboot boot log:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The orange box (not working):&lt;/P&gt;&lt;P&gt;CPLD:&amp;nbsp; V1.4&lt;/P&gt;&lt;P&gt;PPA Firmware: Version 0.1&lt;/P&gt;&lt;P&gt;EEPROM: NXID v1&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The gray box (working):&lt;/P&gt;&lt;P&gt;CPLD:&amp;nbsp; V1.5&lt;/P&gt;&lt;P&gt;PPA Firmware: Version 0.2&lt;/P&gt;&lt;P&gt;EEPROM: Invalid ID (0b 0c 03 04)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any idea why the orange box has the cores boot at different EL? Should&amp;nbsp; the color of the box mean something (like secure)?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 20 Jun 2017 14:44:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1043ARDB-Cores-boot-at-different-exception-levels/m-p/667167#M2463</guid>
      <dc:creator>zalbassam</dc:creator>
      <dc:date>2017-06-20T14:44:11Z</dc:date>
    </item>
    <item>
      <title>Re:  [LS1043ARDB] Cores boot at different exception levels</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1043ARDB-Cores-boot-at-different-exception-levels/m-p/667168#M2464</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;A _jive_internal="true" data-content-finding="Community" data-userid="295081" data-username="zalbassam" href="https://community.nxp.com/people/zalbassam"&gt;Zaid Albassam&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The problem should be caused by PPA firmware not compatible with U-BOOT 2016.012. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please flash the attached ppa image on the problem board.&lt;/P&gt;&lt;P&gt;PPA address on NOR flash of LS1043.&lt;/P&gt;&lt;P&gt;bank 0:0x60500000&lt;/P&gt;&lt;P&gt;bank 4: 0x64500000&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 26 Jun 2017 09:20:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1043ARDB-Cores-boot-at-different-exception-levels/m-p/667168#M2464</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2017-06-26T09:20:59Z</dc:date>
    </item>
    <item>
      <title>Re:  [LS1043ARDB] Cores boot at different exception levels</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1043ARDB-Cores-boot-at-different-exception-levels/m-p/667169#M2465</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/yipingwang"&gt;yipingwang&lt;/A&gt;‌,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My board now shows that the PPA version is upped to v0.2, and with that my problem is resolved.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I wished that U-boot could detect these incompatibility with the PPA and at least print a warning in the boot log, It could have saved me couple of days of investigations.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Anyways, thanks for the help.&lt;/P&gt;&lt;P&gt;Zaid&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 26 Jun 2017 14:55:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1043ARDB-Cores-boot-at-different-exception-levels/m-p/667169#M2465</guid>
      <dc:creator>zalbassam</dc:creator>
      <dc:date>2017-06-26T14:55:01Z</dc:date>
    </item>
  </channel>
</rss>