<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LayerscapeのトピックRe: LS1021A-TWR: Full reprogram</title>
    <link>https://community.nxp.com/t5/Layerscape/LS1021A-TWR-Full-reprogram/m-p/664919#M2420</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV class=""&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I recreated the CW RAM application project.&lt;/P&gt;&lt;P&gt;Now programming works fine.&lt;/P&gt;&lt;P&gt;Thank you !&lt;/P&gt;&lt;P&gt;Z.V&lt;/P&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 03 Feb 2017 23:17:52 GMT</pubDate>
    <dc:creator>z_v</dc:creator>
    <dc:date>2017-02-03T23:17:52Z</dc:date>
    <item>
      <title>LS1021A-TWR: Full reprogram</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1021A-TWR-Full-reprogram/m-p/664917#M2418</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In order to reprogram the original image I did the following:&lt;/P&gt;&lt;P&gt;SW2 - 01001111&lt;/P&gt;&lt;P&gt;SW3 - 01100101&lt;/P&gt;&lt;P&gt;(This is setup I got here)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But in CW I got the message:&lt;/P&gt;&lt;P&gt;Error: The algorithm was not able to run on the target of the flash is not configured properly&lt;/P&gt;&lt;P&gt;Error: Getting flash ID failed&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can you please help ?&lt;/P&gt;&lt;P&gt;Both banks are currently not running.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Z.V&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 03 Feb 2017 08:08:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1021A-TWR-Full-reprogram/m-p/664917#M2418</guid>
      <dc:creator>z_v</dc:creator>
      <dc:date>2017-02-03T08:08:57Z</dc:date>
    </item>
    <item>
      <title>Re: LS1021A-TWR: Full reprogram</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1021A-TWR-Full-reprogram/m-p/664918#M2419</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Which exactly TWR revision is in question?&lt;/P&gt;&lt;P&gt;Please provide photos of the on-board inscriptions and stickers.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please provide additional information about CodeWarrior setup:&lt;/P&gt;&lt;P&gt;1) which Debug Configuration is used?&lt;/P&gt;&lt;P&gt;2) complete Flash Programmer log as a text file&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 03 Feb 2017 12:27:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1021A-TWR-Full-reprogram/m-p/664918#M2419</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2017-02-03T12:27:50Z</dc:date>
    </item>
    <item>
      <title>Re: LS1021A-TWR: Full reprogram</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1021A-TWR-Full-reprogram/m-p/664919#M2420</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV class=""&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I recreated the CW RAM application project.&lt;/P&gt;&lt;P&gt;Now programming works fine.&lt;/P&gt;&lt;P&gt;Thank you !&lt;/P&gt;&lt;P&gt;Z.V&lt;/P&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 03 Feb 2017 23:17:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1021A-TWR-Full-reprogram/m-p/664919#M2420</guid>
      <dc:creator>z_v</dc:creator>
      <dc:date>2017-02-03T23:17:52Z</dc:date>
    </item>
  </channel>
</rss>