<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: A Question About GPIO1 On The LS1021ATWR Development Board in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/A-Question-About-GPIO1-On-The-LS1021ATWR-Development-Board/m-p/407956#M241</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;LS1021A Reference Manual, Table 4-15 "RCW Field Descriptions", the description of the "UART_BASE" field has the following note:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;NOTE: Note that UART_EXT field must be set to all&lt;/P&gt;&lt;P&gt;0's for UART_BASE to take effect.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In your case UART_EXT seems to be set to "100" if my calculations are correct&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Apr 2015 16:18:09 GMT</pubDate>
    <dc:creator>alexander_yakov</dc:creator>
    <dc:date>2015-04-15T16:18:09Z</dc:date>
    <item>
      <title>A Question About GPIO1 On The LS1021ATWR Development Board</title>
      <link>https://community.nxp.com/t5/Layerscape/A-Question-About-GPIO1-On-The-LS1021ATWR-Development-Board/m-p/407955#M240</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi everybody,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We have a (hopefully) quick question about GPIO support on the LS1021a-twr development board.&amp;nbsp; Specifically GPIO port 1.&amp;nbsp; We've created a project in codewarrior for us to try to wiggle the pins on GPIO1, specifically pin GPIO1[15], but we don't seem to see any change on the various GPIO1 registers located at memory offset 0x02300008 (even after setting the GPIO1 DIR pins to outputs).&amp;nbsp; We're able to change the direction and data of GPIO3 (memory address 0x02320000), but not GPIO1, which is the one that we kind of need at the moment.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are currently loading the RCW and U-Boot image from SD card.&amp;nbsp; We believe we have disabled all the UART support properly, in order for the GPIO pins to be set up as, well, GPIO.&amp;nbsp; The RCW we're using is as follows:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;0608000a 00000000 00000000 00000000&lt;/P&gt;&lt;P&gt;20000000 00407900 60025a00 21046000&lt;/P&gt;&lt;P&gt;00000000 00000000 00000000 21000000&lt;/P&gt;&lt;P&gt;20024800 24bb1540 00000000 00000000&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there any field that we may have missed that is needed to support all GPIO ports?&amp;nbsp; Or is there some flag needed when compiling the U-Boot image that will enable all GPIO ports?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Patrick&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 14 Apr 2015 16:19:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/A-Question-About-GPIO1-On-The-LS1021ATWR-Development-Board/m-p/407955#M240</guid>
      <dc:creator>patrickmorrow</dc:creator>
      <dc:date>2015-04-14T16:19:34Z</dc:date>
    </item>
    <item>
      <title>Re: A Question About GPIO1 On The LS1021ATWR Development Board</title>
      <link>https://community.nxp.com/t5/Layerscape/A-Question-About-GPIO1-On-The-LS1021ATWR-Development-Board/m-p/407956#M241</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;LS1021A Reference Manual, Table 4-15 "RCW Field Descriptions", the description of the "UART_BASE" field has the following note:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;NOTE: Note that UART_EXT field must be set to all&lt;/P&gt;&lt;P&gt;0's for UART_BASE to take effect.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In your case UART_EXT seems to be set to "100" if my calculations are correct&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Apr 2015 16:18:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/A-Question-About-GPIO1-On-The-LS1021ATWR-Development-Board/m-p/407956#M241</guid>
      <dc:creator>alexander_yakov</dc:creator>
      <dc:date>2015-04-15T16:18:09Z</dc:date>
    </item>
  </channel>
</rss>