<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Layerscape中的主题 Re: Clock outputs from LS1021A</title>
    <link>https://community.nxp.com/t5/Layerscape/Clock-outputs-from-LS1021A/m-p/655008#M2325</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Have a great day,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;LS1021A has several timers which can generate ~1KHz from the system clock (or form an external clock). &lt;BR /&gt;These timers are :&lt;/P&gt;&lt;P&gt;&amp;nbsp;Flex Timer - Please see chapter 1.4.11 FlexTimer module (FTM) and for details chapter 21 FlexTimer Module (FTM) in the LS1021A reference manual. Output signals are FTMn_CHm in the Data Sheet pinout list. For example FTM1_CH0 is channel 0 output of flex timer module1.&lt;/P&gt;&lt;P&gt;&amp;nbsp;Timer-baud-rate generator. Please see Chapter 30.3.3.2 Multiplexing and timers-baud-rate generators (BRGs), BRG configuration registers 1-4 (BRGCn) in the reference manual. Output signals are BRGOn.&lt;/P&gt;&lt;P&gt;&amp;nbsp;IEEE 1588 integration timer. See chapter 20.9.7 Hardware assist for IEEE Std. 1588 compliant timestamping in the manula and application note “Support for IEEE 1588™ Protocol in PowerQUICC and QorIQ Processors”&lt;BR /&gt; &lt;A href="http://cache.nxp.com/files/32bit/doc/app_note/AN3423.pdf"&gt;http://cache.nxp.com/files/32bit/doc/app_note/AN3423.pdf&lt;/A&gt;&lt;BR /&gt; It can provide pulses on 2 outputs: TSEC_1588_PULSE_OUT1 and TSEC_1588_PULSE_OUT1.&lt;/P&gt;&lt;P&gt;Notice that timer’s outputs are shared by different timers and other blocks signals. For example, pin Y2 may provide one of these signals GPIO4_05/EC3_RXD1/TSEC_1588_PULSE_OUT1/FTM3_CH3.&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 21 Oct 2016 14:34:32 GMT</pubDate>
    <dc:creator>r8070z</dc:creator>
    <dc:date>2016-10-21T14:34:32Z</dc:date>
    <item>
      <title>Clock outputs from LS1021A</title>
      <link>https://community.nxp.com/t5/Layerscape/Clock-outputs-from-LS1021A/m-p/655007#M2324</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, &lt;/P&gt;&lt;P&gt;I need to give four 1KHz clock outputs from LS1021 to different modules&amp;nbsp;as a&amp;nbsp;diagnostic pulse (ticks).&lt;/P&gt;&lt;P&gt;Can someone suggest which pins can be used for this purpose?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 21 Oct 2016 11:41:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Clock-outputs-from-LS1021A/m-p/655007#M2324</guid>
      <dc:creator>deepaknaiknavar</dc:creator>
      <dc:date>2016-10-21T11:41:42Z</dc:date>
    </item>
    <item>
      <title>Re: Clock outputs from LS1021A</title>
      <link>https://community.nxp.com/t5/Layerscape/Clock-outputs-from-LS1021A/m-p/655008#M2325</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Have a great day,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;LS1021A has several timers which can generate ~1KHz from the system clock (or form an external clock). &lt;BR /&gt;These timers are :&lt;/P&gt;&lt;P&gt;&amp;nbsp;Flex Timer - Please see chapter 1.4.11 FlexTimer module (FTM) and for details chapter 21 FlexTimer Module (FTM) in the LS1021A reference manual. Output signals are FTMn_CHm in the Data Sheet pinout list. For example FTM1_CH0 is channel 0 output of flex timer module1.&lt;/P&gt;&lt;P&gt;&amp;nbsp;Timer-baud-rate generator. Please see Chapter 30.3.3.2 Multiplexing and timers-baud-rate generators (BRGs), BRG configuration registers 1-4 (BRGCn) in the reference manual. Output signals are BRGOn.&lt;/P&gt;&lt;P&gt;&amp;nbsp;IEEE 1588 integration timer. See chapter 20.9.7 Hardware assist for IEEE Std. 1588 compliant timestamping in the manula and application note “Support for IEEE 1588™ Protocol in PowerQUICC and QorIQ Processors”&lt;BR /&gt; &lt;A href="http://cache.nxp.com/files/32bit/doc/app_note/AN3423.pdf"&gt;http://cache.nxp.com/files/32bit/doc/app_note/AN3423.pdf&lt;/A&gt;&lt;BR /&gt; It can provide pulses on 2 outputs: TSEC_1588_PULSE_OUT1 and TSEC_1588_PULSE_OUT1.&lt;/P&gt;&lt;P&gt;Notice that timer’s outputs are shared by different timers and other blocks signals. For example, pin Y2 may provide one of these signals GPIO4_05/EC3_RXD1/TSEC_1588_PULSE_OUT1/FTM3_CH3.&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 21 Oct 2016 14:34:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Clock-outputs-from-LS1021A/m-p/655008#M2325</guid>
      <dc:creator>r8070z</dc:creator>
      <dc:date>2016-10-21T14:34:32Z</dc:date>
    </item>
  </channel>
</rss>