<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: DDR3L AC/DC input high voltage too low in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/DDR3L-AC-DC-input-high-voltage-too-low/m-p/651228#M2257</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It is convenient to investigate the issue as Technical Case:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.freescale.com/thread/381898"&gt;https://community.freescale.com/thread/381898&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 08 Dec 2016 06:25:51 GMT</pubDate>
    <dc:creator>ufedor</dc:creator>
    <dc:date>2016-12-08T06:25:51Z</dc:date>
    <item>
      <title>DDR3L AC/DC input high voltage too low</title>
      <link>https://community.nxp.com/t5/Layerscape/DDR3L-AC-DC-input-high-voltage-too-low/m-p/651227#M2256</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P style="margin: 0cm 0cm 0pt;"&gt;Hello,&lt;/P&gt;&lt;P style="margin: 0cm 0cm 0pt;"&gt;we use a LS1021A (LS1021AXE7KQB) in a costumer specific Design. As DDR3L-Ram we use 1x Nanya NT5CC256M16DP-DIH with 16-bit Data bus width and 1600MT/s. The control and address lines are terminated with 39Ohm-Resistors tied to VTT (0,675V).&lt;/P&gt;&lt;P style="margin: 0cm 0cm 0pt;"&gt;According to the DDR3-L Compliance Test App (Keysight Test-App, Signal Analyzer: DSO90604A) the High Level VIH.CA (AC) and VIH.CA(DC) at the Adress an Control Input Pins (e.g. A2) are to low (see attached). 760mV instead of 810mV minimum according to the JEDEC Standard No. 79-3-1A.01, Table 4.&lt;/P&gt;&lt;P style="margin: 0cm 0cm 0pt;"&gt;We already tried different Termination resistors (27R and 100R) with the same result.&lt;/P&gt;&lt;P style="margin: 0cm 0cm 0pt;"&gt;What could be the reason for this?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 06 Dec 2016 11:20:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/DDR3L-AC-DC-input-high-voltage-too-low/m-p/651227#M2256</guid>
      <dc:creator>markusthoss</dc:creator>
      <dc:date>2016-12-06T11:20:25Z</dc:date>
    </item>
    <item>
      <title>Re: DDR3L AC/DC input high voltage too low</title>
      <link>https://community.nxp.com/t5/Layerscape/DDR3L-AC-DC-input-high-voltage-too-low/m-p/651228#M2257</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It is convenient to investigate the issue as Technical Case:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.freescale.com/thread/381898"&gt;https://community.freescale.com/thread/381898&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 08 Dec 2016 06:25:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/DDR3L-AC-DC-input-high-voltage-too-low/m-p/651228#M2257</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2016-12-08T06:25:51Z</dc:date>
    </item>
  </channel>
</rss>