<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LayerscapeのトピックBuild u-boot without bitbake</title>
    <link>https://community.nxp.com/t5/Layerscape/Build-u-boot-without-bitbake/m-p/648226#M2192</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I installed SDK 2.0 and installed the toolchain in a specidifed folder.&lt;/P&gt;&lt;P&gt;Then I found u-boot sources and copied them to another folder.&lt;/P&gt;&lt;P&gt;Now I want to compile u-boot with this toolchain.&lt;/P&gt;&lt;P&gt;So I ran:&lt;/P&gt;&lt;P&gt;./fsl-qoriq-glibc-&amp;lt;host_arch&amp;gt;-&amp;lt;core&amp;gt;-toolchain-&amp;lt;release&amp;gt;.sh&lt;/P&gt;&lt;P&gt;make clean&lt;/P&gt;&lt;P&gt;make ls1021atwr_nor_config&lt;/P&gt;&lt;P&gt;make&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But I suspect something is missing. I burned u-boot.bin starting from 0x60100000 and nothing happens.&lt;/P&gt;&lt;P&gt;How can I learn was exactly running when running:&lt;/P&gt;&lt;P&gt;bitbake -c compile -f u-boot&lt;/P&gt;&lt;P&gt;bitbake u-boot&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Z.V&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 29 Dec 2016 04:14:47 GMT</pubDate>
    <dc:creator>z_v</dc:creator>
    <dc:date>2016-12-29T04:14:47Z</dc:date>
    <item>
      <title>Build u-boot without bitbake</title>
      <link>https://community.nxp.com/t5/Layerscape/Build-u-boot-without-bitbake/m-p/648226#M2192</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I installed SDK 2.0 and installed the toolchain in a specidifed folder.&lt;/P&gt;&lt;P&gt;Then I found u-boot sources and copied them to another folder.&lt;/P&gt;&lt;P&gt;Now I want to compile u-boot with this toolchain.&lt;/P&gt;&lt;P&gt;So I ran:&lt;/P&gt;&lt;P&gt;./fsl-qoriq-glibc-&amp;lt;host_arch&amp;gt;-&amp;lt;core&amp;gt;-toolchain-&amp;lt;release&amp;gt;.sh&lt;/P&gt;&lt;P&gt;make clean&lt;/P&gt;&lt;P&gt;make ls1021atwr_nor_config&lt;/P&gt;&lt;P&gt;make&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But I suspect something is missing. I burned u-boot.bin starting from 0x60100000 and nothing happens.&lt;/P&gt;&lt;P&gt;How can I learn was exactly running when running:&lt;/P&gt;&lt;P&gt;bitbake -c compile -f u-boot&lt;/P&gt;&lt;P&gt;bitbake u-boot&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Z.V&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Dec 2016 04:14:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Build-u-boot-without-bitbake/m-p/648226#M2192</guid>
      <dc:creator>z_v</dc:creator>
      <dc:date>2016-12-29T04:14:47Z</dc:date>
    </item>
    <item>
      <title>Re: Build u-boot without bitbake</title>
      <link>https://community.nxp.com/t5/Layerscape/Build-u-boot-without-bitbake/m-p/648227#M2193</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I did the same but used last u-boot code (2016.09) it worked.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Z.V&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Dec 2016 09:30:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Build-u-boot-without-bitbake/m-p/648227#M2193</guid>
      <dc:creator>z_v</dc:creator>
      <dc:date>2016-12-29T09:30:00Z</dc:date>
    </item>
    <item>
      <title>Re: Build u-boot without bitbake</title>
      <link>https://community.nxp.com/t5/Layerscape/Build-u-boot-without-bitbake/m-p/648228#M2194</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;SPAN class=""&gt;&lt;A _jive_internal="true" data-content-finding="Community" data-userid="30650" data-username="z.v" href="https://community.nxp.com/people/z.v"&gt;Vered Zvi&lt;/A&gt;&lt;/SPAN&gt;,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please refer to the following procedure, I have verified the built image, it works on the target board.&lt;/P&gt;&lt;P&gt;$ source /opt/fsl-qoriq/2.0/environment-setup-cortexa7hf-vfp-neon-fsl-linux-gnueabi&lt;/P&gt;&lt;P&gt;$ make CROSS_COMPILE=arm-fsl-linux-gnueabi- ls1021atwr_nor_config&lt;/P&gt;&lt;P&gt;$ make -j 4 COSS_COMPILE=arm-fsl-linux-gnueabi-&amp;nbsp; all&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please use the image u-boot-dtb.bin.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yiping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 23 Jan 2017 05:55:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Build-u-boot-without-bitbake/m-p/648228#M2194</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2017-01-23T05:55:12Z</dc:date>
    </item>
  </channel>
</rss>