<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LayerscapeのトピックLS1012A - eMMC memory support</title>
    <link>https://community.nxp.com/t5/Layerscape/LS1012A-eMMC-memory-support/m-p/646347#M2166</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Can you please recommend eMMC memory which will work properly on LS1012A platform?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As I saw in the data brief, the parameters are following:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Interface on the LS1012A: eSDHC2&lt;/P&gt;&lt;P&gt;eMMC version: eMMC 4.4, eMMC 4.5&lt;/P&gt;&lt;P&gt;1.8V eMMC – modes FS/HS/HS200 or DDR&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can you please confirm this? Did you have chance to use the eMMC with LS1012A already? If yes, can you recommend some eMMC part number compatible with LS1012A?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 23 Sep 2016 09:15:00 GMT</pubDate>
    <dc:creator>markopavlovic</dc:creator>
    <dc:date>2016-09-23T09:15:00Z</dc:date>
    <item>
      <title>LS1012A - eMMC memory support</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1012A-eMMC-memory-support/m-p/646347#M2166</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Can you please recommend eMMC memory which will work properly on LS1012A platform?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As I saw in the data brief, the parameters are following:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Interface on the LS1012A: eSDHC2&lt;/P&gt;&lt;P&gt;eMMC version: eMMC 4.4, eMMC 4.5&lt;/P&gt;&lt;P&gt;1.8V eMMC – modes FS/HS/HS200 or DDR&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can you please confirm this? Did you have chance to use the eMMC with LS1012A already? If yes, can you recommend some eMMC part number compatible with LS1012A?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 23 Sep 2016 09:15:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1012A-eMMC-memory-support/m-p/646347#M2166</guid>
      <dc:creator>markopavlovic</dc:creator>
      <dc:date>2016-09-23T09:15:00Z</dc:date>
    </item>
    <item>
      <title>Re: LS1012A - eMMC memory support</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1012A-eMMC-memory-support/m-p/646348#M2167</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;There is no recommended eMMC for the LS1012A. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;The LS1012a SDHC controller is the same as the LS1021a or LS1043a SDHC controller.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;You can see in community that there is no information about problem the SDHC using on the LS1021a or LS1043a or LS1012a board.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;For example the LS1021a QDS board uses the following eMMC:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;MTFC4GMZDM-1M WT or KLMAG2GE2A-A001 or N2M400FDB311A3CF.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Pavel Chubakov&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 27 Sep 2016 02:44:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1012A-eMMC-memory-support/m-p/646348#M2167</guid>
      <dc:creator>Pavel</dc:creator>
      <dc:date>2016-09-27T02:44:09Z</dc:date>
    </item>
    <item>
      <title>Re: LS1012A - eMMC memory support</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1012A-eMMC-memory-support/m-p/646349#M2168</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Pavel,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do you think SLC or MLC, which one would be better fit for ls1021a&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Sep 2019 13:41:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1012A-eMMC-memory-support/m-p/646349#M2168</guid>
      <dc:creator>jiye</dc:creator>
      <dc:date>2019-09-20T13:41:16Z</dc:date>
    </item>
  </channel>
</rss>