<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Management Signals for SERDES in LS1021A in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/Management-Signals-for-SERDES-in-LS1021A/m-p/641697#M2153</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;Is it required to provide Management signals (MDC/MDIO) to the external PHY device for the SGMII interface in LS1021A? I mean does the Serdes interface itself can be used for the configuration PHY chip instead of the MDC/MDIO signals?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 24 Jan 2017 12:31:43 GMT</pubDate>
    <dc:creator>deepaknaiknavar</dc:creator>
    <dc:date>2017-01-24T12:31:43Z</dc:date>
    <item>
      <title>Management Signals for SERDES in LS1021A</title>
      <link>https://community.nxp.com/t5/Layerscape/Management-Signals-for-SERDES-in-LS1021A/m-p/641697#M2153</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;Is it required to provide Management signals (MDC/MDIO) to the external PHY device for the SGMII interface in LS1021A? I mean does the Serdes interface itself can be used for the configuration PHY chip instead of the MDC/MDIO signals?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 24 Jan 2017 12:31:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Management-Signals-for-SERDES-in-LS1021A/m-p/641697#M2153</guid>
      <dc:creator>deepaknaiknavar</dc:creator>
      <dc:date>2017-01-24T12:31:43Z</dc:date>
    </item>
    <item>
      <title>Re: Management Signals for SERDES in LS1021A</title>
      <link>https://community.nxp.com/t5/Layerscape/Management-Signals-for-SERDES-in-LS1021A/m-p/641698#M2154</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Probably you could have a look at theTBI registers inside the eTSEC controller.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you are planning to use a SFP you could also use fixed phy controllers in linux to get a connection.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Jan 2017 10:25:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Management-Signals-for-SERDES-in-LS1021A/m-p/641698#M2154</guid>
      <dc:creator>erdani80</dc:creator>
      <dc:date>2017-01-25T10:25:02Z</dc:date>
    </item>
    <item>
      <title>Re: Management Signals for SERDES in LS1021A</title>
      <link>https://community.nxp.com/t5/Layerscape/Management-Signals-for-SERDES-in-LS1021A/m-p/641699#M2155</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;SGMII specification provides only for transferring&amp;nbsp; link status updates &lt;BR /&gt;over the SGMII link. Refer to SGMII Spesc, Section "Control Information &lt;BR /&gt;Exchanged Between Links". There are no provisions for setting or reading&lt;BR /&gt;any PHY register over SGMII. Thus, if you wish to have full control&lt;BR /&gt;over your PHY, yes,&amp;nbsp; you need to connect it to an out-of-band management&lt;BR /&gt;interface.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Platon&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 06 Feb 2017 09:30:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Management-Signals-for-SERDES-in-LS1021A/m-p/641699#M2155</guid>
      <dc:creator>bpe</dc:creator>
      <dc:date>2017-02-06T09:30:32Z</dc:date>
    </item>
  </channel>
</rss>