<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic What RTC driver and part for the LS1043ARDB? in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/What-RTC-driver-and-part-for-the-LS1043ARDB/m-p/634163#M2053</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;STRONG&gt;1) To clarify, what is the RTC &lt;EM&gt;part number&lt;/EM&gt; used by the LS1043ARDB eval board?&amp;nbsp;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;2) What driver is&amp;nbsp; used for that RTC part number on the LS1043ARDB eval?&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt; 3) To be more specific, is the RTC part number for the LS1043ARDB eval the &lt;SPAN style="font-size: 11pt; font-family: Calibri;"&gt;M41T81S part&lt;/SPAN&gt;?&amp;nbsp;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In kernel defconfig and .config, I see the following DS3232 configured, which I believe may be the Dallas off-chip part discussed in the SDK documentation.&amp;nbsp; But the RTC chip is not the DS3232 off-chip part from what I understand.&amp;nbsp; Is the RTC part number for the LS1043ARDB eval the &lt;SPAN style="font-size: 11pt; font-family: Calibri;"&gt;M41T81S&lt;/SPAN&gt;?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I see the &lt;SPAN style="font-size: 11pt; font-family: Calibri;"&gt;M41T80&lt;/SPAN&gt; but NXP&amp;nbsp; doesn't have this driver configured in the kernel configuration.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;CONFIG_RTC_DRV_DS3232=y&lt;BR /&gt;CONFIG_RTC_DRV_PCF2127=y&lt;/P&gt;&lt;P&gt;CONFIG_RTC_CLASS=y&lt;BR /&gt;CONFIG_RTC_DRV_EFI=y&lt;BR /&gt;CONFIG_RTC_DRV_XGENE=y&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So, I'm confused what part and driver is being used for the real-time clock on the LS1043ardb that provides the clock for the 5 WDOGs.&lt;STRONG&gt; &lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;4) Is the SDK 2.0 kernel configured and is it using the RTC at&amp;nbsp; on the LS1043ARDB eval board even though the RTC logic is there and presumably works?&amp;nbsp; &lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please clarify for customers the part number, driver, and what is or is not being used on the LS1043ARDB for the RTC that provides the clock to the 5 WDOGs. This is a bit frustrating for customers that need the WDOGs even if they may be planning to use an "off-chip" RTC.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;5) Has the RTC been validated on the LS1043ARDB?&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 30 Mar 2017 03:30:25 GMT</pubDate>
    <dc:creator>tracysmith</dc:creator>
    <dc:date>2017-03-30T03:30:25Z</dc:date>
    <item>
      <title>What RTC driver and part for the LS1043ARDB?</title>
      <link>https://community.nxp.com/t5/Layerscape/What-RTC-driver-and-part-for-the-LS1043ARDB/m-p/634163#M2053</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;STRONG&gt;1) To clarify, what is the RTC &lt;EM&gt;part number&lt;/EM&gt; used by the LS1043ARDB eval board?&amp;nbsp;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;2) What driver is&amp;nbsp; used for that RTC part number on the LS1043ARDB eval?&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt; 3) To be more specific, is the RTC part number for the LS1043ARDB eval the &lt;SPAN style="font-size: 11pt; font-family: Calibri;"&gt;M41T81S part&lt;/SPAN&gt;?&amp;nbsp;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In kernel defconfig and .config, I see the following DS3232 configured, which I believe may be the Dallas off-chip part discussed in the SDK documentation.&amp;nbsp; But the RTC chip is not the DS3232 off-chip part from what I understand.&amp;nbsp; Is the RTC part number for the LS1043ARDB eval the &lt;SPAN style="font-size: 11pt; font-family: Calibri;"&gt;M41T81S&lt;/SPAN&gt;?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I see the &lt;SPAN style="font-size: 11pt; font-family: Calibri;"&gt;M41T80&lt;/SPAN&gt; but NXP&amp;nbsp; doesn't have this driver configured in the kernel configuration.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;CONFIG_RTC_DRV_DS3232=y&lt;BR /&gt;CONFIG_RTC_DRV_PCF2127=y&lt;/P&gt;&lt;P&gt;CONFIG_RTC_CLASS=y&lt;BR /&gt;CONFIG_RTC_DRV_EFI=y&lt;BR /&gt;CONFIG_RTC_DRV_XGENE=y&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So, I'm confused what part and driver is being used for the real-time clock on the LS1043ardb that provides the clock for the 5 WDOGs.&lt;STRONG&gt; &lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;4) Is the SDK 2.0 kernel configured and is it using the RTC at&amp;nbsp; on the LS1043ARDB eval board even though the RTC logic is there and presumably works?&amp;nbsp; &lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please clarify for customers the part number, driver, and what is or is not being used on the LS1043ARDB for the RTC that provides the clock to the 5 WDOGs. This is a bit frustrating for customers that need the WDOGs even if they may be planning to use an "off-chip" RTC.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;5) Has the RTC been validated on the LS1043ARDB?&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 30 Mar 2017 03:30:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/What-RTC-driver-and-part-for-the-LS1043ARDB/m-p/634163#M2053</guid>
      <dc:creator>tracysmith</dc:creator>
      <dc:date>2017-03-30T03:30:25Z</dc:date>
    </item>
    <item>
      <title>Re: What RTC driver and part for the LS1043ARDB?</title>
      <link>https://community.nxp.com/t5/Layerscape/What-RTC-driver-and-part-for-the-LS1043ARDB/m-p/634164#M2054</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;Look at the following pages:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fcode.metager.de%2Fsource%2Fxref%2Fdenx%2Fu-boot%2Fdoc%2FuImage.FIT%2Fhowto.txt" rel="nofollow" target="_blank"&gt;http://code.metager.de/source/xref/denx/u-boot/doc/uImage.FIT/howto.txt&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;and&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fmanpages.ubuntu.com%2Fmanpages%2Fxenial%2Fman1%2Fmkimage.1.html" rel="nofollow" target="_blank"&gt;http://manpages.ubuntu.com/manpages/xenial/man1/mkimage.1.html&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Pavel Chubakov&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 04 Apr 2017 10:53:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/What-RTC-driver-and-part-for-the-LS1043ARDB/m-p/634164#M2054</guid>
      <dc:creator>Pavel</dc:creator>
      <dc:date>2017-04-04T10:53:49Z</dc:date>
    </item>
    <item>
      <title>Re: What RTC driver and part for the LS1043ARDB?</title>
      <link>https://community.nxp.com/t5/Layerscape/What-RTC-driver-and-part-for-the-LS1043ARDB/m-p/634165#M2055</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;OL&gt;&lt;LI&gt;&lt;SPAN style="font-size: 10.0pt;"&gt; The LS1043ARDB board uses the &lt;/SPAN&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;PT7C4338 as RTC. This RTC is practically compatible to DS3232. &lt;/SPAN&gt;&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;OL start="2"&gt;&lt;LI&gt;&lt;SPAN style="font-size: 10.0pt;"&gt; The rtc-ds3232.c file is used as RTC driver. See attached file.&lt;/SPAN&gt;&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;OL start="3"&gt;&lt;LI&gt;&lt;SPAN style="font-size: 10.0pt;"&gt; This SDK contains driver for &lt;SPAN style="color: black;"&gt;M41T80. See the rtc-m41t80.c file using the following path:&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; color: black;"&gt;/QorIQ-SDK-V2.0-20160527-yocto/build_ls1043ardb/tmp/work/ls1043ardb-fsl-linux/linux-qoriq/4.1-r0/git/drivers/rtc&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; color: black;"&gt;See attached screenshot from SDK 2.0 kernel menu.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Pavel Chubakov&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Apr 2017 09:59:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/What-RTC-driver-and-part-for-the-LS1043ARDB/m-p/634165#M2055</guid>
      <dc:creator>Pavel</dc:creator>
      <dc:date>2017-04-06T09:59:54Z</dc:date>
    </item>
  </channel>
</rss>