<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: How to power cycle SD card? in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/How-to-power-cycle-SD-card/m-p/631552#M2027</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Could you create service request about this problem? See the following page:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/381898"&gt;How I could create a Service Request?&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Add link to this Community (&lt;A href="https://community.nxp.com/thread/448086"&gt;How to power cycle SD card?&lt;/A&gt;) in this service request.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Pavel Chubakov&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 13 Apr 2017 01:47:23 GMT</pubDate>
    <dc:creator>Pavel</dc:creator>
    <dc:date>2017-04-13T01:47:23Z</dc:date>
    <item>
      <title>How to power cycle SD card?</title>
      <link>https://community.nxp.com/t5/Layerscape/How-to-power-cycle-SD-card/m-p/631545#M2020</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a problem on the ls1012ardb sd card and need help.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If I use a UHS-I card on the LS1012ARDB and switch the ESDHC1 to SDR104 mode with 1.8V signalling, everything works fine. However after I restart the board (without removing the card from the slot), by writing RESET_REQ in the RSTCR register, and try to reinit the sd card, the sd card refuses to switch to the 1.8v signalling (ACMD41 returns with S18A=0). If i remove and reinsert the card, 1.8v signalling is accepted and SDR104 works. I tried to reset the eSDHC block, but didnt help.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My question, Is there a way to power cycle the sd card to work around the problem?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;SD spec 4.01 in 4.2.3.1 states:&lt;/P&gt;&lt;P&gt;"UHS-I supported host sets S18R=1 in the argument of ACMD41 to request the card to switch 1.8V signaling level. UHS-I card respond with S18A=1 in the response of ACMD41 (if in 3.3V signaling&lt;BR /&gt;mode) and then host can issue voltage switch command. Once voltage switch is performed, UHS-I card&lt;BR /&gt;indicates S18A=0 to keep current signal voltage. In UHS-II mode, the card always indicates S18A=0."&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 30 Mar 2017 00:49:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/How-to-power-cycle-SD-card/m-p/631545#M2020</guid>
      <dc:creator>zalbassam</dc:creator>
      <dc:date>2017-03-30T00:49:31Z</dc:date>
    </item>
    <item>
      <title>Re: How to power cycle SD card?</title>
      <link>https://community.nxp.com/t5/Layerscape/How-to-power-cycle-SD-card/m-p/631546#M2021</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Iam still stuck on this one :smileysad: Any one please can help here? &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 03 Apr 2017 13:02:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/How-to-power-cycle-SD-card/m-p/631546#M2021</guid>
      <dc:creator>zalbassam</dc:creator>
      <dc:date>2017-04-03T13:02:45Z</dc:date>
    </item>
    <item>
      <title>Re: How to power cycle SD card?</title>
      <link>https://community.nxp.com/t5/Layerscape/How-to-power-cycle-SD-card/m-p/631547#M2022</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;It looks like that SD driver does not detect SD card after power up if SD card was connected before power up.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;Look at description of the CINS bit in the LS1012a Reference Manual.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Pavel Chubakov&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 04 Apr 2017 06:19:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/How-to-power-cycle-SD-card/m-p/631547#M2022</guid>
      <dc:creator>Pavel</dc:creator>
      <dc:date>2017-04-04T06:19:11Z</dc:date>
    </item>
    <item>
      <title>Re: How to power cycle SD card?</title>
      <link>https://community.nxp.com/t5/Layerscape/How-to-power-cycle-SD-card/m-p/631548#M2023</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Pavel,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your answer. Your answer doesnt answer my question. As I described in the question, after a warm reset (with the card is plugged) the card does get detected, however the card has already switched to 1.8v signalling and only a power cycle to the card would get it back to the 3.3v signalling. This issue is blocking us from supporting UHS-I for the esdhc. So:&lt;/P&gt;&lt;P&gt;1. Is the UHS-I modes for the ESDHC supposed to be supported on the LS1012ARDB?&lt;/P&gt;&lt;P&gt;2. if the answer to 1 is yes, How to power cycle the sd card for the case described above?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks again for your support.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Apr 2017 01:05:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/How-to-power-cycle-SD-card/m-p/631548#M2023</guid>
      <dc:creator>zalbassam</dc:creator>
      <dc:date>2017-04-05T01:05:02Z</dc:date>
    </item>
    <item>
      <title>Re: How to power cycle SD card?</title>
      <link>https://community.nxp.com/t5/Layerscape/How-to-power-cycle-SD-card/m-p/631549#M2024</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Actually I have the same question as Zaid as well.&amp;nbsp; Once the SD card is switched from 3.3V to 1.8V is there any way to switch it back?&amp;nbsp; For example ... if I want to operate at faster SD frequency I switch the card to 1.8V but let's say I want to go back to a slower frequency then how do I switch the card back to 3.3V ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thx&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 10 Apr 2017 13:12:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/How-to-power-cycle-SD-card/m-p/631549#M2024</guid>
      <dc:creator>kamhabs</dc:creator>
      <dc:date>2017-04-10T13:12:26Z</dc:date>
    </item>
    <item>
      <title>Re: How to power cycle SD card?</title>
      <link>https://community.nxp.com/t5/Layerscape/How-to-power-cycle-SD-card/m-p/631550#M2025</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;Do you use command sequence from the Section 3.9.4 of the &lt;SPAN style="background: white;"&gt;SD spec 4.01&lt;/SPAN&gt;?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Pavel Chubakov&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Apr 2017 11:04:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/How-to-power-cycle-SD-card/m-p/631550#M2025</guid>
      <dc:creator>Pavel</dc:creator>
      <dc:date>2017-04-12T11:04:22Z</dc:date>
    </item>
    <item>
      <title>Re: How to power cycle SD card?</title>
      <link>https://community.nxp.com/t5/Layerscape/How-to-power-cycle-SD-card/m-p/631551#M2026</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes! and it works with:&lt;/P&gt;&lt;P&gt;- Cold restart (unplug and replug the power cable) while the card is in the slot.&lt;/P&gt;&lt;P&gt;- Removed and inserted the card.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;That means the command sequence is correct. no?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It does NOT work when:&lt;/P&gt;&lt;P&gt;- The board is warm restarted (by writing RESET_REQ in the RSTCR register, or pressing the reset button) while the card is in slot.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Apr 2017 11:58:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/How-to-power-cycle-SD-card/m-p/631551#M2026</guid>
      <dc:creator>zalbassam</dc:creator>
      <dc:date>2017-04-12T11:58:36Z</dc:date>
    </item>
    <item>
      <title>Re: How to power cycle SD card?</title>
      <link>https://community.nxp.com/t5/Layerscape/How-to-power-cycle-SD-card/m-p/631552#M2027</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Could you create service request about this problem? See the following page:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/381898"&gt;How I could create a Service Request?&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Add link to this Community (&lt;A href="https://community.nxp.com/thread/448086"&gt;How to power cycle SD card?&lt;/A&gt;) in this service request.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Pavel Chubakov&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Apr 2017 01:47:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/How-to-power-cycle-SD-card/m-p/631552#M2027</guid>
      <dc:creator>Pavel</dc:creator>
      <dc:date>2017-04-13T01:47:23Z</dc:date>
    </item>
  </channel>
</rss>