<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LayerscapeのトピックRe: LS1021A-TWR: Missing eth devices</title>
    <link>https://community.nxp.com/t5/Layerscape/LS1021A-TWR-Missing-eth-devices/m-p/614887#M1808</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;A _jive_internal="true" data-content-finding="Community" data-userid="30650" data-username="z.v" href="https://community.nxp.com/people/z.v"&gt;Vered Zvi&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have your tried whether Yocto Kernel worked fine with your built rootfs filesystem?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Would you please provide you Kernel 4.1.13&amp;nbsp; boot up console log?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yiping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 16 Jan 2017 09:00:05 GMT</pubDate>
    <dc:creator>yipingwang</dc:creator>
    <dc:date>2017-01-16T09:00:05Z</dc:date>
    <item>
      <title>LS1021A-TWR: Missing eth devices</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1021A-TWR-Missing-eth-devices/m-p/614886#M1807</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I compiled kernel 4.1.13 with ls1021a_defconfig.&lt;/P&gt;&lt;P&gt;The root file system is busybox 1.25.1.&lt;/P&gt;&lt;P&gt;For some reason, there are no eth devices. Only 'lo'&lt;/P&gt;&lt;P&gt;Can you explain why ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;With Yokto's kernel, it works fine.&lt;/P&gt;&lt;P&gt;I want to use a newer kernel from kernel.org&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Z.V&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 13 Jan 2017 11:10:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1021A-TWR-Missing-eth-devices/m-p/614886#M1807</guid>
      <dc:creator>z_v</dc:creator>
      <dc:date>2017-01-13T11:10:34Z</dc:date>
    </item>
    <item>
      <title>Re: LS1021A-TWR: Missing eth devices</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1021A-TWR-Missing-eth-devices/m-p/614887#M1808</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;A _jive_internal="true" data-content-finding="Community" data-userid="30650" data-username="z.v" href="https://community.nxp.com/people/z.v"&gt;Vered Zvi&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have your tried whether Yocto Kernel worked fine with your built rootfs filesystem?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Would you please provide you Kernel 4.1.13&amp;nbsp; boot up console log?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yiping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 16 Jan 2017 09:00:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1021A-TWR-Missing-eth-devices/m-p/614887#M1808</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2017-01-16T09:00:05Z</dc:date>
    </item>
    <item>
      <title>Re: LS1021A-TWR: Missing eth devices</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1021A-TWR-Missing-eth-devices/m-p/614888#M1809</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN class=""&gt;Hello &lt;A _jive_internal="true" class="" data-containerid="-1" data-containertype="-1" data-content-finding="Community" data-objectid="30650" data-objecttype="3" href="https://community.nxp.com/people/z.v"&gt;Vered Zvi&lt;/A&gt;,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;As I answered you previously, please use the following procedure to build Linux Kernel image manually.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;I assume that you have already installed the standalone Toolchain provided in SDK 2.0 ARMv7 Image ISO in the folder /opt/fsl-qoriq/2.0/.&lt;BR /&gt;1. Please execute the following commands to export CC and LD environment.&lt;BR /&gt;$source /opt/fsl-qoriq/2.0/environment-setup-cortexa7hf-vfp-neon-fsl-linux-gnueabi&lt;BR /&gt;2. Go to Kernel source folder, configure Linux Kernel&lt;BR /&gt;$ cp arch/arm/configs/ls1021a_defconfig&amp;nbsp;&amp;nbsp;&amp;nbsp; .config&lt;BR /&gt;Configure Kernel according your requirement and save the configuration&lt;BR /&gt;$ make ARCH=arm menuconfig&lt;BR /&gt;3. Build uImage with the following command, and get uImage in the folder arch/arm/boot/.&lt;BR /&gt;$ make -j 4 uImage ARCH=arm LOADADDR=0x80008000&lt;BR /&gt;4. Build dtb file, and get the file ls1021a-twr.dtb in the folder arch/arm/boot/dts/.&lt;BR /&gt;$ make ARCH=arm ls1021a-twr.dtb&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;If your problem remains, please provide the whole UART console log.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yiping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 22 Jan 2017 05:09:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1021A-TWR-Missing-eth-devices/m-p/614888#M1809</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2017-01-22T05:09:05Z</dc:date>
    </item>
  </channel>
</rss>