<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Which pin used RTC or TA_BB_RTC used for WDOG for LS1043ARDB and SDK 2.0? in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/Which-pin-used-RTC-or-TA-BB-RTC-used-for-WDOG-for-LS1043ARDB-and/m-p/609288#M1750</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Chapter 39 of RM LS1021&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Watchdog Timer (WDOG) All WDOG modules use 32 KHz clock, driven at device input RTC or TA_BB_RTC pin for their counters. The WDOG uses the low frequency reference clock (RTC) for its counter and control operations. The low frequency reference clock is a free-running clock and can't be gated.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is this the case for the LS1043ARDB and is it the RTC or the TA_BB_RTC pins that are used for the LS1043ARDB, and which pin does the SDK 2.0 support for the LS1043ARDB for the counters for the WDOG modules?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 22 Mar 2017 11:31:37 GMT</pubDate>
    <dc:creator>tracysmith</dc:creator>
    <dc:date>2017-03-22T11:31:37Z</dc:date>
    <item>
      <title>Which pin used RTC or TA_BB_RTC used for WDOG for LS1043ARDB and SDK 2.0?</title>
      <link>https://community.nxp.com/t5/Layerscape/Which-pin-used-RTC-or-TA-BB-RTC-used-for-WDOG-for-LS1043ARDB-and/m-p/609288#M1750</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Chapter 39 of RM LS1021&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Watchdog Timer (WDOG) All WDOG modules use 32 KHz clock, driven at device input RTC or TA_BB_RTC pin for their counters. The WDOG uses the low frequency reference clock (RTC) for its counter and control operations. The low frequency reference clock is a free-running clock and can't be gated.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is this the case for the LS1043ARDB and is it the RTC or the TA_BB_RTC pins that are used for the LS1043ARDB, and which pin does the SDK 2.0 support for the LS1043ARDB for the counters for the WDOG modules?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Mar 2017 11:31:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Which-pin-used-RTC-or-TA-BB-RTC-used-for-WDOG-for-LS1043ARDB-and/m-p/609288#M1750</guid>
      <dc:creator>tracysmith</dc:creator>
      <dc:date>2017-03-22T11:31:37Z</dc:date>
    </item>
    <item>
      <title>Re: Which pin used RTC or TA_BB_RTC used for WDOG for LS1043ARDB and SDK 2.0?</title>
      <link>https://community.nxp.com/t5/Layerscape/Which-pin-used-RTC-or-TA-BB-RTC-used-for-WDOG-for-LS1043ARDB-and/m-p/609289#M1751</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;WDOG receives a clock which is ORed version of TA_BB_RTC and RTC - please refer to the QorIQ LS1043A Reference Manual, Figure 4-7. Clock subsystem block diagram - IP modules.&lt;/P&gt;&lt;P&gt;On the LS1043ARDB the 32 KHz clock is applied to both inputs TA_BB_RTC and RTC.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 Mar 2017 03:01:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Which-pin-used-RTC-or-TA-BB-RTC-used-for-WDOG-for-LS1043ARDB-and/m-p/609289#M1751</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2017-03-23T03:01:50Z</dc:date>
    </item>
  </channel>
</rss>