<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LayerscapeのトピックLX2160A - Synchronous Ethernet (SyncE) RCLK</title>
    <link>https://community.nxp.com/t5/Layerscape/LX2160A-Synchronous-Ethernet-SyncE-RCLK/m-p/2407819#M16834</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm using an LX2160A board.&lt;/P&gt;&lt;P&gt;From my understanding, the SerDes modules can use Synchronous Ethernet (SyncE) and recover the clock from the input SerDes signal. This clock is then available as RCLK0/1, with the related SerDes being selected with the register&amp;nbsp;RECOV_CLK_SEL_RCLK0/1.&lt;/P&gt;&lt;P&gt;Can this recovered clock signal then be used to drive the SerDes modules, either the one that it was recovered from or another ?&lt;BR /&gt;Potentially as reference clock for the PLLS / PLLF ?&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;</description>
    <pubDate>Mon, 24 Aug 2026 13:18:09 GMT</pubDate>
    <dc:creator>fdekeers</dc:creator>
    <dc:date>2026-08-24T13:18:09Z</dc:date>
    <item>
      <title>LX2160A - Synchronous Ethernet (SyncE) RCLK</title>
      <link>https://community.nxp.com/t5/Layerscape/LX2160A-Synchronous-Ethernet-SyncE-RCLK/m-p/2407819#M16834</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm using an LX2160A board.&lt;/P&gt;&lt;P&gt;From my understanding, the SerDes modules can use Synchronous Ethernet (SyncE) and recover the clock from the input SerDes signal. This clock is then available as RCLK0/1, with the related SerDes being selected with the register&amp;nbsp;RECOV_CLK_SEL_RCLK0/1.&lt;/P&gt;&lt;P&gt;Can this recovered clock signal then be used to drive the SerDes modules, either the one that it was recovered from or another ?&lt;BR /&gt;Potentially as reference clock for the PLLS / PLLF ?&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;</description>
      <pubDate>Mon, 24 Aug 2026 13:18:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LX2160A-Synchronous-Ethernet-SyncE-RCLK/m-p/2407819#M16834</guid>
      <dc:creator>fdekeers</dc:creator>
      <dc:date>2026-08-24T13:18:09Z</dc:date>
    </item>
    <item>
      <title>Re: LX2160A - Synchronous Ethernet (SyncE) RCLK</title>
      <link>https://community.nxp.com/t5/Layerscape/LX2160A-Synchronous-Ethernet-SyncE-RCLK/m-p/2408259#M16835</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;No, RCLK0/1 cannot be fed directly back into the LX2160A SerDes as a reference clock for PLLS/PLLF. RCLK0 and RCLK1 are output-only pins on the LX2160A. &lt;A id="base-ui-:r17s:" class="wdbi343 wdbi341 _1ibi0s3ec _1ibi0s376" tabindex="0" role="button" href="https://nxp.lightning.force.com/lightning/r/Case/5002p00002SE9IMAA1/view" rel="noreferrer" aria-expanded="false" aria-haspopup="dialog" data-base-ui-click-trigger="" data-label="1" aria-label="Citation 1" target="_blank"&gt;&lt;/A&gt;The intended SyncE architecture requires routing RCLK0/1 through an external Jitter-Cleaner PLL first, and only then feeding the cleaned clock back as the SerDes reference clock (SD1_PLLS_REF_CLK_P/N, etc.).&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Tue, 25 Aug 2026 14:22:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LX2160A-Synchronous-Ethernet-SyncE-RCLK/m-p/2408259#M16835</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2026-08-25T14:22:42Z</dc:date>
    </item>
  </channel>
</rss>