<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: CodeWarrior for LA1224 plugin in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/CodeWarrior-for-LA1224-plugin/m-p/2403599#M16830</link>
    <description>&lt;P&gt;Please download pack&amp;nbsp;com.freescale.armv8.11.5.15.E200.INT.Win.updatesite.230810 1.zip from the following link.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://support.nxp.com/s/case/500Te00000eF7lOIAS/community-codewarrior-for-la1224-plugin?language=en_US" target="_blank"&gt;https://support.nxp.com/s/case/500Te00000eF7lOIAS/community-codewarrior-for-la1224-plugin?language=en_US&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Please prepare a clean installation environment. Please install&amp;nbsp;CW_ARMv8_v2020.06_b200629GA_Win_Offline.exe first. Then open CodeWarrior IDE in a new worksapce path. Then install the service pack&amp;nbsp;com.freescale.armv8.11.5.15.E200.INT.Win.updatesite.230810 1.zip from&amp;nbsp;Help-&amp;gt;Install New Software-&amp;gt;Add-&amp;gt;Archive in CodeWarrior IDE.&lt;/P&gt;</description>
    <pubDate>Tue, 11 Aug 2026 09:10:14 GMT</pubDate>
    <dc:creator>yipingwang</dc:creator>
    <dc:date>2026-08-11T09:10:14Z</dc:date>
    <item>
      <title>CodeWarrior for LA1224 plugin</title>
      <link>https://community.nxp.com/t5/Layerscape/CodeWarrior-for-LA1224-plugin/m-p/2401781#M16818</link>
      <description>&lt;P&gt;Hello,&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;I am currently In the middle of evaluating&amp;nbsp;LA1224-RDB and I have some questions regarding the software environment. As I understand I can have a Linux app running on the existing NxP image on LX2160A for evaluation purposes. Furthermore I suppose LA1224 is running baremetal with freertos. I saw that I can have firmware for LA1224 in a Linux directory on the LX2160A. Is this given from NxP? What does it support? I suppose that if I want to develop something further than the given firmware I have to get a codewarrior license and TAP.&lt;BR /&gt;&lt;BR /&gt;I have downloaded CW_ARMv8_v2020.06_b200629GA_Win_Setup.exe however the LP1224 is not available. After searching the NxP site I read that I need an extra toolchain on top of CW_ARMv8. What is the full url to download the add on?&amp;nbsp; I read&amp;nbsp;&lt;A href="https://community.nxp.com/t5/Layerscape/CodeWarrior-for-LA1224/m-p/2107181" target="_blank"&gt;CodeWarrior for LA1224&lt;/A&gt;&amp;nbsp;and only a partial url is given "&lt;SPAN&gt;com.freescale.armv8.11.5.15.E200.INT.Win.updatesite.230810 1.zip"&lt;BR /&gt;&lt;BR /&gt;Any further information on how to work on those processors is welcome.&lt;BR /&gt;&lt;BR /&gt;Kind Regards&lt;BR /&gt;N. Alexopoulos&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 04 Aug 2026 09:41:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/CodeWarrior-for-LA1224-plugin/m-p/2401781#M16818</guid>
      <dc:creator>nalexopo</dc:creator>
      <dc:date>2026-08-04T09:41:56Z</dc:date>
    </item>
    <item>
      <title>Re: CodeWarrior for LA1224 plugin</title>
      <link>https://community.nxp.com/t5/Layerscape/CodeWarrior-for-LA1224-plugin/m-p/2403599#M16830</link>
      <description>&lt;P&gt;Please download pack&amp;nbsp;com.freescale.armv8.11.5.15.E200.INT.Win.updatesite.230810 1.zip from the following link.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://support.nxp.com/s/case/500Te00000eF7lOIAS/community-codewarrior-for-la1224-plugin?language=en_US" target="_blank"&gt;https://support.nxp.com/s/case/500Te00000eF7lOIAS/community-codewarrior-for-la1224-plugin?language=en_US&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Please prepare a clean installation environment. Please install&amp;nbsp;CW_ARMv8_v2020.06_b200629GA_Win_Offline.exe first. Then open CodeWarrior IDE in a new worksapce path. Then install the service pack&amp;nbsp;com.freescale.armv8.11.5.15.E200.INT.Win.updatesite.230810 1.zip from&amp;nbsp;Help-&amp;gt;Install New Software-&amp;gt;Add-&amp;gt;Archive in CodeWarrior IDE.&lt;/P&gt;</description>
      <pubDate>Tue, 11 Aug 2026 09:10:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/CodeWarrior-for-LA1224-plugin/m-p/2403599#M16830</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2026-08-11T09:10:14Z</dc:date>
    </item>
  </channel>
</rss>