<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LA1224 FR1/FR2 Test Tool (v5.1): Using Option8 time-domain injection for single-carrier waveform in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/LA1224-FR1-FR2-Test-Tool-v5-1-Using-Option8-time-domain/m-p/2366917#M16695</link>
    <description>&lt;P&gt;Hello! If you replace the file generated in the time domain with Fs 491.52 MHz, will the DUC x4 work up to 1966.08 MHz on the VSPA?&lt;BR /&gt;I believe you need to generate a time domain signal with the same Fs frequency as the DAC, i.e., 1966.08 MHz.&lt;/P&gt;</description>
    <pubDate>Mon, 18 May 2026 12:04:08 GMT</pubDate>
    <dc:creator>flappy</dc:creator>
    <dc:date>2026-05-18T12:04:08Z</dc:date>
    <item>
      <title>LA1224 FR1/FR2 Test Tool (v5.1): Using Option8 time-domain injection for single-carrier waveform</title>
      <link>https://community.nxp.com/t5/Layerscape/LA1224-FR1-FR2-Test-Tool-v5-1-Using-Option8-time-domain/m-p/2326708#M16559</link>
      <description>&lt;P&gt;LA1224 FR1/FR2 Test Tool (v5.1): Using Option8 time-domain injection for single-carrier waveform – is a dedicated image/kernel configuration required?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Hi NXP team,&lt;/P&gt;&lt;P&gt;I’m using LA1224-RDB-BHS with FR1/FR2 Test Tool v5.1 and VSPA images in this tool（e.g., MEvspa_images_HS.2T2R_400M_120K_1966_1966_TDDFDD） to validate FR2 single-carrier (SC) waveform transmission in Option8 time-domain mode. I’m using SMA cables with the LA1224-FR2-BRK to loop back the TX to RX on a single LA1224-RDB-BHS device.&lt;/P&gt;&lt;P&gt;Steps I performed:&lt;BR /&gt;1. Generate a 10 ms complex IQ waveform at 491.52 Msps (int16 IQ interleaved), file size 19,660,800 bytes.&lt;BR /&gt;2. Load it via:&lt;BR /&gt;./boot_vspa.sh MEvspa_images_HS.2T2R_400M_120K_1966_1966_TDDFDD&lt;BR /&gt;./channels_start.sh 4&lt;BR /&gt;./set_dfe_state.sh 4 normal&lt;BR /&gt;./update_test_vector.sh my_waveform_10ms.bin&lt;BR /&gt;./dump_time_domain_tx.sh 4&lt;BR /&gt;./dump_time_domain_rx.sh 4&lt;/P&gt;&lt;P&gt;Dumps obtained:&lt;BR /&gt;- TX dump: tx_timedomain_20ms_1966080ksps_dump_ant4.bin (Fs=1.96608 Gsps)&lt;BR /&gt;- RX dump: rx_timedomain_20ms_983040ksps_dump_ant4.bin (Fs=983.04 Msps)&lt;/P&gt;&lt;P&gt;I performed MATLAB correlation-based alignment and best-window comparison.&lt;/P&gt;&lt;P&gt;Observations:&lt;BR /&gt;- Correlation peak scores are very high (e.g., ~0.998), so the injected waveform is definitely being transmitted and received.&lt;BR /&gt;- However, the measured EVM between my reference waveform (A) and TX dump (B) is not negligible:&lt;BR /&gt;- For PN/BPSK + RRC test waveform: A→B EVM ≈ 6.75% (NMSE ≈ -23.4 dB)&lt;BR /&gt;- For another SC waveform: A→B EVM ≈ 22.8%&lt;BR /&gt;- Disabling some kernels does not change EVM significantly:&lt;BR /&gt;./kernels_disable_tx.sh 4 qec cfr dpd&lt;BR /&gt;./update_fine_cfo_nco_freq.sh 4 0&lt;BR /&gt;(EVM/NMSE nearly unchanged)&lt;/P&gt;&lt;P&gt;Questions:&lt;BR /&gt;1. For single-carrier FR2 validation, is the provided VSPA image (with OFDM SCS-based naming) still appropriate, or is there a dedicated single-carrier optimized image?&lt;BR /&gt;2. In Option8 time-domain injection, are upsampling/downsampling/CFO/QEC kernels always in the processing chain? Is there a supported way to bypass them (or guarantee “transparent pass-through”) for SC waveform testing?&lt;BR /&gt;3. What is the expected EVM floor between (A) injected waveform and (B) TX dump in this setup? Is ~6–7% reasonable due to fixed-point/filtering, or does it indicate a misconfiguration?&lt;/P&gt;&lt;P&gt;I can provide exact scripts, config, and waveforms if needed.&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;</description>
      <pubDate>Thu, 05 Mar 2026 03:40:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LA1224-FR1-FR2-Test-Tool-v5-1-Using-Option8-time-domain/m-p/2326708#M16559</guid>
      <dc:creator>SakuraAhua</dc:creator>
      <dc:date>2026-03-05T03:40:44Z</dc:date>
    </item>
    <item>
      <title>Re: LA1224 FR1/FR2 Test Tool (v5.1): Using Option8 time-domain injection for single-carrier waveform</title>
      <link>https://community.nxp.com/t5/Layerscape/LA1224-FR1-FR2-Test-Tool-v5-1-Using-Option8-time-domain/m-p/2327438#M16561</link>
      <description>&lt;P style="margin: 0in; font-family: Calibri; font-size: 11.0pt;" lang="en-US"&gt;LA1224 support is not public.&lt;/P&gt;
&lt;P style="margin: 0in; font-family: Calibri; font-size: 11.0pt;" lang="en-US"&gt;If you need assistance, please create a case at the link below and attach your NDA:&lt;/P&gt;
&lt;P style="margin: 0in; font-family: Calibri; font-size: 11.0pt;" lang="en-US"&gt;&lt;A href="https://support.nxp.com/s/?language=en_US" target="_blank"&gt;https://support.nxp.com/s/?language=en_US&lt;/A&gt;&lt;/P&gt;
&lt;P style="margin: 0in; font-family: Calibri; font-size: 11.0pt;" lang="en-US"&gt;Thanks.&lt;/P&gt;</description>
      <pubDate>Fri, 06 Mar 2026 02:12:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LA1224-FR1-FR2-Test-Tool-v5-1-Using-Option8-time-domain/m-p/2327438#M16561</guid>
      <dc:creator>June_Lu</dc:creator>
      <dc:date>2026-03-06T02:12:22Z</dc:date>
    </item>
    <item>
      <title>Re: LA1224 FR1/FR2 Test Tool (v5.1): Using Option8 time-domain injection for single-carrier waveform</title>
      <link>https://community.nxp.com/t5/Layerscape/LA1224-FR1-FR2-Test-Tool-v5-1-Using-Option8-time-domain/m-p/2366917#M16695</link>
      <description>&lt;P&gt;Hello! If you replace the file generated in the time domain with Fs 491.52 MHz, will the DUC x4 work up to 1966.08 MHz on the VSPA?&lt;BR /&gt;I believe you need to generate a time domain signal with the same Fs frequency as the DAC, i.e., 1966.08 MHz.&lt;/P&gt;</description>
      <pubDate>Mon, 18 May 2026 12:04:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LA1224-FR1-FR2-Test-Tool-v5-1-Using-Option8-time-domain/m-p/2366917#M16695</guid>
      <dc:creator>flappy</dc:creator>
      <dc:date>2026-05-18T12:04:08Z</dc:date>
    </item>
  </channel>
</rss>