<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LayerscapeのトピックImproving Network Packet Processing Efficiency on QorIQ Systems</title>
    <link>https://community.nxp.com/t5/Layerscape/Improving-Network-Packet-Processing-Efficiency-on-QorIQ-Systems/m-p/2365731#M16690</link>
    <description>&lt;P&gt;We are currently using a QorIQ platform in a networking application where traffic load becomes fairly heavy during peak operation. The system itself is stable, but once throughput increases, CPU utilization rises faster than expected and packet latency becomes a little inconsistent.&lt;/P&gt;&lt;P&gt;After spending some time profiling the system, I found that a lot of the slowdown was coming from unnecessary memory copies and queue handling overhead. Reducing some of those operations helped more than I initially expected. I also noticed that cache behavior starts to matter quite a bit once traffic bursts become continuous.&lt;/P&gt;&lt;P&gt;Another thing that improved performance was distributing interrupts more carefully across cores instead of letting everything stack onto a single processing path.&lt;/P&gt;&lt;P&gt;The platform still performs well overall, but I am interested in hearing how others are optimizing packet processing efficiency on QorIQ or Layerscape systems, especially in low-latency or high-throughput&lt;/P&gt;</description>
    <pubDate>Thu, 14 May 2026 20:06:07 GMT</pubDate>
    <dc:creator>jeremiranner</dc:creator>
    <dc:date>2026-05-14T20:06:07Z</dc:date>
    <item>
      <title>Improving Network Packet Processing Efficiency on QorIQ Systems</title>
      <link>https://community.nxp.com/t5/Layerscape/Improving-Network-Packet-Processing-Efficiency-on-QorIQ-Systems/m-p/2365731#M16690</link>
      <description>&lt;P&gt;We are currently using a QorIQ platform in a networking application where traffic load becomes fairly heavy during peak operation. The system itself is stable, but once throughput increases, CPU utilization rises faster than expected and packet latency becomes a little inconsistent.&lt;/P&gt;&lt;P&gt;After spending some time profiling the system, I found that a lot of the slowdown was coming from unnecessary memory copies and queue handling overhead. Reducing some of those operations helped more than I initially expected. I also noticed that cache behavior starts to matter quite a bit once traffic bursts become continuous.&lt;/P&gt;&lt;P&gt;Another thing that improved performance was distributing interrupts more carefully across cores instead of letting everything stack onto a single processing path.&lt;/P&gt;&lt;P&gt;The platform still performs well overall, but I am interested in hearing how others are optimizing packet processing efficiency on QorIQ or Layerscape systems, especially in low-latency or high-throughput&lt;/P&gt;</description>
      <pubDate>Thu, 14 May 2026 20:06:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Improving-Network-Packet-Processing-Efficiency-on-QorIQ-Systems/m-p/2365731#M16690</guid>
      <dc:creator>jeremiranner</dc:creator>
      <dc:date>2026-05-14T20:06:07Z</dc:date>
    </item>
    <item>
      <title>Re: Improving Network Packet Processing Efficiency on QorIQ Systems</title>
      <link>https://community.nxp.com/t5/Layerscape/Improving-Network-Packet-Processing-Efficiency-on-QorIQ-Systems/m-p/2366269#M16692</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;Yes, on QorIQ/Layerscape, packet efficiency is typically optimized by preserving flow-to-core affinity, balancing queues and interrupts across cores, and reducing copies with scatter-gather/zero-copy paths, because those are the main levers NXP documents as improving CPU load, cache locality, and latency consistency.&lt;/P&gt;
&lt;P&gt;One important caveat from the retrieved material: I could find strong guidance on the mechanisms, but not a single universal “best” recipe for all QorIQ/Layerscape systems, because the right mix depends on whether you are running the Linux networking stack, DPAA private drivers, or DPDK/DPAA2 userspace, and on whether the bottleneck is copy overhead, hash skew, interrupt concentration, or queue imbalance. The documentation consistently points to queue/core symmetry, affinity preservation, and copy reduction as the highest-value first steps.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Fri, 15 May 2026 14:48:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Improving-Network-Packet-Processing-Efficiency-on-QorIQ-Systems/m-p/2366269#M16692</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2026-05-15T14:48:01Z</dc:date>
    </item>
  </channel>
</rss>