<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LayerscapeのトピックIssues with configuring TSN on the web interface for ls1028a</title>
    <link>https://community.nxp.com/t5/Layerscape/Issues-with-configuring-TSN-on-the-web-interface-for-ls1028a/m-p/2330997#M16574</link>
    <description>&lt;P&gt;&lt;SPAN&gt;I am planning to use the LS1028A to develop a TSN endpoint device. However, I found in the document REALTIMEEDGEUG.pdf that to configure TSN via the web interface, a PC needs to be connected to the eno0 interface of eneth. The problem is that I also need to use this interface as the endpoint interface to connect to an external switch. I would like to know if I can use the eno1 interface of eneth instead for the web-based configuration, or if I can connect a PC to one of the switch ports (swp0–4) to perform TSN configuration.&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Thu, 12 Mar 2026 03:04:43 GMT</pubDate>
    <dc:creator>LedHx</dc:creator>
    <dc:date>2026-03-12T03:04:43Z</dc:date>
    <item>
      <title>Issues with configuring TSN on the web interface for ls1028a</title>
      <link>https://community.nxp.com/t5/Layerscape/Issues-with-configuring-TSN-on-the-web-interface-for-ls1028a/m-p/2330997#M16574</link>
      <description>&lt;P&gt;&lt;SPAN&gt;I am planning to use the LS1028A to develop a TSN endpoint device. However, I found in the document REALTIMEEDGEUG.pdf that to configure TSN via the web interface, a PC needs to be connected to the eno0 interface of eneth. The problem is that I also need to use this interface as the endpoint interface to connect to an external switch. I would like to know if I can use the eno1 interface of eneth instead for the web-based configuration, or if I can connect a PC to one of the switch ports (swp0–4) to perform TSN configuration.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 12 Mar 2026 03:04:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Issues-with-configuring-TSN-on-the-web-interface-for-ls1028a/m-p/2330997#M16574</guid>
      <dc:creator>LedHx</dc:creator>
      <dc:date>2026-03-12T03:04:43Z</dc:date>
    </item>
    <item>
      <title>Re: Issues with configuring TSN on the web interface for ls1028a</title>
      <link>https://community.nxp.com/t5/Layerscape/Issues-with-configuring-TSN-on-the-web-interface-for-ls1028a/m-p/2331084#M16575</link>
      <description>&lt;P&gt;Will you use&amp;nbsp;&lt;SPAN data-teams="true"&gt;NETCONF/YANG to setup the TSN? Thanks&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 12 Mar 2026 06:45:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Issues-with-configuring-TSN-on-the-web-interface-for-ls1028a/m-p/2331084#M16575</guid>
      <dc:creator>June_Lu</dc:creator>
      <dc:date>2026-03-12T06:45:43Z</dc:date>
    </item>
    <item>
      <title>Re: Issues with configuring TSN on the web interface for ls1028a</title>
      <link>https://community.nxp.com/t5/Layerscape/Issues-with-configuring-TSN-on-the-web-interface-for-ls1028a/m-p/2332044#M16582</link>
      <description>Yes, I intend to use NETCONF/YANG to configure the TSN features on Ethernet. However, the manual mentions that web-based configuration requires the eno0 interface, which I plan to use for connecting to an external switch. Since the development board is still in procurement, I currently don’t have access to the necessary hardware.</description>
      <pubDate>Fri, 13 Mar 2026 01:04:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Issues-with-configuring-TSN-on-the-web-interface-for-ls1028a/m-p/2332044#M16582</guid>
      <dc:creator>LedHx</dc:creator>
      <dc:date>2026-03-13T01:04:40Z</dc:date>
    </item>
    <item>
      <title>Re: Issues with configuring TSN on the web interface for ls1028a</title>
      <link>https://community.nxp.com/t5/Layerscape/Issues-with-configuring-TSN-on-the-web-interface-for-ls1028a/m-p/2332069#M16583</link>
      <description>&lt;P style="margin: 0in; line-height: 15pt; font-family: 'Segoe UI'; font-size: 10.5pt;"&gt;Will you use the LS1028ARDB evaluation board, or will you design a custom board for your application?&lt;/P&gt;
&lt;P style="margin: 0in; line-height: 15pt; font-family: 'Segoe UI'; font-size: 10.5pt;"&gt;Thank you.&lt;/P&gt;</description>
      <pubDate>Fri, 13 Mar 2026 02:00:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Issues-with-configuring-TSN-on-the-web-interface-for-ls1028a/m-p/2332069#M16583</guid>
      <dc:creator>June_Lu</dc:creator>
      <dc:date>2026-03-13T02:00:19Z</dc:date>
    </item>
    <item>
      <title>Re: Issues with configuring TSN on the web interface for ls1028a</title>
      <link>https://community.nxp.com/t5/Layerscape/Issues-with-configuring-TSN-on-the-web-interface-for-ls1028a/m-p/2332075#M16584</link>
      <description>LS1028ARDB evaluation board</description>
      <pubDate>Fri, 13 Mar 2026 02:02:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Issues-with-configuring-TSN-on-the-web-interface-for-ls1028a/m-p/2332075#M16584</guid>
      <dc:creator>LedHx</dc:creator>
      <dc:date>2026-03-13T02:02:21Z</dc:date>
    </item>
    <item>
      <title>Re: Issues with configuring TSN on the web interface for ls1028a</title>
      <link>https://community.nxp.com/t5/Layerscape/Issues-with-configuring-TSN-on-the-web-interface-for-ls1028a/m-p/2336631#M16592</link>
      <description>&lt;P style="margin: 0in; font-family: Calibri; font-size: 11.0pt;" lang="en-US"&gt;After discussing with the internal team, we recommend using eno0 as the management interface for TSN configuration.&lt;/P&gt;
&lt;P style="margin: 0in; font-family: Calibri; font-size: 11.0pt;" lang="en-US"&gt;The eno1 port is not routed to an external connector on the LS1028ARDB and therefore cannot be used.&lt;/P&gt;
&lt;P style="margin: 0in; font-family: Calibri; font-size: 11.0pt;"&gt;&lt;SPAN&gt;Although the switch ports (swp0&lt;/SPAN&gt;&lt;SPAN&gt;–&lt;/SPAN&gt;&lt;SPAN&gt;swp4) can be accessed if configured, using them as the management port may restrict some TSN features on that same port.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P style="margin: 0in; font-family: Calibri; font-size: 11.0pt;" lang="en-US"&gt;Thanks.&lt;/P&gt;</description>
      <pubDate>Fri, 20 Mar 2026 10:36:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Issues-with-configuring-TSN-on-the-web-interface-for-ls1028a/m-p/2336631#M16592</guid>
      <dc:creator>June_Lu</dc:creator>
      <dc:date>2026-03-20T10:36:46Z</dc:date>
    </item>
  </channel>
</rss>