<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic LX2080/2160,Serial port in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/LX2080-2160-Serial-port/m-p/2324602#M16530</link>
    <description>&lt;P&gt;&lt;SPAN&gt;LX2080 processor. Among a batch of boards, only one exhibits probabilistic gibberish on the serial port at power-on, while the others function normally. What could be the cause of this issue, and where should troubleshooting begin?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;thanks!&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Sat, 28 Feb 2026 07:32:45 GMT</pubDate>
    <dc:creator>YY2410</dc:creator>
    <dc:date>2026-02-28T07:32:45Z</dc:date>
    <item>
      <title>LX2080/2160,Serial port</title>
      <link>https://community.nxp.com/t5/Layerscape/LX2080-2160-Serial-port/m-p/2324602#M16530</link>
      <description>&lt;P&gt;&lt;SPAN&gt;LX2080 processor. Among a batch of boards, only one exhibits probabilistic gibberish on the serial port at power-on, while the others function normally. What could be the cause of this issue, and where should troubleshooting begin?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;thanks!&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Sat, 28 Feb 2026 07:32:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LX2080-2160-Serial-port/m-p/2324602#M16530</guid>
      <dc:creator>YY2410</dc:creator>
      <dc:date>2026-02-28T07:32:45Z</dc:date>
    </item>
    <item>
      <title>Re: LX2080/2160,Serial port</title>
      <link>https://community.nxp.com/t5/Layerscape/LX2080-2160-Serial-port/m-p/2325493#M16546</link>
      <description>&lt;P&gt;If only &lt;STRONG&gt;one&lt;/STRONG&gt; LX2080-based board in a batch shows &lt;STRONG&gt;probabilistic gibberish on the serial port at power‑on&lt;/STRONG&gt;, while all others behave normally, the issue is almost certainly &lt;STRONG&gt;hardware‑related&lt;/STRONG&gt;, not firmware‑related.&lt;/P&gt;
&lt;P&gt;Below are the &lt;STRONG&gt;most common root causes&lt;/STRONG&gt; and &lt;STRONG&gt;where to start troubleshooting&lt;/STRONG&gt;—ranked by likelihood based on similar FPGA/SoC/MCU board behavior.&lt;/P&gt;
&lt;P&gt;&lt;STRONG&gt;Most Likely Root Causes&lt;/STRONG&gt;&lt;/P&gt;
&lt;OL&gt;
&lt;LI&gt;&lt;STRONG&gt; UART clock source instability (crystal / oscillator issue)&lt;/STRONG&gt;&lt;/LI&gt;
&lt;/OL&gt;
&lt;P&gt;If the CPU/UART clock is unstable at early boot, the UART baud rate is wrong temporarily → resulting in random characters.&lt;/P&gt;
&lt;P&gt;Common suspects:&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;A defective &lt;STRONG&gt;crystal oscillator&lt;/STRONG&gt; (main XO or UART-related PLL reference).&lt;/LI&gt;
&lt;LI&gt;Bad solder joints → intermittent oscillation.&lt;/LI&gt;
&lt;LI&gt;Wrong or drifting load capacitors.&lt;/LI&gt;
&lt;LI&gt;Power‑on ramp too slow for the oscillator.&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;OL start="2"&gt;
&lt;LI&gt;&lt;STRONG&gt; Power rail instability at startup&lt;/STRONG&gt;&lt;/LI&gt;
&lt;/OL&gt;
&lt;P&gt;If core/IO power rails dip or ramp too slowly, early‑boot logic runs unstable.&lt;/P&gt;
&lt;P&gt;Possible issues:&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;Bad PMIC / DC‑DC converter.&lt;/LI&gt;
&lt;LI&gt;Bad LDO on that board.&lt;/LI&gt;
&lt;LI&gt;Weak or damaged decoupling capacitor (missing, broken, wrong value).&lt;/LI&gt;
&lt;LI&gt;Inrush current different from other boards.&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;UART is often among the first peripherals to show instability.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;OL start="3"&gt;
&lt;LI&gt;&lt;STRONG&gt; Poor soldering on the LX2080 or surrounding passives&lt;/STRONG&gt;&lt;/LI&gt;
&lt;/OL&gt;
&lt;P&gt;Symptoms:&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;Intermittent TX pin drive.&lt;/LI&gt;
&lt;LI&gt;Clock pin or reset pin connection intermittent.&lt;/LI&gt;
&lt;LI&gt;Unstable boot ROM execution.&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;Causes:&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;BGA solder voids / cold joints.&lt;/LI&gt;
&lt;LI&gt;Marginally soldered passives around the UART or oscillator.&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;This explains the &lt;STRONG&gt;probabilistic&lt;/STRONG&gt; nature.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;OL start="4"&gt;
&lt;LI&gt;&lt;STRONG&gt; Reset circuit not meeting timing&lt;/STRONG&gt;&lt;/LI&gt;
&lt;/OL&gt;
&lt;P&gt;If reset is released too early or bounces, the chip may start running before power/clock is fully stable.&lt;/P&gt;
&lt;P&gt;Check:&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;Reset supervisor IC&lt;/LI&gt;
&lt;LI&gt;Reset pull-up/pull-down resistors&lt;/LI&gt;
&lt;LI&gt;RC delay components&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;OL start="5"&gt;
&lt;LI&gt;&lt;STRONG&gt; Damaged or marginal UART transceiver (if external)&lt;/STRONG&gt;&lt;/LI&gt;
&lt;/OL&gt;
&lt;P&gt;If the board uses:&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;RS‑232 transceiver (e.g., MAX3232)&lt;/LI&gt;
&lt;LI&gt;USB‑to‑UART chip (e.g., CP2102, CH340, FT232) any marginal chip can scramble output.&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;Common symptoms:&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;Random characters.&lt;/LI&gt;
&lt;LI&gt;Works sometimes after multiple power cycles.&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 03 Mar 2026 09:07:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LX2080-2160-Serial-port/m-p/2325493#M16546</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2026-03-03T09:07:55Z</dc:date>
    </item>
  </channel>
</rss>