<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic LS1021A-TWR  - No ethernet devices under linux in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/LS1021A-TWR-No-ethernet-devices-under-linux/m-p/601242#M1647</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I built kernel 4.1.13 for LS1021A and ran it on the TWR.&amp;nbsp;&lt;/P&gt;&lt;P&gt;The root file system is busybox and the dtb is &lt;STRONG&gt;identical&lt;/STRONG&gt; to the one used in Yocto project provided by NXP.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Under u-boot, all 3 ethernet devices work fine.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Under linux, I can see only the "lo" device.&lt;/P&gt;&lt;P&gt;Is there any component I should add to the linux configuration ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The 4.1.13 is a vanilla kernel from kernel.org patched so I can run:&lt;/P&gt;&lt;P&gt;make ls1021a_defconfig&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Z.V&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 10 Jan 2017 02:25:06 GMT</pubDate>
    <dc:creator>z_v</dc:creator>
    <dc:date>2017-01-10T02:25:06Z</dc:date>
    <item>
      <title>LS1021A-TWR  - No ethernet devices under linux</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1021A-TWR-No-ethernet-devices-under-linux/m-p/601242#M1647</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I built kernel 4.1.13 for LS1021A and ran it on the TWR.&amp;nbsp;&lt;/P&gt;&lt;P&gt;The root file system is busybox and the dtb is &lt;STRONG&gt;identical&lt;/STRONG&gt; to the one used in Yocto project provided by NXP.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Under u-boot, all 3 ethernet devices work fine.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Under linux, I can see only the "lo" device.&lt;/P&gt;&lt;P&gt;Is there any component I should add to the linux configuration ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The 4.1.13 is a vanilla kernel from kernel.org patched so I can run:&lt;/P&gt;&lt;P&gt;make ls1021a_defconfig&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Z.V&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 10 Jan 2017 02:25:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1021A-TWR-No-ethernet-devices-under-linux/m-p/601242#M1647</guid>
      <dc:creator>z_v</dc:creator>
      <dc:date>2017-01-10T02:25:06Z</dc:date>
    </item>
  </channel>
</rss>