<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Layerscape中的主题 LX2160A DDR memory connections</title>
    <link>https://community.nxp.com/t5/Layerscape/LX2160A-DDR-memory-connections/m-p/2305059#M16435</link>
    <description>&lt;P&gt;Regarding DDR memory connections to the LX2160A&lt;/P&gt;&lt;P&gt;I'm considering connecting nine 8-bit DDR4 memory modules (8 x 9 = 72 bits) to the LX2160, and dividing them into TOP and BOTTOM locations to minimize the implementation area.&lt;/P&gt;&lt;P&gt;In this case, would it be possible to use address mirroring to configure TOP = CS0 as five chips and BOTTOM = CS1 as four chips?&lt;/P&gt;</description>
    <pubDate>Tue, 03 Feb 2026 08:18:14 GMT</pubDate>
    <dc:creator>kurokawa</dc:creator>
    <dc:date>2026-02-03T08:18:14Z</dc:date>
    <item>
      <title>LX2160A DDR memory connections</title>
      <link>https://community.nxp.com/t5/Layerscape/LX2160A-DDR-memory-connections/m-p/2305059#M16435</link>
      <description>&lt;P&gt;Regarding DDR memory connections to the LX2160A&lt;/P&gt;&lt;P&gt;I'm considering connecting nine 8-bit DDR4 memory modules (8 x 9 = 72 bits) to the LX2160, and dividing them into TOP and BOTTOM locations to minimize the implementation area.&lt;/P&gt;&lt;P&gt;In this case, would it be possible to use address mirroring to configure TOP = CS0 as five chips and BOTTOM = CS1 as four chips?&lt;/P&gt;</description>
      <pubDate>Tue, 03 Feb 2026 08:18:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LX2160A-DDR-memory-connections/m-p/2305059#M16435</guid>
      <dc:creator>kurokawa</dc:creator>
      <dc:date>2026-02-03T08:18:14Z</dc:date>
    </item>
    <item>
      <title>Re: LX2160A DDR memory connections</title>
      <link>https://community.nxp.com/t5/Layerscape/LX2160A-DDR-memory-connections/m-p/2305203#M16436</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/214864"&gt;@kurokawa&lt;/a&gt;&lt;/P&gt;
&lt;P&gt;LX2160A supports DDR address mirroring.&lt;/P&gt;
&lt;P&gt;Asymmetric population (5 devices on CS0 and 4 devices on CS1) is not feasible.&lt;BR /&gt;Address mirroring should be applied in a balanced topology.&lt;BR /&gt;for the specific chip-selection, it should be 64-bit data width, not 8x 5-chip = 40-bits or 8x 4-chips = 32-bits&lt;/P&gt;
&lt;P&gt;there are 3 topologies:&lt;/P&gt;
&lt;P&gt;way 1: (single-controller and single-rank, without address mirroring)&lt;BR /&gt;TOP: 5 x8 DRAM parts for data + 1 x8 DRAM part for ECC with CS0&lt;BR /&gt;BOTTOM: 4 x8 DRAM parts for data with CS0&lt;/P&gt;
&lt;P&gt;way 2: (single-controller and dual-ranks, with address mirroring)&lt;BR /&gt;TOP: 4 x16 DRAM parts for data + 1 x16 DRAM part(only 8-bits used) for ECC with CS0 of DDRC1&lt;BR /&gt;BOTTOM: 4 x16 DRAM parts for data + 1 x16 DRAM part(only 8-bits used) for ECC with CS1 of DDRC1&lt;/P&gt;
&lt;P&gt;way 3 (dual-controllers and single-rank for better performance):&lt;BR /&gt;TOP: 4 x16 DRAM parts for data + 1 x16 DRAM part(only 8-bits used) for ECC with CS0 of DDRC1&lt;BR /&gt;BOTTOM: 4 x16 DRAM parts for data + 1 x16 DRAM part(only 8-bits used) for ECC with CS0 of DDRC2&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;if .mirrored_dimm = 1 in mocked SPD way in ATF, DDR driver sets DDR_SDRAM_CFG_2[MD_EN] = 1.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 04 Feb 2026 09:55:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LX2160A-DDR-memory-connections/m-p/2305203#M16436</guid>
      <dc:creator>shengzhou_liu</dc:creator>
      <dc:date>2026-02-04T09:55:52Z</dc:date>
    </item>
    <item>
      <title>Re: LX2160A DDR memory connections</title>
      <link>https://community.nxp.com/t5/Layerscape/LX2160A-DDR-memory-connections/m-p/2305265#M16437</link>
      <description>&lt;P&gt;Thank you for your reply.&lt;/P&gt;&lt;P&gt;Just to be sure, let me confirm way 2.&lt;/P&gt;&lt;P&gt;If using 8-bit chips and using one controller, is it possible to perform address mirroring by placing 9 chips on the TOP and 9 chips on the BOTTOM (18 chips in total)?&lt;/P&gt;</description>
      <pubDate>Tue, 03 Feb 2026 11:11:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LX2160A-DDR-memory-connections/m-p/2305265#M16437</guid>
      <dc:creator>kurokawa</dc:creator>
      <dc:date>2026-02-03T11:11:45Z</dc:date>
    </item>
    <item>
      <title>Re: LX2160A DDR memory connections</title>
      <link>https://community.nxp.com/t5/Layerscape/LX2160A-DDR-memory-connections/m-p/2306013#M16439</link>
      <description>&lt;P&gt;Yes, it is feasible to that using 8-bit chips and one controller to perform address mirroring by placing 9 chips on the TOP and 9 chips on the BOTTOM.&lt;/P&gt;
&lt;P&gt;But from the perspective of performance, the bandwidth performance of using dual-controllers with single-rank is better than that of using single-controller with dual-ranks.&lt;/P&gt;</description>
      <pubDate>Wed, 04 Feb 2026 09:57:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LX2160A-DDR-memory-connections/m-p/2306013#M16439</guid>
      <dc:creator>shengzhou_liu</dc:creator>
      <dc:date>2026-02-04T09:57:15Z</dc:date>
    </item>
  </channel>
</rss>