<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Booting U-Boot on an LS1043A-based board in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/Booting-U-Boot-on-an-LS1043A-based-board/m-p/600033#M1639</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Have you tried to update U-Boot using pre-built image from the SDK Images ISO?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 08 Sep 2016 03:39:29 GMT</pubDate>
    <dc:creator>ufedor</dc:creator>
    <dc:date>2016-09-08T03:39:29Z</dc:date>
    <item>
      <title>Booting U-Boot on an LS1043A-based board</title>
      <link>https://community.nxp.com/t5/Layerscape/Booting-U-Boot-on-an-LS1043A-based-board/m-p/600032#M1638</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We've got a new LS1043 based SBC and it's generally working well. We can get to the U-Boot prompt, boot Linux, etc. But in order to do this, we had to remove most of the functions in arch_cpu_init(). Specifically, we have to remove __asm_invalidate_dcache_all(), __asm_invalidate_tlb_all(), and early_mmu_setup(). This is our first ARM card, so I'm still getting up to speed on ARM, but I can't figure out why these things would cause the board to hang. We don't have an ARM JTAG debugger, so I haven't been able to look at exactly what's going wrong. Anyone got any suggestions?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;John&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 07 Sep 2016 23:25:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Booting-U-Boot-on-an-LS1043A-based-board/m-p/600032#M1638</guid>
      <dc:creator>johnschmoller</dc:creator>
      <dc:date>2016-09-07T23:25:44Z</dc:date>
    </item>
    <item>
      <title>Re: Booting U-Boot on an LS1043A-based board</title>
      <link>https://community.nxp.com/t5/Layerscape/Booting-U-Boot-on-an-LS1043A-based-board/m-p/600033#M1639</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Have you tried to update U-Boot using pre-built image from the SDK Images ISO?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 08 Sep 2016 03:39:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Booting-U-Boot-on-an-LS1043A-based-board/m-p/600033#M1639</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2016-09-08T03:39:29Z</dc:date>
    </item>
    <item>
      <title>Re: Booting U-Boot on an LS1043A-based board</title>
      <link>https://community.nxp.com/t5/Layerscape/Booting-U-Boot-on-an-LS1043A-based-board/m-p/600034#M1640</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Fedor,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Sorry for the delay. The pre-built images wouldn't work on any board other than your development system because of your QIXIS FPGA. I downloaded the 2.0 SDK and I had to take quite a bit out of the LS1043AQDS image, but I tested with and without those lines I mentioned and it boots without&amp;nbsp;and doesn't with.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I did notice one very interesting thing. We were able to get the QSPI image working. This QSPI QDS image does not include arch_cpu_init(). &amp;nbsp;The SPL image only includes arch_cpu_init() if the board is an LS2080A. Could this just be an oversight for NOR boot? &amp;nbsp;Perhaps arch_cpu_init() should not be called for the LS1043A?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;John&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 19 Sep 2016 21:53:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Booting-U-Boot-on-an-LS1043A-based-board/m-p/600034#M1640</guid>
      <dc:creator>johnschmoller</dc:creator>
      <dc:date>2016-09-19T21:53:56Z</dc:date>
    </item>
    <item>
      <title>Re: Booting U-Boot on an LS1043A-based board</title>
      <link>https://community.nxp.com/t5/Layerscape/Booting-U-Boot-on-an-LS1043A-based-board/m-p/600035#M1641</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please try pre-built images from the SDK 2.0 (QorIQ Linux SDK v2.0 AARCH64 IMAGE.iso) which contains images for the LS1043ARDB.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 20 Sep 2016 03:02:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Booting-U-Boot-on-an-LS1043A-based-board/m-p/600035#M1641</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2016-09-20T03:02:08Z</dc:date>
    </item>
    <item>
      <title>Re: Booting U-Boot on an LS1043A-based board</title>
      <link>https://community.nxp.com/t5/Layerscape/Booting-U-Boot-on-an-LS1043A-based-board/m-p/600036#M1642</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We have an RDB, but we cannot run the precompiled binaries on our hardware. The precompiled binary does run on the RDB. But SDK 2.0 also does not call arch_cpu_init(). That call was introduced in mainline when ARM moved to the unified arch/arm/lib/board.c. It seems like that function is the weak link, it's not meant to be called on the LS1043A. Can you confirm that this needs to be changed in mainline U-Boot?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 20 Sep 2016 20:11:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Booting-U-Boot-on-an-LS1043A-based-board/m-p/600036#M1642</guid>
      <dc:creator>johnschmoller</dc:creator>
      <dc:date>2016-09-20T20:11:06Z</dc:date>
    </item>
    <item>
      <title>Re: Booting U-Boot on an LS1043A-based board</title>
      <link>https://community.nxp.com/t5/Layerscape/Booting-U-Boot-on-an-LS1043A-based-board/m-p/600037#M1643</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;gt; We have an RDB, but we cannot run the precompiled binaries on our hardware.&lt;/P&gt;&lt;P&gt;&amp;gt; The precompiled binary does run on the RDB.&lt;/P&gt;&lt;P&gt;This means that you have to doublecheck your design referring the AN5012 - LS1043A Design Checklist and the processor's Data Sheet (pay special attention to the notes after Table 1 and Table 2).&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Sep 2016 02:08:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Booting-U-Boot-on-an-LS1043A-based-board/m-p/600037#M1643</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2016-09-21T02:08:59Z</dc:date>
    </item>
  </channel>
</rss>