<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LayerscapeのトピックRe: Failure on DPDMUX default interface configured when external traffic is available</title>
    <link>https://community.nxp.com/t5/Layerscape/Failure-on-DPDMUX-default-interface-configured-when-external/m-p/2270313#M16376</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm using Kernel:&amp;nbsp;5.15.71 and MC version: 10.38.1. BSP is based on LSDK21.08.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 31 Dec 2025 02:01:08 GMT</pubDate>
    <dc:creator>dunk</dc:creator>
    <dc:date>2025-12-31T02:01:08Z</dc:date>
    <item>
      <title>Failure on DPDMUX default interface configured when external traffic is available</title>
      <link>https://community.nxp.com/t5/Layerscape/Failure-on-DPDMUX-default-interface-configured-when-external/m-p/2269891#M16370</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Following procedure will cause error message from MC:&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;[E, qbman_rec_isr:391, QBMAN] QBMAN recoverable event 0x1000000&lt;BR /&gt;[E, dpmng_dump_rerr_fqid:1335, QBMAN] REL_FQ (FQ[0]) has 1 messages, dumping up to 16:&lt;BR /&gt;[E, dpmng_dump_rerr_fqid:1361, QBMAN] Message:&lt;BR /&gt;0x00125340: 2f930000 000000ab 00000000 00000000&lt;BR /&gt;0x00125350: 00000000 00000000 00000000 00000000&lt;BR /&gt;0x00125360: 2f180280 18000000 8a030000 00000000&lt;BR /&gt;0x00125370: 00000000 00000000 00000000 00000000&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;This error message can be produced by enabling/configuring the default interface of dpdmux instance and external traffic is available.&lt;/P&gt;&lt;P&gt;Case 1: DPL enable default interface&lt;/P&gt;&lt;P&gt;With DPL of following setting with 'default_if = &amp;lt;0x1&amp;gt;;'&lt;/P&gt;&lt;P&gt;--&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;dpdmux@1 {&lt;BR /&gt;&amp;nbsp; &amp;nbsp; compatible = "fsl,dpdmux";&lt;BR /&gt;&amp;nbsp; &amp;nbsp; options = "DPDMUX_OPT_CLS_MASK_SUPPORT", "DPDMUX_OPT_AUTO_MAX_FRAME_LEN";&lt;BR /&gt;&amp;nbsp; &amp;nbsp; method = "DPDMUX_METHOD_CUSTOM";&lt;BR /&gt;&amp;nbsp; &amp;nbsp; manip = "DPDMUX_MANIP_NONE";&lt;BR /&gt;&amp;nbsp; &amp;nbsp; num_ifs = &amp;lt;0x2&amp;gt;;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;&amp;nbsp;default_if = &amp;lt;0x1&amp;gt;;&lt;BR /&gt;};&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;--&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Case 2: DPL not to enable default interface of DPDMUX&lt;/P&gt;&lt;P&gt;Option 'default_if = &amp;lt;0x1&amp;gt;;' is not set. But using dpdk to configure the default interface.&lt;/P&gt;&lt;P&gt;API 'dpdmux_if_set_default' is used for this.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any suggestion to avoid such error?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 30 Dec 2025 07:15:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Failure-on-DPDMUX-default-interface-configured-when-external/m-p/2269891#M16370</guid>
      <dc:creator>dunk</dc:creator>
      <dc:date>2025-12-30T07:15:16Z</dc:date>
    </item>
    <item>
      <title>Re: Failure on DPDMUX default interface configured when external traffic is available</title>
      <link>https://community.nxp.com/t5/Layerscape/Failure-on-DPDMUX-default-interface-configured-when-external/m-p/2270165#M16373</link>
      <description>&lt;P&gt;Hello.&lt;/P&gt;
&lt;P&gt;Please share the MC version, BSP and kernel version, Processor and board used.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards.&lt;/P&gt;</description>
      <pubDate>Tue, 30 Dec 2025 17:55:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Failure-on-DPDMUX-default-interface-configured-when-external/m-p/2270165#M16373</guid>
      <dc:creator>Oswalag</dc:creator>
      <dc:date>2025-12-30T17:55:46Z</dc:date>
    </item>
    <item>
      <title>Re: Failure on DPDMUX default interface configured when external traffic is available</title>
      <link>https://community.nxp.com/t5/Layerscape/Failure-on-DPDMUX-default-interface-configured-when-external/m-p/2270313#M16376</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm using Kernel:&amp;nbsp;5.15.71 and MC version: 10.38.1. BSP is based on LSDK21.08.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 31 Dec 2025 02:01:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Failure-on-DPDMUX-default-interface-configured-when-external/m-p/2270313#M16376</guid>
      <dc:creator>dunk</dc:creator>
      <dc:date>2025-12-31T02:01:08Z</dc:date>
    </item>
    <item>
      <title>Re: Failure on DPDMUX default interface configured when external traffic is available</title>
      <link>https://community.nxp.com/t5/Layerscape/Failure-on-DPDMUX-default-interface-configured-when-external/m-p/2291352#M16397</link>
      <description>&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;The issue could be due to a software version incompatibility , please take a look into the LLDPUG, there is where MC 10.38.0 was validated, this with Kernel&amp;nbsp;v6.1.55.&lt;/P&gt;
&lt;P&gt;I recommend you to test again using the LLDP mentioned before building the images with Yocto.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards.&lt;/P&gt;</description>
      <pubDate>Sun, 11 Jan 2026 01:56:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Failure-on-DPDMUX-default-interface-configured-when-external/m-p/2291352#M16397</guid>
      <dc:creator>Oswalag</dc:creator>
      <dc:date>2026-01-11T01:56:16Z</dc:date>
    </item>
  </channel>
</rss>