<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Layerscape中的主题 Re: LX2160A support 100G QSFP</title>
    <link>https://community.nxp.com/t5/Layerscape/LX2160A-support-100G-QSFP/m-p/2198436#M16270</link>
    <description>Dear &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/256487"&gt;@sheep-sleep&lt;/a&gt;,&lt;BR /&gt;&lt;BR /&gt;100G to 4x25G splitter lanes.&lt;BR /&gt;&lt;BR /&gt;you need to use a PHY like the "Broadcom BCM87102", then it's necessary to add it to the device tree, once configured , you need to build the image.&lt;BR /&gt;thanks for your preference.&lt;BR /&gt;BR&lt;BR /&gt;LFGP</description>
    <pubDate>Tue, 04 Nov 2025 17:13:26 GMT</pubDate>
    <dc:creator>LFGP</dc:creator>
    <dc:date>2025-11-04T17:13:26Z</dc:date>
    <item>
      <title>LX2160A support 100G QSFP</title>
      <link>https://community.nxp.com/t5/Layerscape/LX2160A-support-100G-QSFP/m-p/2198237#M16268</link>
      <description>&lt;P&gt;I want use the QSFP support 100G，I write the image to sd card lx2160a_rev2_cex7_clearfog-cx_sd_2000_700_2400_18_5_2-6e436bb.img.xz,&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;restool dpmac info dpmac.3/4/5/6&lt;/SPAN&gt; &lt;SPAN&gt;maximum supported rate 25000 Mbps&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;According to the official manual，if&amp;nbsp;&lt;SPAN&gt;SERDES configuration of 18，The 4 ports on QSFP can be accessed via 40G to 4x10G or 100G to 4x25G splitter cables。but I want use the QSFP support 100G connect to device，no need to breakout&amp;nbsp;the network port.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;What should I do? Do I need to rewrite the image? If so, which image do I need to rewrite?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 04 Nov 2025 09:59:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LX2160A-support-100G-QSFP/m-p/2198237#M16268</guid>
      <dc:creator>sheep-sleep</dc:creator>
      <dc:date>2025-11-04T09:59:51Z</dc:date>
    </item>
    <item>
      <title>Re: LX2160A support 100G QSFP</title>
      <link>https://community.nxp.com/t5/Layerscape/LX2160A-support-100G-QSFP/m-p/2198436#M16270</link>
      <description>Dear &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/256487"&gt;@sheep-sleep&lt;/a&gt;,&lt;BR /&gt;&lt;BR /&gt;100G to 4x25G splitter lanes.&lt;BR /&gt;&lt;BR /&gt;you need to use a PHY like the "Broadcom BCM87102", then it's necessary to add it to the device tree, once configured , you need to build the image.&lt;BR /&gt;thanks for your preference.&lt;BR /&gt;BR&lt;BR /&gt;LFGP</description>
      <pubDate>Tue, 04 Nov 2025 17:13:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LX2160A-support-100G-QSFP/m-p/2198436#M16270</guid>
      <dc:creator>LFGP</dc:creator>
      <dc:date>2025-11-04T17:13:26Z</dc:date>
    </item>
  </channel>
</rss>