<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic SBOM also created for another processor board when there is a different designated target board in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/SBOM-also-created-for-another-processor-board-when-there-is-a/m-p/2187672#M16214</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am trying to create an SBOM for the yocto real-time-edge for the lx2160ardb-rev2. I have been able to do so by setting the local.conf to create-spdx and have done so.&amp;nbsp;&lt;/P&gt;&lt;P&gt;However, when I look at the json files of the kernel as an example, I see that it mentions use of the imx8 processor and this makes me confused since I set the target board to be the lx2160ardb-rev2.&lt;/P&gt;&lt;P&gt;If anyone could shed some light on the creation of the SBOM and how to create an SBOM for my correct target of the lx2160ardb-rev2 that would be greatly appreciated.&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;</description>
    <pubDate>Thu, 16 Oct 2025 16:45:43 GMT</pubDate>
    <dc:creator>FEI-Namg</dc:creator>
    <dc:date>2025-10-16T16:45:43Z</dc:date>
    <item>
      <title>SBOM also created for another processor board when there is a different designated target board</title>
      <link>https://community.nxp.com/t5/Layerscape/SBOM-also-created-for-another-processor-board-when-there-is-a/m-p/2187672#M16214</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am trying to create an SBOM for the yocto real-time-edge for the lx2160ardb-rev2. I have been able to do so by setting the local.conf to create-spdx and have done so.&amp;nbsp;&lt;/P&gt;&lt;P&gt;However, when I look at the json files of the kernel as an example, I see that it mentions use of the imx8 processor and this makes me confused since I set the target board to be the lx2160ardb-rev2.&lt;/P&gt;&lt;P&gt;If anyone could shed some light on the creation of the SBOM and how to create an SBOM for my correct target of the lx2160ardb-rev2 that would be greatly appreciated.&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;</description>
      <pubDate>Thu, 16 Oct 2025 16:45:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/SBOM-also-created-for-another-processor-board-when-there-is-a/m-p/2187672#M16214</guid>
      <dc:creator>FEI-Namg</dc:creator>
      <dc:date>2025-10-16T16:45:43Z</dc:date>
    </item>
  </channel>
</rss>