<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LS1043A Jumbo frame support in Linux Mainline in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/LS1043A-Jumbo-frame-support-in-Linux-Mainline/m-p/2186093#M16206</link>
    <description>Dear &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/180431"&gt;@timsalabim&lt;/a&gt;,&lt;BR /&gt;unfortunately  we don't have anything for the  Linux Mainline Kernel regarding jumbo frames, due they are managed by the block DPAA we recommend to use the NXP SDK.&lt;BR /&gt;&lt;BR /&gt;BR&lt;BR /&gt;LFGP &lt;BR /&gt;</description>
    <pubDate>Tue, 14 Oct 2025 23:43:50 GMT</pubDate>
    <dc:creator>LFGP</dc:creator>
    <dc:date>2025-10-14T23:43:50Z</dc:date>
    <item>
      <title>LS1043A Jumbo frame support in Linux Mainline</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1043A-Jumbo-frame-support-in-Linux-Mainline/m-p/2184792#M16199</link>
      <description>&lt;P&gt;Dear NXP support,&amp;nbsp;&lt;/P&gt;&lt;P&gt;we are evaluating Jumbo Frames on LS1043A with a custom specific board, but when changing the MTU size in Linux the system shows:&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;Error: mtu greater than device maximum.&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;During my research, I came across the following NXP Community thread:&lt;BR /&gt;&lt;A href="https://community.nxp.com/t5/Layerscape/Why-is-LS1043-MTU-limited-to-2K-not-4K/m-p/847022" target="_blank" rel="noopener"&gt;https://community.nxp.com/t5/Layerscape/Why-is-LS1043-MTU-limited-to-2K-not-4K/m-p/847022&lt;/A&gt;&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;Which refers to FMAN&amp;nbsp;&lt;SPAN&gt;Errata&amp;nbsp;A-010022 and a patch to fix this&amp;nbsp;behavior in the NXP LSDK Kernel.&lt;BR /&gt;But I did not find anything similar for Linux Mainline Kernel, are there any fixes NXP can provide to support Jumbo Frames ?&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;thank you in advance&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 13 Oct 2025 10:58:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1043A-Jumbo-frame-support-in-Linux-Mainline/m-p/2184792#M16199</guid>
      <dc:creator>timsalabim</dc:creator>
      <dc:date>2025-10-13T10:58:08Z</dc:date>
    </item>
    <item>
      <title>Re: LS1043A Jumbo frame support in Linux Mainline</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1043A-Jumbo-frame-support-in-Linux-Mainline/m-p/2184945#M16200</link>
      <description>Dear &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/180431"&gt;@timsalabim&lt;/a&gt;,&lt;BR /&gt;&lt;BR /&gt;Did you set the DPAA Ethernet driver into the Kernel to support jumbo frames? &lt;BR /&gt;please review, into the LLDP user manual, the subsection "7.2.2.5.2.2 Kconfig options" and the "7.2.2.5.3.3 Jumbo frames support". &lt;BR /&gt;BR&lt;BR /&gt;LFGP</description>
      <pubDate>Mon, 13 Oct 2025 14:49:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1043A-Jumbo-frame-support-in-Linux-Mainline/m-p/2184945#M16200</guid>
      <dc:creator>LFGP</dc:creator>
      <dc:date>2025-10-13T14:49:48Z</dc:date>
    </item>
    <item>
      <title>Re: LS1043A Jumbo frame support in Linux Mainline</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1043A-Jumbo-frame-support-in-Linux-Mainline/m-p/2184983#M16201</link>
      <description>&lt;P&gt;Hello,&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;thanks for the reply, the mentioned option are only available in the NXP based Linux kernel, which uses &lt;STRONG&gt;CONFIG_FSL_SDK_DPAA&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://docs.nxp.com/bundle/UG10081_LLDP_L6.1.55_2.2.0/page/topics/jumbo_frames_support.html" target="_blank"&gt;https://docs.nxp.com/bundle/UG10081_LLDP_L6.1.55_2.2.0/page/topics/jumbo_frames_support.html&lt;/A&gt;&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;In the Linux Mainline kernel &lt;STRONG&gt;CONFIG_FSL_DPPA_ETH&lt;/STRONG&gt; is used which does not have the extended options in the kernel menuconfig&lt;BR /&gt;&lt;BR /&gt;&lt;A href="https://git.kernel.org/pub/scm/linux/kernel/git/stable/linux.git/tree/drivers/net/ethernet/freescale/dpaa/Kconfig?h=v6.12.52" target="_self"&gt;https://git.kernel.org/pub/scm/linux/kernel/git/stable/linux.git/tree/drivers/net/ethernet/freescale/dpaa/Kconfig?h=v6.12.52&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;best regards&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;Tim&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 13 Oct 2025 15:44:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1043A-Jumbo-frame-support-in-Linux-Mainline/m-p/2184983#M16201</guid>
      <dc:creator>timsalabim</dc:creator>
      <dc:date>2025-10-13T15:44:07Z</dc:date>
    </item>
    <item>
      <title>Re: LS1043A Jumbo frame support in Linux Mainline</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1043A-Jumbo-frame-support-in-Linux-Mainline/m-p/2186093#M16206</link>
      <description>Dear &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/180431"&gt;@timsalabim&lt;/a&gt;,&lt;BR /&gt;unfortunately  we don't have anything for the  Linux Mainline Kernel regarding jumbo frames, due they are managed by the block DPAA we recommend to use the NXP SDK.&lt;BR /&gt;&lt;BR /&gt;BR&lt;BR /&gt;LFGP &lt;BR /&gt;</description>
      <pubDate>Tue, 14 Oct 2025 23:43:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1043A-Jumbo-frame-support-in-Linux-Mainline/m-p/2186093#M16206</guid>
      <dc:creator>LFGP</dc:creator>
      <dc:date>2025-10-14T23:43:50Z</dc:date>
    </item>
    <item>
      <title>Re: LS1043A Jumbo frame support in Linux Mainline</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1043A-Jumbo-frame-support-in-Linux-Mainline/m-p/2191382#M16235</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;SPAN&gt;LFGP,&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;thank you for the reply,&amp;nbsp;Since Layerscape CPUs are primarily intended for network equipment, we as manufacturer are very interested in using the Linux mainline kernel, as the platforms are supported for a very long time and we are not dependent on NXP for kernel updates. This is becoming increasingly important for us and our customers, especially in light of the Cyber Resilience Act.&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;best regards&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;Tim&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 23 Oct 2025 09:28:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1043A-Jumbo-frame-support-in-Linux-Mainline/m-p/2191382#M16235</guid>
      <dc:creator>timsalabim</dc:creator>
      <dc:date>2025-10-23T09:28:49Z</dc:date>
    </item>
  </channel>
</rss>