<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Layerscape中的主题 Re: LS1046A-LX2160A connection</title>
    <link>https://community.nxp.com/t5/Layerscape/LS1046A-LX2160A-connection/m-p/2180911#M16173</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;You can set mac to mac connection or through a phy for auto-negotiation.&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;u-Boot sets the SerDes to auto-negotiate over SGMII. If the&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;device at the other end of an SGMII link is configurable to send a&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;PHY-side response of auto-negotiation type SGMII, then nothing has&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;to be changed. If the other end has no autoneg support&amp;nbsp; or supports&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;only the MAC side SGMII auto-negotiation, then see LS1046ARM, Sections 31.8.1.1&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;and 31.8.1.2.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;If you want to use a phy you can refer to both reference design boards (for example&amp;nbsp;AQR113C).&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Tue, 07 Oct 2025 03:35:15 GMT</pubDate>
    <dc:creator>Oswalag</dc:creator>
    <dc:date>2025-10-07T03:35:15Z</dc:date>
    <item>
      <title>LS1046A-LX2160A connection</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1046A-LX2160A-connection/m-p/2180027#M16169</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have&amp;nbsp; a question regarding an LS1046A to LX2160A connection. If I configure a LS1046A SERDES to 2.5G SGMII, what would be the simplest way to connect it to a LX2160A SERDES port. This can be either fixed link, or phy/other. I'm looking for the best way to go about it, least amount of parts and most reliable.&lt;/P&gt;&lt;P&gt;DD&lt;/P&gt;</description>
      <pubDate>Fri, 03 Oct 2025 17:39:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1046A-LX2160A-connection/m-p/2180027#M16169</guid>
      <dc:creator>ddnxpcom</dc:creator>
      <dc:date>2025-10-03T17:39:38Z</dc:date>
    </item>
    <item>
      <title>Re: LS1046A-LX2160A connection</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1046A-LX2160A-connection/m-p/2180911#M16173</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;You can set mac to mac connection or through a phy for auto-negotiation.&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;u-Boot sets the SerDes to auto-negotiate over SGMII. If the&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;device at the other end of an SGMII link is configurable to send a&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;PHY-side response of auto-negotiation type SGMII, then nothing has&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;to be changed. If the other end has no autoneg support&amp;nbsp; or supports&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;only the MAC side SGMII auto-negotiation, then see LS1046ARM, Sections 31.8.1.1&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;and 31.8.1.2.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;If you want to use a phy you can refer to both reference design boards (for example&amp;nbsp;AQR113C).&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 07 Oct 2025 03:35:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1046A-LX2160A-connection/m-p/2180911#M16173</guid>
      <dc:creator>Oswalag</dc:creator>
      <dc:date>2025-10-07T03:35:15Z</dc:date>
    </item>
  </channel>
</rss>