<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LayerscapeのトピックRe: LLDP 5.15.71 add application issue based on LX2160ARDB</title>
    <link>https://community.nxp.com/t5/Layerscape/LLDP-5-15-71-add-application-issue-based-on-LX2160ARDB/m-p/2177807#M16157</link>
    <description>&lt;P&gt;Please unzip the attached file and put this recipe in&amp;nbsp;sources/poky/meta/recipes-core/util-linux/util-linux-libuuid_2.38.1.bb&lt;/P&gt;</description>
    <pubDate>Tue, 30 Sep 2025 02:25:24 GMT</pubDate>
    <dc:creator>yipingwang</dc:creator>
    <dc:date>2025-09-30T02:25:24Z</dc:date>
    <item>
      <title>LLDP 5.15.71 add application issue based on LX2160ARDB</title>
      <link>https://community.nxp.com/t5/Layerscape/LLDP-5-15-71-add-application-issue-based-on-LX2160ARDB/m-p/2176216#M16133</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;We are trying to add docker-ce into yocto LLDP 5.15-71, but it shows below error:&lt;/P&gt;&lt;P&gt;Do you have any solution about ubuntu and yocto package conflicts issue?&lt;/P&gt;&lt;P&gt;bitbake&amp;nbsp;ls-image-main&lt;/P&gt;&lt;P&gt;Error:&lt;BR /&gt;Problem: package util-linux-2.37.4-r0.aarch64 requires util-linux-libuuid, but none of the providers can be installed&lt;BR /&gt;- package ubuntu-main-22.04.1-r0.aarch64 conflicts with libuuid1 provided by libuuid1-2.37.4-r0.aarch64&lt;BR /&gt;- package ubuntu-main-22.04.1-r0.aarch64 obsoletes libuuid1 provided by libuuid1-2.37.4-r0.aarch64&lt;BR /&gt;- package docker-ce-20.10.12+ce+git906f57ff5b7100013dfef066ea8fe367706468df-r0.aarch64 requires util-linux, but none of the providers can be installed&lt;BR /&gt;- conflicting requests&lt;BR /&gt;(try to add '--allowerasing' to command line to replace conflicting packages or '--skip-broken' to skip uninstallable packages)&lt;/P&gt;&lt;P&gt;BR,&lt;/P&gt;&lt;P&gt;Jack Ho&lt;/P&gt;</description>
      <pubDate>Fri, 26 Sep 2025 03:27:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LLDP-5-15-71-add-application-issue-based-on-LX2160ARDB/m-p/2176216#M16133</guid>
      <dc:creator>jackho</dc:creator>
      <dc:date>2025-09-26T03:27:04Z</dc:date>
    </item>
    <item>
      <title>Re: LLDP 5.15.71 add application issue based on LX2160ARDB</title>
      <link>https://community.nxp.com/t5/Layerscape/LLDP-5-15-71-add-application-issue-based-on-LX2160ARDB/m-p/2177807#M16157</link>
      <description>&lt;P&gt;Please unzip the attached file and put this recipe in&amp;nbsp;sources/poky/meta/recipes-core/util-linux/util-linux-libuuid_2.38.1.bb&lt;/P&gt;</description>
      <pubDate>Tue, 30 Sep 2025 02:25:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LLDP-5-15-71-add-application-issue-based-on-LX2160ARDB/m-p/2177807#M16157</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2025-09-30T02:25:24Z</dc:date>
    </item>
  </channel>
</rss>