<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Layerscape中的主题 LS1046 does not boot from SD card</title>
    <link>https://community.nxp.com/t5/Layerscape/LS1046-does-not-boot-from-SD-card/m-p/2175961#M16130</link>
    <description>&lt;P&gt;I am trying to boot from SD card, LS1046 using OK1046A-C2 Single Board Computer from forlinx.&lt;/P&gt;&lt;P&gt;I am flashing the SD card using the following command&lt;/P&gt;&lt;P&gt;flex-installer -i auto -m ls1046ardb -d /dev/sdq -p 4P=128M:2G:8G:-1&lt;/P&gt;&lt;P&gt;And it installs all partitions into SD card successfully(attached file showing instalation finishing successfully)&lt;/P&gt;&lt;P&gt;But then when I connect it to OK1046-C2 board and try to boot these are the kernel messages I get(full boot log attached)&lt;/P&gt;&lt;P&gt;[ 3.108076] mmc0: SDHCI controller on 1560000.esdhc [1560000.esdhc] using ADMA 64-bit&lt;BR /&gt;[ 3.108968] Freescale USDPAA process IRQ driver&lt;BR /&gt;[ 3.112360] optee: probing for conduit method.&lt;BR /&gt;[ 3.125802] optee: revision 2.6&lt;BR /&gt;[ 3.126122] optee: initialized driver&lt;BR /&gt;[ 3.138321] NET: Registered protocol family 26&lt;BR /&gt;[ 3.142792] u32 classifier&lt;BR /&gt;[ 3.145510] input device check on&lt;BR /&gt;[ 3.149185] Actions configured&lt;BR /&gt;[ 3.152903] Initializing XFRM netlink socket&lt;BR /&gt;[ 3.157214] NET: Registered protocol family 10&lt;BR /&gt;[ 3.162081] Segment Routing with IPv6&lt;BR /&gt;[ 3.165785] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver&lt;BR /&gt;[ 3.171894] NET: Registered protocol family 17&lt;BR /&gt;[ 3.176352] NET: Registered protocol family 15&lt;BR /&gt;[ 3.180809] Bridge firewalling registered&lt;BR /&gt;[ 3.184924] 8021q: 802.1Q VLAN Support v1.8&lt;BR /&gt;[ 3.189111] lib80211: common routines for IEEE802.11 drivers&lt;BR /&gt;[ 3.193552] mmc0: error -110 whilst initialising SD card&lt;BR /&gt;[ 3.200103] 9pnet: Installing 9P2000 support&lt;BR /&gt;[ 3.204387] tsn generic netlink module v1 init...&lt;BR /&gt;[ 3.209119] Key type dns_resolver registered&lt;BR /&gt;[ 3.213550] registered taskstats version 1&lt;BR /&gt;[ 3.217654] Loading compiled-in X.509 certificates&lt;BR /&gt;[ 3.223313] Btrfs loaded, crc32c=crc32c-generic&lt;BR /&gt;[ 3.229821] ALSA device list:&lt;BR /&gt;[ 3.232784] No soundcards found.&lt;BR /&gt;[ 3.236370] Waiting for root device PARTUUID=c52a6a85-04...&lt;BR /&gt;[ 3.339452] random: crng init done&lt;/P&gt;</description>
    <pubDate>Thu, 25 Sep 2025 16:19:01 GMT</pubDate>
    <dc:creator>douglassilva</dc:creator>
    <dc:date>2025-09-25T16:19:01Z</dc:date>
    <item>
      <title>LS1046 does not boot from SD card</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1046-does-not-boot-from-SD-card/m-p/2175961#M16130</link>
      <description>&lt;P&gt;I am trying to boot from SD card, LS1046 using OK1046A-C2 Single Board Computer from forlinx.&lt;/P&gt;&lt;P&gt;I am flashing the SD card using the following command&lt;/P&gt;&lt;P&gt;flex-installer -i auto -m ls1046ardb -d /dev/sdq -p 4P=128M:2G:8G:-1&lt;/P&gt;&lt;P&gt;And it installs all partitions into SD card successfully(attached file showing instalation finishing successfully)&lt;/P&gt;&lt;P&gt;But then when I connect it to OK1046-C2 board and try to boot these are the kernel messages I get(full boot log attached)&lt;/P&gt;&lt;P&gt;[ 3.108076] mmc0: SDHCI controller on 1560000.esdhc [1560000.esdhc] using ADMA 64-bit&lt;BR /&gt;[ 3.108968] Freescale USDPAA process IRQ driver&lt;BR /&gt;[ 3.112360] optee: probing for conduit method.&lt;BR /&gt;[ 3.125802] optee: revision 2.6&lt;BR /&gt;[ 3.126122] optee: initialized driver&lt;BR /&gt;[ 3.138321] NET: Registered protocol family 26&lt;BR /&gt;[ 3.142792] u32 classifier&lt;BR /&gt;[ 3.145510] input device check on&lt;BR /&gt;[ 3.149185] Actions configured&lt;BR /&gt;[ 3.152903] Initializing XFRM netlink socket&lt;BR /&gt;[ 3.157214] NET: Registered protocol family 10&lt;BR /&gt;[ 3.162081] Segment Routing with IPv6&lt;BR /&gt;[ 3.165785] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver&lt;BR /&gt;[ 3.171894] NET: Registered protocol family 17&lt;BR /&gt;[ 3.176352] NET: Registered protocol family 15&lt;BR /&gt;[ 3.180809] Bridge firewalling registered&lt;BR /&gt;[ 3.184924] 8021q: 802.1Q VLAN Support v1.8&lt;BR /&gt;[ 3.189111] lib80211: common routines for IEEE802.11 drivers&lt;BR /&gt;[ 3.193552] mmc0: error -110 whilst initialising SD card&lt;BR /&gt;[ 3.200103] 9pnet: Installing 9P2000 support&lt;BR /&gt;[ 3.204387] tsn generic netlink module v1 init...&lt;BR /&gt;[ 3.209119] Key type dns_resolver registered&lt;BR /&gt;[ 3.213550] registered taskstats version 1&lt;BR /&gt;[ 3.217654] Loading compiled-in X.509 certificates&lt;BR /&gt;[ 3.223313] Btrfs loaded, crc32c=crc32c-generic&lt;BR /&gt;[ 3.229821] ALSA device list:&lt;BR /&gt;[ 3.232784] No soundcards found.&lt;BR /&gt;[ 3.236370] Waiting for root device PARTUUID=c52a6a85-04...&lt;BR /&gt;[ 3.339452] random: crng init done&lt;/P&gt;</description>
      <pubDate>Thu, 25 Sep 2025 16:19:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1046-does-not-boot-from-SD-card/m-p/2175961#M16130</guid>
      <dc:creator>douglassilva</dc:creator>
      <dc:date>2025-09-25T16:19:01Z</dc:date>
    </item>
    <item>
      <title>Re: LS1046 does not boot from SD card</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1046-does-not-boot-from-SD-card/m-p/2176240#M16135</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;Which version of LSDK are you testing?&lt;/P&gt;</description>
      <pubDate>Fri, 26 Sep 2025 04:16:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1046-does-not-boot-from-SD-card/m-p/2176240#M16135</guid>
      <dc:creator>Oswalag</dc:creator>
      <dc:date>2025-09-26T04:16:39Z</dc:date>
    </item>
    <item>
      <title>Re: LS1046 does not boot from SD card</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1046-does-not-boot-from-SD-card/m-p/2176273#M16137</link>
      <description>I am testing with LSDK 2108, but I did not had successfull results with 2012 either.</description>
      <pubDate>Fri, 26 Sep 2025 05:09:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1046-does-not-boot-from-SD-card/m-p/2176273#M16137</guid>
      <dc:creator>douglassilva</dc:creator>
      <dc:date>2025-09-26T05:09:21Z</dc:date>
    </item>
  </channel>
</rss>