<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: DPSW no buffer discard in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/DPSW-no-buffer-discard/m-p/2174702#M16121</link>
    <description>&lt;P&gt;&lt;SPAN&gt;Is there a solution that uses DPSW?&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Wed, 24 Sep 2025 03:28:34 GMT</pubDate>
    <dc:creator>linxings</dc:creator>
    <dc:date>2025-09-24T03:28:34Z</dc:date>
    <item>
      <title>DPSW no buffer discard</title>
      <link>https://community.nxp.com/t5/Layerscape/DPSW-no-buffer-discard/m-p/2174231#M16119</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Hello,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I used the ls - addsw command to create a dpsw, and during the running test, I discovered an issue.&lt;BR /&gt;When my packet rate reaches 1.2Gbps, dpsw will experience no buffer discard, and its rate can only reach 945Mbps.&lt;BR /&gt;May I ask how I should solve this problem?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;The corresponding dprc resources are shown in the file.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 23 Sep 2025 10:13:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/DPSW-no-buffer-discard/m-p/2174231#M16119</guid>
      <dc:creator>linxings</dc:creator>
      <dc:date>2025-09-23T10:13:26Z</dc:date>
    </item>
    <item>
      <title>Re: DPSW no buffer discard</title>
      <link>https://community.nxp.com/t5/Layerscape/DPSW-no-buffer-discard/m-p/2174375#M16120</link>
      <description>&lt;P&gt;Hello, And now we want to use DPSW to do traffic bifurcation between DPDK and Linux Kernel on in DPAA2, according to the LLDPUG, we only need to replace DPDMUX with DPSW and the steps to configure the setup are same as DPDMUX. You could use recent released LSDK Layerscape Linux Distribution POC User Guide Rev, L6.1.55_2.2.0&lt;/P&gt;
&lt;P&gt;&lt;A href="https://docs.nxp.com/bundle/Layerscape_Linux_Distribution_POC_User_Guide/page/topics/setting_up_ethernet_switch_capability.html" target="_blank"&gt;https://docs.nxp.com/bundle/Layerscape_Linux_Distribution_POC_User_Guide/page/topics/setting_up_ethernet_switch_capability.html&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Tue, 23 Sep 2025 14:04:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/DPSW-no-buffer-discard/m-p/2174375#M16120</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2025-09-23T14:04:38Z</dc:date>
    </item>
    <item>
      <title>Re: DPSW no buffer discard</title>
      <link>https://community.nxp.com/t5/Layerscape/DPSW-no-buffer-discard/m-p/2174702#M16121</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Is there a solution that uses DPSW?&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 24 Sep 2025 03:28:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/DPSW-no-buffer-discard/m-p/2174702#M16121</guid>
      <dc:creator>linxings</dc:creator>
      <dc:date>2025-09-24T03:28:34Z</dc:date>
    </item>
    <item>
      <title>Re: DPSW no buffer discard</title>
      <link>https://community.nxp.com/t5/Layerscape/DPSW-no-buffer-discard/m-p/2175062#M16122</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;Yes, you can check the RM or this page:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://docs.nxp.com/bundle/GUID-487B2E69-BB19-42CB-AC38-7EF18C0FE3AE/page/GUID-6B20C5FB-B787-4CC1-B6AB-351276113960.html#" target="_blank"&gt;https://docs.nxp.com/bundle/GUID-487B2E69-BB19-42CB-AC38-7EF18C0FE3AE/page/GUID-6B20C5FB-B787-4CC1-B6AB-351276113960.html#&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Wed, 24 Sep 2025 13:24:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/DPSW-no-buffer-discard/m-p/2175062#M16122</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2025-09-24T13:24:18Z</dc:date>
    </item>
  </channel>
</rss>