<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Synchonous uart support with LS1043A in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/Synchonous-uart-support-with-LS1043A/m-p/2172263#M16116</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;the DUART modules implemented&amp;nbsp;are designed for asynchronous communication, the LS1043A implements the QE, it has 2 UCC that could be use and configure for synchronous UART but it isn't tested nor supported in the BSP.&lt;/P&gt;</description>
    <pubDate>Thu, 18 Sep 2025 20:42:33 GMT</pubDate>
    <dc:creator>Oswalag</dc:creator>
    <dc:date>2025-09-18T20:42:33Z</dc:date>
    <item>
      <title>Synchonous uart support with LS1043A</title>
      <link>https://community.nxp.com/t5/Layerscape/Synchonous-uart-support-with-LS1043A/m-p/2171997#M16112</link>
      <description>&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;Is the LS1043A supports&amp;nbsp; synchronous Uart communication. Our application needs to use 3 UARTS&amp;nbsp; in synchronous mode and LS1043A should&amp;nbsp; give&amp;nbsp;&amp;nbsp;tclk and rclk as outputs.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 18 Sep 2025 12:06:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Synchonous-uart-support-with-LS1043A/m-p/2171997#M16112</guid>
      <dc:creator>Pamid</dc:creator>
      <dc:date>2025-09-18T12:06:15Z</dc:date>
    </item>
    <item>
      <title>Re: Synchonous uart support with LS1043A</title>
      <link>https://community.nxp.com/t5/Layerscape/Synchonous-uart-support-with-LS1043A/m-p/2172263#M16116</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;the DUART modules implemented&amp;nbsp;are designed for asynchronous communication, the LS1043A implements the QE, it has 2 UCC that could be use and configure for synchronous UART but it isn't tested nor supported in the BSP.&lt;/P&gt;</description>
      <pubDate>Thu, 18 Sep 2025 20:42:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Synchonous-uart-support-with-LS1043A/m-p/2172263#M16116</guid>
      <dc:creator>Oswalag</dc:creator>
      <dc:date>2025-09-18T20:42:33Z</dc:date>
    </item>
  </channel>
</rss>