<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic How can I modify LS1046A RCW settings for FPGA configuration? in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/How-can-I-modify-LS1046A-RCW-settings-for-FPGA-configuration/m-p/2162111#M16040</link>
    <description>&lt;P&gt;We are using an assembly of 9 boards, and each board contains one FPGA.&lt;/P&gt;&lt;P&gt;Among them, only one board has the CPU(LS1046A) and the central control FPGA.&lt;/P&gt;&lt;P&gt;Our board is configured to boot from eMMC.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I modified the U-Boot source code and increased the IFC_AMASK2 value from the default 64KB to 1MB.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;We plan to access these boards using the addresses 0x7FBx_0000 (where x = 0 ~ 8 is used for board selection).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The central control FPGA reads ifc_a[27:16], and among them, ifc_a[19:16] is used for board selection.&lt;/P&gt;&lt;P&gt;Our expectation is that:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;When accessing 0x7FB00000, the value should be 0&lt;/LI&gt;&lt;LI&gt;When accessing 0x7FB10000, it should be 1&lt;/LI&gt;&lt;LI&gt;… and so on, up to 8 for the 9 boards.&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Below I have attached my RCW source, the U-Boot source, and two schematics showing the FPGA connections.&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;LI-PRODUCT title="LS1046A" id="LS1046A"&gt;&lt;/LI-PRODUCT&gt;&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 02 Sep 2025 11:18:30 GMT</pubDate>
    <dc:creator>2sanghaesea</dc:creator>
    <dc:date>2025-09-02T11:18:30Z</dc:date>
    <item>
      <title>How can I modify LS1046A RCW settings for FPGA configuration?</title>
      <link>https://community.nxp.com/t5/Layerscape/How-can-I-modify-LS1046A-RCW-settings-for-FPGA-configuration/m-p/2162111#M16040</link>
      <description>&lt;P&gt;We are using an assembly of 9 boards, and each board contains one FPGA.&lt;/P&gt;&lt;P&gt;Among them, only one board has the CPU(LS1046A) and the central control FPGA.&lt;/P&gt;&lt;P&gt;Our board is configured to boot from eMMC.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I modified the U-Boot source code and increased the IFC_AMASK2 value from the default 64KB to 1MB.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;We plan to access these boards using the addresses 0x7FBx_0000 (where x = 0 ~ 8 is used for board selection).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The central control FPGA reads ifc_a[27:16], and among them, ifc_a[19:16] is used for board selection.&lt;/P&gt;&lt;P&gt;Our expectation is that:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;When accessing 0x7FB00000, the value should be 0&lt;/LI&gt;&lt;LI&gt;When accessing 0x7FB10000, it should be 1&lt;/LI&gt;&lt;LI&gt;… and so on, up to 8 for the 9 boards.&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Below I have attached my RCW source, the U-Boot source, and two schematics showing the FPGA connections.&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;LI-PRODUCT title="LS1046A" id="LS1046A"&gt;&lt;/LI-PRODUCT&gt;&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 02 Sep 2025 11:18:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/How-can-I-modify-LS1046A-RCW-settings-for-FPGA-configuration/m-p/2162111#M16040</guid>
      <dc:creator>2sanghaesea</dc:creator>
      <dc:date>2025-09-02T11:18:30Z</dc:date>
    </item>
    <item>
      <title>Re: How can I modify LS1046A RCW settings for FPGA configuration?</title>
      <link>https://community.nxp.com/t5/Layerscape/How-can-I-modify-LS1046A-RCW-settings-for-FPGA-configuration/m-p/2162313#M16043</link>
      <description>&lt;P&gt;Dear&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/242417"&gt;@2sanghaesea&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I hope you are doing well.&lt;/P&gt;
&lt;P&gt;please don't use&amp;nbsp; the next signals (even if you reconfigured them into the RCW), use them just for booting,&amp;nbsp; the rest of the signals are ok.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="LFGP_0-1756834531065.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/355234i596FC3E62BFBA75E/image-size/medium?v=v2&amp;amp;px=400" role="button" title="LFGP_0-1756834531065.png" alt="LFGP_0-1756834531065.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;LFGP_0-1756834531065.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;LFGP&lt;/P&gt;</description>
      <pubDate>Tue, 02 Sep 2025 17:38:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/How-can-I-modify-LS1046A-RCW-settings-for-FPGA-configuration/m-p/2162313#M16043</guid>
      <dc:creator>LFGP</dc:creator>
      <dc:date>2025-09-02T17:38:10Z</dc:date>
    </item>
  </channel>
</rss>